4.1. Release notes - 09_01_00¶
4.1.1. Documentation¶
The documentation included with the PSDK QNX J784S4 is specific to the PSDK QNX J784S4 package.
PSDK RTOS J784S4 package documentation (PSDK RTOS Components) must also be referenced, for full understanding of PSDK QNX J784S4 support.
4.1.2. PSDK QNX J784S4 Features¶
Note
Reference PSDK RTOS J784S4 package documentation (LINK) for an extensive list of new and current features supported by PSDK QNX + PSDK RTOS. This section lists only the features that are PSDK QNX J784S4 specific.
Note
For features & drivers enabled by the QNX BSP, please refer to BSP Documentation or contact QNX.
Note
The release is tested on Ubuntu (x86_64) 18.04 & 22.04 system and may not work on earlier or later Ubuntu systems.
4.1.2.1. Enabled in this Release¶
Features enabled in this release, specific to PSDK QNX J784S4 addon package are:
The release package now has version controlled with git with a single release commit to enable convenient patching
Added Lossless encoding support for the VPU encoder
Updated shared memory allocator allocations for VisionApps carveout
CPSW updates - Note: Please use the PSDK RTOS release 09_01_00
Removed dependency on remote device.
UDMA updates
UDMA driver refactor to enable concurrent access of udma resources
Added test capability to support larger memcpy for UDMA
Bug Fixes
IPC driver returns incorrect return code during a timeout
Remove dependency on bootloader to set the MMCSD clocks
Added support to allocate UDMA proxy per process
For additional new updates, please refer PSDK RTOS package documentation (PSDK RTOS Components).
4.1.2.2. Enabled in Previous Releases¶
Features enabled in previous release, specific to PSDK QNX J784S4 addon package are:
Support for QNX SDP 7.1
Shared Memory Allocator Resource Manager
SCIClient Resource Manager
A72 OpenVx Integration
A72 Vision Apps Demo Support
UDMA Resource Manager
IPC Resource Manager
K3conf utility
SBL Boot flow support for QNX
DDR BW analysis tool
Datasheet added for IPC and io-pkt cpsw ethernet drivers
Support and validation with the PSDK RTOS release
PDK library build updated from using PDK makefile system to QNX makefile
Update to build system to use QCONF_OVERRIDE and support for .sym file
Debug build profile deprecate from the PSDK QNX build system
Datasheet added for VPU Codec
IO-PKT CPSW2G Driver
A72 driver for CPSW2G
Support for gPTP
Use of enet-lld
SMMU support
HW-checksum offloading
IO-PKT CPSW9G Virtual Driver
A72 driver for CPSW9G
Use of enet-lld
Time sync with EthFW support added to CPSW9G Virtual driver
HW-checksum offloading
Single core multicast support
Support for dynamic IP and MAC configuration
VPU video codec updates
Resource manager support for VPU video encoder
Resource manager support for VPU video decoder
Multicore codec support.
Codec IO-buffer and Internal buffer management using SharedMemoryAllocator.
Supports usage of DDR high-mem (>4G range). Default base address is “0x8 C000 0000” with a total of 768MB.
OMX IL Component support for VPU video encoder and File-based OMX encoder test application (H.264 & HEVC)
Supports logging at different levels
Supports a multi-threaded implementation
Encoder multichannel support upto 8x1080p streams
Encoder supports performance upto 1x1080p at 60fps and 2x1080p at 30fps
OMX IL Component support for VPU video decoder and File-based OMX decoder test application (H.264 & HEVC)
Supports zero-copy buffer passing between application and codec
Supports I, P and B frame decoding
Supports decode of stream headers in advance
Supports logging at different levels
Supports a multi-threaded implementation
HW Watchdog for Decoder
Decoder to recovery from SW stream errors
Decoder supports deblocking filter
VPU codec (encoder and decoder) with test app
HEVC & H.264 4K Encode support with file-to-file encode test app
HEVC & H.264 4K Decode support with file-to-file decode test app
Multi-instance HEVC/H.264 Encode & Decode support with multi-inst test app
OMX IL Component support for VPU video encode & decode (H.264 & HEVC)
Decode/Encode: Support for 2x HW VPU instances for Video Encode / Decode
Decode/Encode: Supports Interrupt mode for VPU codec
Decode/Encode: Supports 8 channel D1@30fps Encode + 8 channel D1@30fps Decode
Encode: Supports Rate control - VBR and CBR
Encode: Supports CBR (e.g., for Video Conferencing), 2-10 Mbps
Decode: Performance profiler added for VPU decode
Decode: Publish Codec Capabilities through API
Bug fixes
Sciclient random ACK failure fixed.
UDMA Resource Manager fixed the duplicate UDMA flow-id allocation
Running iperf with parallel instance of cpsw2g and cpsw9g
The ipc_test failing to ping ipc echo testb DM image
The tiudma-mgr cannot be restarted after being slayed
The udma_memcpy_test hangs forever in case of failure
CPSW2G direct ethernet cable connection
Decode: Fixed junk frames at the end for streams greater than 1080p
Decode/Encode: Multi-instance decode/encode failure fixed
Decode: OMX decoder fails to decode H.264 Level5 bitstreams of long play length
Decode: VPU fails to decode high-bitrate (>100 Mbps) 4K resolution videos
Decode: OMX decoder fails to decode 2x 4K HEVC/H264 bitstreams due to out-of-memory
Decode: OMX decode application does not check for num input bufs being exactly 2
Decode: OMX decode of 4x H.264 1080p bitstreams produces incorrect output frames
For additional new updates, please refer PSDK RTOS package documentation (PSDK RTOS Components).
4.1.2.3. Change Requests¶
None
4.1.2.4. Errata¶
Please refer release note in the PSDK RTOS J784S4 package documentation (PSDK RTOS Components) for the complete errata list.
4.1.3. Software Dependencies¶
4.1.3.1. QNX Dependency¶
Note
The PSDK QNX addon package is dependent on installations from QNX Software Center. The below QNX packages were used for PSDK QNX 09_01_00 build and verification.
4.1.3.1.1. QNX SDP 7.1¶
QNX SDP 710 Package |
Build ID |
Package ID |
Package Version |
---|---|---|---|
QNX® Software Development Platform 7.1 |
472 |
com.qnx.sdp710 |
7.1.0.00472T202006132107S |
QNX® SDP 7.1 Screen Board Support J784S4 (with Debug Symbols) |
137 |
com.qnx.qnx710.target.screen.board.j784s4 |
3.2.0.00137T202210261823L |
QNX® SDP7.1 BSP for Texas Instruments Jacinto 7 J784S4 Evaluation Modules |
12 |
com.qnx.qnx710.bsp.ti_j784s4_evm |
0.0.7.00012T202306011431L |
QNX® SDP 7.1 Multimedia - OpenMAX IL API (with Debug Symbols) |
404 |
com.qnx.qnx710.target.mm.openmaxil.core |
2.1.0.00404T202201111113L |
4.1.3.2. PSDK RTOS Dependency¶
The PSDK QNX package is an addon package to the PSDK RTOS release, as such the PSDK RTOS is required.
4.1.3.3. PSDK LINUX Dependency¶
If SPL boot mode is to be supported, downloading the PSDK LINUX 09_01_00 package is recommended for access to the pre-built binaries.
4.1.4. Device Support and Validation Information¶
SoC |
Build Host (OS) |
Run Target (OS) |
Test Platform |
---|---|---|---|
J784S4 |
x86_64 (Linux Ubuntu 18.04) |
R5F & C7x running TI-RTOS A72 running QNX |
TI EVM with daughter cards |
Note
Refer EVM Setup for J784S4 for more details on the TI EVM support.
4.1.5. Open Defects¶
Below table lists all the open defects:
ID |
Head Line |
---|---|
VPU: QNX Encoder Performance - 4x 1080p60 not met. At 47fps now |
|
VPU: OMX video decode should exit gracefully when trying to decode a bad video file |
|
VPU: OMX decoder fails to decode H.264 mixed resolution 1080p/720p video |
|
QNX: J721S2 & J784S4 IPC round trip time is greater than expected range |
|
Virtual client: io-pkt: Fix memory leak during CPSW recovery |
4.1.6. Known Issues¶
A list of key known issues with the PSDK QNX release is provided below.
Note
Refer to individual PSDK RTOS Components release notes for known issues in each component
Index |
Module |
Description |
---|---|---|
1 |
QNX IPC RM |
RPMessage_recv() can fail during combinatorial stress run |
2 |
QNX UDMA RM |
UDMA resource manager may not free UDMA resources when client exits unexpectedly. |
3 |
QNX CPSW |
CPSW recovery functionality is not functional as of the early release. |
4.1.7. Additional Reports¶
For additional reports like test report, traceability refer PSDK RTOS Additional Reports