4.1. Release notes - 11_01_00

4.1.1. Documentation

The documentation included with the PSDK QNX SDK is specific to the PSDK QNX J721S2 package and for SDP 8.0.

PSDK RTOS J721S2 package documentation (PSDK RTOS Components) must also be referenced, for full understanding of PSDK QNX J721S2 support.

4.1.2. PSDK QNX J721S2 Features

Note

  • Reference PSDK RTOS J721S2 package documentation (LINK) for an extensive list of new and current features supported by PSDK QNX + PSDK RTOS. This section lists only the features that are PSDK QNX J721S2 specific.

  • For features & drivers enabled by the QNX BSP, please refer to BSP Documentation or contact QNX.

  • The release is tested on Ubuntu (x86_64) 22.04 system and may not work on earlier or later Ubuntu systems.

  • If using low-mem codec carveout prior to this release, please adjust your startup carveouts accrdingly, as the TI configuration no longer provides this by default

4.1.2.1. Enabled in this Release

Features enabled in this release, specific to PSDK QNX J721S2 package are:

  • IPC Resource manager now has an argument to configure the ISR thread priority.

    • Non-ISR threads remain configurable via the QNX on -p <priority> <executable> utility.

  • Added support for reading CPU load information in app_utils.

  • Added utility reading DIE ID information (run use ti-hwmon for more details).

  • Added utility for reading VTM temperature sensor information (run use ti-hwmon for more details).

  • Bug fixes

    • OSAL: Fixed HwiP_create not respecting requested thread priorities.

For additional new updates, please refer PSDK RTOS package documentation (PSDK RTOS Components).

4.1.2.2. Enabled in Previous Releases

Features enabled in previous release, specific to the PSDK QNX J721S2 package are:

  • Freed up unused low-mem codec careveout (256MB) in j721s2-evm-ti.build file

  • Shared Memory Allocator Resource Manager

  • SCIClient Resource Manager

  • A72 OpenVx Integration

  • A72 Vision Apps Demo Support

  • UDMA Resource Manager

  • IPC Resource Manager

  • K3conf utility

  • SBL Boot flow support for QNX

  • DDR BW analysis tool

  • Datasheet added for IPC and io-pkt cpsw ethernet drivers

  • Support and validation with the PSDK RTOS release

  • PDK library build updated from using PDK makefile system to QNX makefile

  • Update to build system to use QCONF_OVERRIDE and support for .sym file

  • Debug build profile deprecate from the PSDK QNX build system

  • Datasheet added for VPU Codec

  • The release package now has version controlled with git with a single release commit to enable convenient patching

  • Added Lossless encoding support for the VPU encoder

  • Adapted devnp API changes to match ETHFW changes to support static TX channels

  • Freed up unused low-mem codec careveout (256MB) in j721s2-evm-ti.build file

  • A developer note for enabling QNX display driver is available.

  • Safety qualified drivers for UDMA, OSAL, SCIClient and safety qualified OSAL library

    • Please get in touch with your TI contact for details on how to request for the CSP (Compliance Support Package).

  • VPU video codec updates

    • Empirical values for internal and external buffers used for Codec published.

    • Various encode and decode fps rates published.

    • Added Lossless encoding support for the VPU encoder

    • Updated shared memory allocator allocations for VisionApps carveout

    • Resource manager support for VPU video encoder

    • Resource manager support for VPU video decoder

    • Codec IO-buffer and Internal buffer management using SharedMemoryAllocator.

    • Supports usage of DDR high-mem (>4G range). Default base address is “0x8 C000 0000” with a total of 768MB.

  • OMX IL Component support for VPU video encoder and File-based OMX encoder test application (H.264 & HEVC)

    • Configurable GOP Preset support. Can configure combinations of I and P frames

    • Supports logging at different levels

    • Supports a multi-threaded implementation

    • Encoder multichannel support upto 8x1080p streams

    • Encoder supports performance upto 1x1080p at 60fps and 2x1080p at 30fps

    • Added SPS & PPS NAL units along with each IDR frame

  • OMX IL Component support for VPU video decoder and File-based OMX decoder test application (H.264 & HEVC)

    • Support for YUV 420 and pseudo-YUV 422 output formats.

    • Supports zero-copy buffer passing between application and codec

    • Supports I, P and B frame decoding

    • Supports decode of stream headers in advance

    • Supports logging at different levels

    • Supports a multi-threaded implementation

    • HW Watchdog for Decoder

    • Decoder to recovery from SW stream errors

    • Decoder supports deblocking filter

    • Support for block-level spatial & temporal error concealment

    • Support for user input to determine number of non-linear frame buffers

  • VPU codec (encoder and decoder) with test app

    • HEVC & H.264 4K Encode support with file-to-file encode test app

    • HEVC & H.264 4K Decode support with file-to-file decode test app

    • Multi-instance HEVC/H.264 Encode & Decode support with multi-inst test app

  • Bug fixes

    • UDMA driver refactor to enable concurrent access of udma resources

    • Added test capability to support larger memcpy for UDMA

    • IPC driver returns incorrect return code during a timeout

    • Remove dependency on bootloader to set the MMCSD clocks

    • Added support to allocate UDMA proxy per process

    • The ipc_test failing to ping ipc echo testb DM image

    • The tiudma-mgr cannot be restarted after being slayed

    • The udma_memcpy_test hangs forever in case of failure

    • CPSW2G direct ethernet cable connection

    • Decode: Fixed junk frames at the end for streams greater than 1080p

    • Decode/Encode: Multi-instance decode/encode failure fixed

    • Decode: OMX decoder fails to decode H.264 Level5 bitstreams of long play length

    • Decode: VPU fails to decode high-bitrate (>100 Mbps) 4K resolution videos

    • Decode: OMX decoder fails to decode 2x 4K HEVC/H264 bitstreams due to out-of-memory

    • Decode: OMX decode application does not check for num input bufs being exactly 2

    • Decode: OMX decode of 4x H.264 1080p bitstreams produces incorrect output frames

    • Added qnxfs partition for SD card boot to address boot time delay

    • Sciclient random ACK failure fixed.

    • UDMA Resource Manager fixed the duplicate UDMA flow-id allocation

    • Remove DEBUG_PRINT flag in the ipclld common.mk file

    • Address Compiler Warning -Wno-address-of-packed-member

    • OSAL: DebugP_log1 using _SLOG_ERROR instead of _SLOG_LOG

For additional new updates, please refer PSDK RTOS package documentation (PSDK RTOS Components).

4.1.2.3. Change Requests

The following Change requests have been made for this release.

  • Deprecate cpsw2/5/9g driver based on io-pkt driver for QNX SDP 7.1 post 11.x release. Maintain io-pkt with existing features until the next major release.

4.1.2.4. Errata

Please refer release note in the PSDK RTOS J721S2 package documentation (PSDK RTOS Components) for the complete errata list.

4.1.2.5. Hardware support

Note

Refer to Release Notes in PSDK RTOS User Guide(LINK) for detailed information on supported Hardware.

4.1.3. Software Dependencies

4.1.3.1. QNX Dependency

Note

The PSDK QNX package is dependent on installations from QNX Software Center. The below QNX packages were used for PSDK QNX 11_01_00 build and verification.

4.1. QNX SDP 8.0

Important

For information on io-sock ethernet driver refer to the developer note CPSW Ethernet driver support - io-sock vs io-pkt.

QNX SDP 800 Package

Build ID

Package ID

Package Version

QNX® Software Development Platform 8.0

141

com.qnx.qnx800

8.0.0.00141T202311271501L (Validated against this version contact QNX for latest)

QNX® SDP 8.0 Screen Board Support J721S2 (with Debug Symbols)

132

com.qnx.qnx800.target.screen.board.j721s2

4.0.2.00132T202501161817L

QNX® SDP 8.0 BSP for Texas Instruments Jacinto 7 J721S2 Evaluation Modules

337

com.qnx.qnx800.bsp.hw.ti_j721s2_evm

0.3.0.00337T202507311445L

QNX® SDP 8.0 Networking - io-sock

600

com.qnx.qnx800.target.net.iosock

0.3.0.00600T202507302003L

QNX® SDP 8.0 Networking - io-sock cpsw Drivers

104

com.qnx.qnx800.target.net.devs.cpsw

0.3.0.00104T202507311314L

4.1.4. Device Support and Validation Information

SoC

Build Host (OS)

Run Target (OS)

Test Platform

J721S2

x86_64 (Linux Ubuntu 22.04)

R5Fs running TI-RTOS

A72 running QNX

TI EVM with daughter cards

Note

Refer EVM Setup for J721S2 for more details on the TI EVM support.

4.1.5. Open Defects

Below table lists all the current open defects:

ID

Head Line

EXT_PSDKQA-5

QNX: J721S2 & J784S4 IPC round trip time is greater than expected range

EXT_PSDKQA-8

VPU: OMX decoder fails to decode H.264 mixed resolution 1080p/720p video

EXT_PSDKQA-16

VPU: QNX Encoder Performance - 4x 1080p60 not met. At 47fps now

EXT_PSDKQA-24

SDK to evaluate and remove short_enums compiler flag across modules

EXT_PSDKQA-28

QNX IPC - Need to make the task priority a configurable item

4.1.6. Closed Issues

Below table lists all the defects closed from previous releases:

ID

Head Line

EXT_PSDKQA-23

Address Compiler Warning -Wno-address-of-packed-member

EXT_PSDKQA-25

OSAL: DebugP_log1 using _SLOG_ERROR instead of _SLOG_LOG

EXT_PSDKQA-27

Remove DEBUG_PRINT flag in the ipclld common.mk file

4.1.7. Known Issues

A list of key known issues with the PSDK QNX release is provided below.

Note

Refer to individual PSDK RTOS Components release notes for known issues in each component

Index

Module

Description

1

QNX UDMA RM

UDMA resource manager may not free UDMA resources when client exits unexpectedly.

2

QNX Networking (io-sock)

Issues have been seen trying to run io-sock with revision com.qnx.qnx800.target.net.iosock/0.0.2.00417T202407041502L. Please use the specified revision mentioned above. Further support should be directed to QNX.

4.1.8. Additional Reports

For additional reports like test report, traceability refer PSDK RTOS Additional Reports