8. CCS Setup for J721S2

Code Composer Studio is an integrated development environment (IDE) that supports TI’s Micro controller and Embedded Processors portfolio. It provides useful tools to develop and debug embedded applications.

Please visit Code Composer Studio product (https://www.ti.com/tool/ccstudio) for more information.

Important

  • Below screen shots and examples show paths and instructions for Windows. The same applies for Linux except use Linux file/folder paths instead.

  • In QNX+RTOS mode, SPL/uboot or the SBL loads the R5F, C7x, A72 binaries

    • CCS is needed to debug the software on R5F, C7x (and A72 when in RTOS mode).

  • In RTOS only mode, CCS is needed to load and run the binaries on different CPU cores in the SoC.

  • The CCS emulation pack and CSP (Chip Support Package) needs to be downloaded separately.

8.1. CPU names used in PSDK_RTOS/PSDK_QNX vs CCS

Below table shows the mapping of names in PSDK RTOS and CCS

CPU name in PSDK RTOS

CPU name in CCS

mcu1_0 / mcu1_1

MCU_Cortex_R5_0 / MCU_Cortex_R5_1

mcu2_0 / mcu2_1

MAIN_Cortex_R5_0_0 / MAIN_Cortex_R5_0_1

mcu3_0 / mcu3_1

MAIN_Cortex_R5_1_0 / MAIN_Cortex_R5_1_1

mpu1

CortexA72_0_0

c7x_1

C71x_0

c7x_2

C71x_1

8.2. Step 1: Install CCS

  1. Install CCS v11.0 : CCS can be downloaded from https://software-dl.ti.com/ccs/esd/documents/ccs_downloads.html#code-composer-studio-version-11-downloads

  2. CCS installation details are available on https://software-dl.ti.com/ccs/esd/CCSv11/CCS_11_0_0/exports/CCS_11.0.0_ReleaseNotes.htm

  3. This release is tested on below CCS version 11.0.0.00012

    _images/ccs_version.png

    Fig. 8.1 CCS: IDE version

  4. During installation, there is a ‘Setup’ step where you can select components. Be sure to select: “TDAx Driver Assistance SoCs & Jacinto DRAx Infotainment SoCs” as shown below:

    _images/ccs_setup.png

    Fig. 8.2 CCS: Download Components

  5. Here after we’ll be referring to the CCS installation directory as ${CCS_INSTALL_PATH}

    In Linux, this will be

    ${HOME}/ti/ccsv1100/ccs
    

    In Windows, this will be

    C:\\ti\\ccsv1100\\ccs\
    

8.3. Step 2: Install CCS Chip Support Package and Emulation packs

Note

  • J721S2 CSP is included in the PDK Package

  • This is present in ${PDK_INSTALL_DIR}/J721S2_CSP

8.3.1. Step 2.1: Install CSP (chip support package) for J721S2 SoC

  • For Windows,

    • Copy the contents of the folder ${PDK_INSTALL_DIR}/J721S2_CSP/ccs_patch_windows/ccs_base to the ${CCS_INSTALL_PATH}/ccs_base folder.

  • For Linux,

    • Copy the contents of the folder ${PDK_INSTALL_DIR}/J721S2_CSP/ccs_patch_linux/ccs_base to the ${CCS_INSTALL_PATH}/ccs_base folder.

  • Make sure that you replace the files when prompted.

  • Copy the contents of the folder ${PDK_INSTALL_DIR}/J721S2_CSP/gel to the ${CCS_INSTALL_PATH}/ccs_base/emulation/gel folder.

8.3.2. Step 2.2: Install CCS emulation pack

  • Install the following file in ${PDK_INSTALL_DIR}/J721S2_CSP to ${CCS_INSTALL_PATH}.

    • For Windows,

      • ti_emupack_setup_9.5.0.00153_win_64.exe

    • For Linux,

      • ti_emupack_setup_9.5.0.00153_linux_x86_64.bin

Warning

  • When prompted for installation folder, you should give the installation folder as ${CCS_INSTALL_PATH}

Warning

For Linux, After CCS installion run the install drivers script:

  • Go to the install scripts directory.

    cd ${CCS_INSTALL_PATH}/install_scripts
    
  • Run install script as sudo

    sudo ./install_drivers.sh
    
  • Restart your PC

8.4. Debugging without HLOS running on A72 (RTOS-only / baremetal)

Important

8.4.1. Step 3: Setup CCS target configuration and GELs files

  1. Create a CCS target config, you can name it J721S2_EVM.ccxml.

    • In Code Composer Studio, go to the File menu and select New -> Target Configuration File

    • Name the Target Configuration file as J721S2_EVM.ccxml and click Finish

    • Select Connection as Texas Instruments XDS110 USB Debug Probe, if you are using on board debugger (J3 usb connector)

    • Select Connection as Spectrum Digital XDS560V2 STM USB Emulator, if you are using Spectrum digital XDS560 USB debugger connected to JTAG Mipi connector (J16)

    • Select the Board as Jacinto7AEP shown below

      _images/ccs_target_config_j721s2.png

      Fig. 8.3 CCS: Target Configuration

  2. Load the initialization script of the Cortex_M4F_0 core with the J7AEP Gels as shown below.

    • Open the Advanced tab of the target configuration file J721S2_EVM.ccxml

    • Go to CORTEX_M4F_0 under SMS_TIFSM

    • Set the initialization script

    • Gel files can be found at below path

      **${CCS_INSTALL_PATH}/ccs_base/emulation/gel/J7AEP_TDA4AL/J7AEP_SI.gel
      
      _images/ccs_target_config_init_script_j721s2.png

      Fig. 8.4 CCS: Target Configuration Initialization Script

8.4.2. Step 4: Load RTOS/baremetal application binaries thru CCS

Note

  • When using CCS boot flow, please configure EVM in NOBOOT mode ( see No Boot Mode ) for connecting and loading binaries via CCS.

  • NO BOOT Mode Switch Settings:-

  • SW8[1-8] = 1000 1000

  • SW9[1-8] = 0111 0000

  • The launch.js file below is responsible to load and run the DMSC. It is also responsible to set the board configuration input for the DMSC. The board configuration is passed by the PDK example ${PSDK_RTOS_PATH}/pdk_j721s2_{version}/packages/ti/drv/sciclient/examples/sciclient_ccs_init executing on the MCU R5F core. The default board configuration is available for reference at ${PSDK_RTOS_PATH}/pdk_j721s2_{version}/packages/ti/drv/sciclient/soc/V1/sciclient_defaultBoardcfg.c

  • All PDK and SDK examples require the DMSC firmware to be executed.

  • launch.js file is also responsible to load the ${PSDK_RTOS_PATH}/pdk_j721s2_{version}/packages/ti/drv/sciclient/examples/sciserver_testapp which is used to service the RM and PM services on MCU1_0. Refer mcu1_0_app_with_sysfw PSDK RTOS developer note for details. The sciserver_testapp is a simple RTOS based application which runs the Sciserver used to service RM and PM requests from cores other than MCU1_0.

  • For applications developed and debugged on MCU1_0 application one can disable loading the Sciserver_testapp by setting the loadSciserverFlag to 0. Please do go through the mcu1_0_app_with_sysfw PSDK RTOS developer note page for details on what libraries should be linked on the MCU1_0 application to run RM and PM services.

  1. GEL initialization

    • Open the launch.js script in an editor. Script is present in below path:

      ${PSDK_RTOS_PATH}/pdk_j721s2_{version}/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721s2/launch.js
      
    • ${PSDK_RTOS_PATH} is the path to your PSDK RTOS installation, for example:

      /ti/ti-processor-sdk-rtos-j721s2-evm-xx_xx_xx_xx
      
    • Edit the variable “pdkPath” with the absolute path of the pdk package, i.e ${PSDK_RTOS_PATH}/pdk_j721s2_{version}/packages

    • Open Code Composer Studio and launch the Target Configuration previously setup

      _images/ccs_launch_ccxml.png

      Fig. 8.5 CCS: Launch CCS Target Configuration

    • Go to the View Target configurations and launch a target configuration is done by right clicking on it.

    • Open the scripting console in CCS - Go to the View menu and then select Scripting Console

    • Load the launch.js script as shown below.

      _images/ccs_launch_script_j721s2.png

      Fig. 8.6 CCS: Launch script

    • Wait till the script finishes. This step can take considerable time as it configures PLL etc. in the SOC via GEL files and configures DDR. This will connect to the MCU_Cortex_R5_0 core.

      _images/ccs_launch_script1_j721s2.png

      Fig. 8.7 CCS: Scripting Console Output

      _images/ccs_launch_script2_j721s2.png

      Fig. 8.8 CCS: Console Output

    • After script completes execution you should see below in Debug window

      _images/launch_dss_script_complete.png

      Fig. 8.9 CCS: Launch script Complete

  2. Load and run the binaries in CCS. Debug as usual using CCS.

    • Now you can connect to any core and load the corresponding application binaries.

      _images/ccs_connect_target.png

      Fig. 8.10 CCS: Loading the demo application binary

    • Go to the Run menu and then select Load -> Select Program to Load

    • In the Load Program window, browse to application binary you want to load.

      _images/ccs_load_binary.png

      Fig. 8.11 CCS: Loading the demo application binary

    • Go to the Run menu and then select Resume to start executing demo binary.

8.5. Debugging with HLOS running on A72 (Linux / QNX)

Important

  • This section is applicable only if you are loading a HLOS (Linux or QNX) application. To debug RTOS cores using CCS when not running Linux or QNX on A72, refer section Debugging without HLOS running on A72 (RTOS-only / baremetal).

  • CCS cannot be used to debug applications on the A72. For Linux, it is recommended to use gdb which comes preinstalled on the filesystem. For QNX, it is recommended to use QNX Momentics.

8.5.1. Step 3: Setup CCS target configuration

  1. Install CCS, CCS emulation packs and the CSP as per Step 1: Install CCS.

  2. Create a CCS target config, you can name it “J721S2_EVM_NO_GEL.ccxml”.

    • Select Connection as Texas Instruments XDS110 USB Debug Probe, if you are using on board debugger (J3 usb connector)

    • Select Connection as Spectrum Digital XDS560V2 STM USB Emulator, if you are using Spectrum digital XDS560 USB debugger connected to JTAG Mipi connector (J16)

    • Select the Board as Jacinto7AEP shown below

      _images/ccs_target_config_j721s2.png

      Fig. 8.12 CCS: Target Configuration

    • Remove the gel file path (....emulationgelJ721S2_TDA4VLgelJ721S2.gel) from CORTEX_M4F_0 under SMS_TIFSM

8.5.2. Step 4: Load RTOS core firmware symbols thru CCS

  1. Load the debug version of the firmware binaries on the HLOS file system, and boot device.

  2. Launch the target config file created

    _images/ccs_target_config_launched_j721s2.png

    Fig. 8.13 CCS: Target Configuration launched

  3. Now you can connect to the required non-A72 core (i.e R5, C7x_0 etc) and load the symbols of the application binary.

    _images/ccs_target_config_load_symbols.png

    Fig. 8.14 CCS: Load symbols in the connected non-A72 core

  4. Now you can put breakpoints wherever required and debug as usual.

8.6. Debugging with QNX on A72 using QNX Momentics IDE

  1. For debuging with QNX on A72, make sure you have the QDE Momentics tool installed in your PC.

  2. Follow the steps mentioned in QNX website to connect to the board from QDE