5. PSDK QNX Components

5.1. QNX BSP release

The QNX BSP package must be downloaded from QNX Software Center or Contact QNX.

Note

Refer Release Notes software dependencies section for more information.

For the purposes of creating a consolidated build process and in turn allowing for support of scripts to create SD content, the BSP needs to be extracted to the folder within the PSDK QNX build environment as show below.

For QNX SDP 7.1:

# Unzip the BSP
mkdir -p ${PSDK_RTOS_PATH}/psdkqa/qnx/bsp
cd ${PSDK_RTOS_PATH}/psdkqa/qnx/bsp
unzip ${QNX_BASE}/bsp/BSP_ti-j7-tda4vmeco-evm_br-710_be-710_<version>.zip

5.1.1. TI Modifications to the BSP

Memory Carveout

Memory sections with pre-defined physical addresses must be set aside in the QNX BSP IFS build file so that the memory is not given to other programs and can be used solely by the remote cores and video codec

Specify a section to be set aside by modifying the startup line to use the “-r” option. To reserve 0x80000000 bytes, starting at physical address 0x90000000, on J721S2 QNX BSP, the build file the arguments would be (highlighted below):

[+keeplinked] startup-j721s2-evm -v -r0x90000000,0x10000000,1 -r0xA0000000,0x60000000,1 -r0x880000000,0x10000000,1

Note

  • For video codecs, the memory carveout is at address 0x90000000 and of size 0x10000000

  • For vision apps remote cores, the memory carveout is at address 0xA0000000 and of size 0x70000000
    • The initial remote core carevout 0x60000000 is in the lower 4GB memory range starting at address 0xA0000000.

    • The remaining remote core carevout 0x10000000 is in the higher 4GB memory range starting at address 0x880000000.

Reference TI build file

The reference TI build file is provide in the qnx/scripts/bsp/<BSP_REVISION> directory.

# Copy in TI specific build scripts and settings to allow building of a QNX-IFS which supports
# vision_apps demos and video codec demos
cp ${PSDK_RTOS_PATH}/psdkqa/qnx/scripts/bsp/<BSP_REVISION>/j721s2-evm-ti.build ${PSDK_RTOS_PATH}/psdkqa/qnx/bsp/images/

Note

Other build file deltas between QNX and TI PSDK QNX environment may be present. TI modifies build scripts for ease of use on TI EVM and running of demonstration software

5.2. SCI Client Resource Manager

The SCI Client Resource Manager (tisci-mgr) provides support for multiple users to make use of the sciclient library from PSDK RTOS without interfering with each other requests. It provides a mechanism to serialize the transactions to the DMSC.

Note

The tisci-mgr logs the SYSFW information to the slogger.

Note

Refer PSDK RTOS Components for more information about each individual component.

5.3. IPC Resource Manager

5.3.1. Overview

The IPC resource manager (tiipc-mgr) provides a processor-agnostic API which can be used for communication between processors in a multi-processor environment.

The IPC resource manager provides a user library (tiipc-usr) that exposes the IPC LLD API to QNX applications for communication through the IPC resource manager. The IPC LLD API is described in detail in the PDK documentation.

5.3.2. Example Application

An IPC example application (ipc_test) is provided to test the IPC communication with remote cores running the IPC echo test remote core firmware images.. To use this application, the appropriate remote core firmware images need to be built and placed on the target filesystem. The following remote core firmware images are needed:

Firmware Name

Core(s)

ipc_qnx_echo_testb_freertos

use for mcu1_0

ipc_qnx_echo_test_freertos

use for mcu2_0, mcu2_1, mcu3_0, mcu3_1, C7x_1 and C7x_2

For remote core firmware build instructions, please refer to the IPC LLD PDK documentation.

Note

For the ipc_test to work with ipc echo test remote core firmware images, The IPC resource manager (tiipc-mgr) need to be built with “VISION_APPS_BUILD_FLAGS_MAK=0” build flag, so that the correct VRING_BASE_ADDRESS is used.

Note

The below step to copy the remote core firmware to the rootfs partition of target filesystem is applicable only to the SPL-UBOOT bootflow. For the SBL-BootApp bootflow, the ipc echo test image need to be bundled into the Appimage. Please refer to the MCUSW documentation for details.

Once the remote core firmware is built, copy the images to the target filesystem in the rootfs partition. Existing firmware binaries should be backed up as required. The ex02* firmware binaries should be renamed to the firmware name expected by the bootloader. For example:

cp ipc_qnx_echo_test_freertos_c7x_1_release.xe71 ${ROOTFS}/lib/firmware/j721s2-c71_0-fw
cp ipc_qnx_echo_test_freertos_c7x_2_release.xe71 ${ROOTFS}/lib/firmware/j721s2-c71_1-fw
cp ipc_qnx_echo_test_freertos_mcu3_1_release.xer5f ${ROOTFS}/lib/firmware/j721s2-main-r5f1_1-fw
cp ipc_qnx_echo_test_freertos_mcu3_0_release.xer5f ${ROOTFS}/lib/firmware/j721s2-main-r5f1_0-fw
cp ipc_qnx_echo_test_freertos_mcu2_1_release.xer5f ${ROOTFS}/lib/firmware/j721s2-main-r5f0_1-fw
cp ipc_qnx_echo_test_freertos_mcu2_0_release.xer5f ${ROOTFS}/lib/firmware/j721s2-main-r5f0_0-fw

Note

As seen above, the mcu1_0 firmware image is not copied to the target filesystem in the rootfs partition. Instead it need to be built into the tispl.bin as part of the SPL-UBOOT boot binaries.

For testing ipc with mcu1_0 image, the PSDK Linux package is required to be installed. The default SPL-UBOOT binaries include the ipc test mcu1_0 image that work with Linux only. Hence for QNX, we need to rebuilt the SPL-UBOOT to include the “ipc_qnx_echo_testb_freertos_mcu1_0_release” image.

Below are the steps to do this:

  1. Build “ipc_qnx_echo_testb_freertos_mcu1_0_release” image.

cd ${PSDK_RTOS_PATH}/pdk_j721s2_08_00_03_XX/packages/ti/build
make -s ipc_qnx_echo_testb_freertos BOARD=j721s2_evm CORE=mcu1_0 -j2
  1. Copy the genreate mcu1_0 firmware image to the PSDK Linux path mentioned below and rebuild UBOOT.

cp ${PSDK_RTOS_PATH}/pdk_j721s2_08_00_03_XX/packages/ti/binary/ipc_qnx_echo_testb_freertos/bin/j721s2_evm/ipc_qnx_echo_testb_freertos_mcu1_0_release_strip.xer5f ${PSDK_LINUX_PATH}/board-support/prebuilt-images/ipc_echo_testb_mcu1_0_release_strip.xer5f
cd ${PSDK_LINUX_PATH}
make u-boot_clean
make u-boot
  1. Copy the newly generated UBOOT file to the SD card boot partiton

cd ${PSDK_LINUX_PATH}/board-support/u-boot_build/r5/tiboot3.bin ${BOOTFS}
cd ${PSDK_LINUX_PATH}/board-support/u-boot_build/a72/tispl.bin  ${BOOTFS}
cd ${PSDK_LINUX_PATH}/board-support/u-boot_build/a72/u-boot.img  ${BOOTFS}

After copying the firmware and booting the target, the ipc_test can be run from the command line (example output given below):

J7EVM@QNX:/# /sd/tibin/ipc_test
IPC_echo_test (core : mpu1_0) .....
responderFxn will stay active. Please use ctrl-c to exit the test when finished.
SendTask7: mpu1_0 <--> C7X_1, Ping- 10, pong - 10 completed
SendTask1: mpu1_0 <--> mcu1_0, Ping- 10, pong - 10 completed
SendTask6: mpu1_0 <--> mcu3_1, Ping- 10, pong - 10 completed
SendTask5: mpu1_0 <--> mcu3_0, Ping- 10, pong - 10 completed
SendTask3: mpu1_0 <--> mcu2_0, Ping- 10, pong - 10 completed
SendTask4: mpu1_0 <--> mcu2_1, Ping- 10, pong - 10 completed
SendTask7: mpu1_0 <--> C7X_2, Ping- 10, pong - 10 completed

Make sure that the tiipc-mgr is running before executing the ipc_test. Note that the test app will not exit. Press “ctrl+c” to exit

Note

If SPL-UBOOT boot flow is used, the ipc_test will not be able to communicate with mcu1_1. All other core will work. Note that mcu1_1 is not loaded with any firmware image.

Note

If SBL / BootApp boot flow is used, the ipc_test will not be able to communicate with mcu1_0, & mcu1_1. All other core will work.

Note

Refer PSDK RTOS Components for more information about each individual component.

5.4. UDMA Resource Manager

The UDMA resource manager (tiudma-mgr) provides support for multiple users to make use of the UDMA functionality without interfering with each other requests.

Note

Refer PSDK RTOS Components for more information about each individual component.

5.5. Shared Memory Allocator

The Shared Memory Allocator resource manager (shmemallocator) provides support for multiple users to allocate memory from the shared memory region. This shared memory region is carvedout of the QNX memory as part of the QNX Startup parameters.

5.6. CPSW2G DEVNP driver

5.6.1. Overview

The CPSW2G DEVNP network driver can be viewed as the “glue” between the underlying cpsw2g lowlevel driver, and the software infrastructure of io-pkt, the protocol stack above it. The “bottom half” of the driver is coded specifically to interact with the PDK’s cpsw & udma low-level drivers, and the “top half” of the driver is coded specifically for io-pkt.

Note

Refer PSDK RTOS Components for more information about each individual component.

Note

The cpsw2g driver’s CPTS interrupt thread must always be higher priority compared to the RX and TX threads of the driver. By default, the network stack thread is at priority 21. Hence the RX and TX thread are created at this priority level. The CPTS interrupt thread is create at priority 22. These priority values can be changed by providing them as command-line parameters. See driver use command.

5.6.2. Running

Boot the board with the SDcard. At the QNX prompt, run below, to mount the SD card and then launch the executable:

tisci-mgr
tiudma-mgr
io-pkt-v6-hc -d cpsw2g
dhclient -nw am0

The cpsw2g driver configures all the driver created threads to have the runmask as 0x2. This is to make sure all the threads run on both cores of A72. In case, the driver has to use a one of the cores only, please use the run_mask_cpu= command-line option.

For debug traces, run the below command before starting the DEVNP driver and start the driver with increased verbose parameter (ex: verbose=0x3ff) this will show all the drivers slog messages

slog2info –c
slog2info -w &

5.6.3. Additonal steps

  • Run “if_up -p am0” to check if the interface is ready

  • Run “ifconfig am0 up” to bring UP the link.

  • Run “dhclient -nw am0” for DHCP server provide the IP address

  • Run “ifconfig -v” to check the assigned IP address and status

  • Run “tcpdump -e” to look at the tcp traffic

5.6.4. Usage of devnp-cpsw2g.so

We can run the below command to get the usage of the DEVNP driver

$ use devnp-cpsw2g.so

devnp-cpsw2g.so j721s2 cpsw2g ethernet driver based on enet low level driver

Syntax:
  io-pkt-v6-hc -d cpsw2g [option[,option ...]] ...

Options (to override autodetected defaults):
  verbose=num             Set verbosity level (default: 0).
  mac-to-mac=1            Set for mac-to-mac mode (default: 0)
  speed=100|1000          Media data rate for port 0 in Mb/s. (default: 1000)
  p0mac=XXXXXXXXXXXX      Custom MAC address to use on port 0.
  ptp=0|1                 1 to enable PTP support (default: 0)
  promiscuous=0|1         1 to enable promiscuous mode (default: 0)
  typed_mem=name          Set the typed memory
  udma_chnum=val          Set the preferred udma channel to use (default: dynamic allocation)
  tx_freeq_threshold=val  Set the tx free Q threshold value (default: 120), must be less than no of TX descriptors.
  tx_descriptor_cnt=val   Set the tx descriptors count value (default: 128, Max: 256)
  rx_descriptor_cnt=val   Set the rx descriptors count value (default: 128, Max: 256)
  run_mask_cpu=val        Set the run mask - cpu core where threads are scheduled (default:2) (0 - core0, 1 - core1, 2 - both core)
  poll_phy_ms=val         Set the frequency in ms, to poll the phy status, and poll for management of resources (default: 2000)
  cache_ops=val           Set the cache operation to on/off (default:0  -> cache-coherency set), 1 - Turn on cache off -> cache-coherency off)
  smmu=0|1                1 to enable smmu support (default: 0)
  virt_id=val             Set the virt_id to use for the dma channel when smmu is enabled
  hw_csum=1               1 to enable hw csum (default: 0)
  joinvlan="1;2;3..."     List of VLANs to join
  rx_intr_prio=val        Set the rx interrupt thread priority (default: 21)
  tx_intr_prio=val        Set the tx interrupt thread priority (default: 21)
  cpts_intr_prio=val      Set the cpts interrupt thread priority (default: 22)
  no_stack_thread=val     1 to disable using the stack thread needed for bridge and fastforward to work  (default: 0)

Examples:
  # Start io-pkt using the driver:
  io-pkt-v6-hc -d cpsw2g
  ifconfig am0 192.0.2.1

  # Start io-pkt using the driver for mac-to-mac mode in gitbit speed
  io-pkt-v6-hc -d cpsw2g verbose=1,mac-to-mac=1,speed=1000
  ifconfig am0 192.0.2.1

  # Start io-pkt using the driver with custom mac address
  io-pkt-v6-hc -d cpsw2g p0mac=001122334455
  ifconfig am0 192.0.2.1

  # Start io-pkt using the driver with typed memory "ram":
  io-pkt-v6-hc -d cpsw2g typed_mem=ram -ptcpip pkt_typed_mem=ram
  ifconfig am0 192.0.2.1

  # Start io-pkt using the driver with typed memory "ram",preferred udma channel "24" and smmu enabled:
  io-pkt-v6-hc -d cpsw2g ptp=1,typed_mem=ram,udma_chnum=24,smmu=1 -ptcpip pkt_typed_mem=ram
  ifconfig am0 192.0.2.1

  # Start io-pkt using the driver with hw csum enabled
  io-pkt-v6-hc -d cpsw2g hw_csum=1
  ifconfig am0 tcp4csum udp4csum tcp6csum udp6csum
  ifconfig am0 192.0.2.1

5.6.5. Starting driver with other options

To run the cpsw2g devnp driver with full debug log (run “slog2info” to see the debug log):

io-pkt-v6-hc –d cpsw2g verbose=0xff

To run the cpsw2g devnp driver in mac-to-mac mode with 1Gbps:

io-pkt-v6-hc –d cpsw2g mac-to-mac=1,speed=1000

To run the cpsw2g devnp driver in mac-to-mac mode with 1Gbps with gPTP:

io-pkt-v6-hc –d cpsw2g ptp=1,mac-to-mac=1,speed=1000

To get a dynamic IP address for the cpsw2g port:

dhclient -nw am0

To get a static IP address for the cpsw2g port:

ifconfig am0 up
ifconfig am0 <static_ip_address>

To enabled HW CSUM offloading support:

io-pkt-v6-hc -d cpsw2g hw_csum=1
ifconfig am0 tcp4csum udp4csum tcp6csum udp6csum
dhclient -nw am0

5.7. K3conf QNX utility

K3CONF is a QNX port of a standalone application designed to provide a quick’n easy way to dynamically diagnose Texas Instruments’ K3 architecture based processors. K3CONF is intended to provide similar experience to that of OMAPCONF that runs on legacy TI platforms.

Note

WARNING: This is work in progress! Please don’t expect things to be complete in any dimension. Use at your own risk. And keep the reset button in reach.

To get more details on how to use k3conf utility, run below:

k3conf --help

5.8. VPU Video Codec

5.8.1. Overview

The WAVE5 Video Processing Unit (VPU) is a 4K Codec that supports both HEVC and H.264/AVC video formats. It provides high performance encode and decode capability for 8-bit YUV video up to 4K @60fps. The VPU is highly optimized for memory bandwidth loading and it has excellent power management.

Encoder:

  • Capable of encoding H.265/HEVC Main and Main Still Picture Profiles @ L5.1 High tier.

  • Capable of encoding H.264/AVC Baseline/Constrained Baseline/Main/High Profiles @ L5.2.

Decoder:

  • Capable of decoding H.265/HEVC Main and Main Still Picture Profiles @ L5.1 High tier.

  • Capable of decoding H.264/AVC Baseline/Constrained Baseline/Main/High Profiles @ L5.2.

Maximum Resolutions Supported:

  • Encoder Maximum resolution: 8192x8192

  • Decoder Maximum resolution: 8192x4320

    • Note: the VPU can handle the high resolutions, above, but frame-rate performance will be limited

Codec Constraints:

  • Encoder Minimum resolution: 256x128

  • H.265/HEVC Decoder Minimum resolution: 8x8

  • H.264/AVC Decoder Minimum resolution: 32x32

  • Picture width for encoding shall be a multiple of 8

  • Picture height for encoding shall be a multiple of 8

Multiple concurrent encode/decode streams:

  • Number of concurrent streams is dependent on the resolutions and frame rates required

5.8.2. Usage

An OMX IL Component for the IMG video encoder and a File-based OMX encoder test application is provided.

For more details, run the use command for: omxil_video_enc

$ use omxil_video_enc

This is a test application for OpenMAX IL video encode.
It takes input frames from a .yuv file and encodes them to a H.264 bitstream file.

Syntax:
    omxil_video_enc <options>

Options:
    -h: help
    -v: increase verbosity, max 7
    -n: stdin not used (no command-line inputs taken)
    -i: input file
    -o: output file
    -c: config file for encoder parameters
    -d: disable display
    -f input format for raw input (.yuv/.rgba/etc.)
       e.g.: nv12,1920x1080@30
             nv12 is the input color format
             1920x1080 is resolution(width x height)
             30 is frame rate.
  Supported input format: nv12.

Examples:
    # Basic built-in help:
    omxil_video_enc -h

    # AVC file-to-file encode:
    omxil_video_enc -vv -i /ti_fs/codec_test/vpu/nv12/8bit_BQTerrace_720x128_9frame_nv12.yuv -o /ti_fs/codec_test/vpu/output/8bit_BQTerrace_720x128.264 -d -f nv12,720x128@30

    # AVC file-to-file encode, with config file specified to override default bitrate, etc. :
    cp ti_fs/codec_test/vpu/nv12/mix_1920x1080_8b_10frm_nv12.yuv /tmp/
    omxil_video_enc -vv -i /tmp/mix_1920x1080_8b_10frm_nv12.yuv -c /ti_fs/codec_test/vpu/cfg/encoder_parameters.conf -o /tmp/mix_1920x1080.264 -d -f nv12,1920x1080@30

Also, a basic version of the VPU Encoder/Decoder driver is provided. It is built as a library. The library accompanies a set of unit-test applications which use file-to-file mode.

For more details, run the use command for: vpu_decoder_test, vpu_encoder_test and vpu_multi_inst_test.

$ use vpu_decoder_test

vpu_decoder_test - This is a VPU Decoder unit-test for file-to-file mode

Syntax:
    vpu_decoder_test <options>

Options (describes primary options, run with -h for more details)
    h           Help
    codec       Codec format (mandatory if using non HEVC encoded input files). Use 0 for AVC, and 12 for HEVC
    input       Input encoded file to decode (mandatory)
    output      Output decoded file (mandatory)

Examples:
    # Basic help built into the executable
    vpu_decoder_test -h

    # AVC file-to-file decode
    vpu_decoder_test --codec 0 --input /ti_fs/codec_test/bitstream/HistoryOfTI-480p.264 --output /ti_fs/codec_test/vpu/output/HistoryOfTI-480p.264-720x416.yuv

    # HEVC file-to-file decode
    vpu_decoder_test --input /ti_fs/codec_test/bitstream/TearOfSteel-Short-1280x720.265 --output /ti_fs/codec_test/vpu/output/TearOfSteel-Short-1280x720.265.yuv

Notes:
    - This test is applicable only on J721S2 SoCs
$ use vpu_encoder_test

vpu_encoder_test - This is a VPU Encoder unit-test for file-to-file mode

Syntax:
    vpu_encoder_test <options>

Options (describes primary options, run with -h for more details)
    h              Help
    cfgFileName    Encoder Config parameters (mandatory)
    codec          Codec format (mandatory if using non HEVC encoded input files). Use 0 for AVC, and 12 for HEVC
    input          Input YUV file to encode (optional). Overrides 'InputFile' in cfg file if defined
    output         Output encoded file (mandatory to store encoded binary into a file)

Examples:
    # Basic help built into the executable
    vpu_encoder_test -h

    # AVC file-to-file encode
    vpu_encoder_test --codec 0 --cfgFileName /ti_fs/codec_test/vpu/cfg/avc_inter_8b_02.cfg --output /ti_fs/codec_test/vpu/output/avc_inter_8b_02.cfg.264

    # HEVC file-to-file encode
    vpu_encoder_test --cfgFileName /ti_fs/codec_test/vpu/cfg/hevc_bg_8b_01.cfg --input /ti_fs/codec_test/vpu/yuv/8bit_BQTerrace_720x128_9frame.yuv --output /ti_fs/codec_test/vpu/output/bg_8b_01.cfg.265

Notes:
    - This test is applicable only on J721S2 SoCs
$ use vpu_multi_inst_test

vpu_multi_inst_test - This is a VPU Multi-instance Decode/Encode unit-test (file-to-file mode)

Syntax:
    vpu_multi_inst_test --instance-num=<N> -e <test-1>,..,<test-N> --codec=<codec-1>,..,<codec-N> --input <in-1>,..,<in-N> --output <out-1>,..,<out-N>

Options (describes primary options, run with -h for more details)
    h              Help
    instance-num   Total number of test instances to run
    e              0: decode, 1: encode (per test)
    codec          Codec format. Use 0 for AVC, and 12 for HEVC (per test)
    enable-wtl     Enables WTL option (per test), if set to 1, for decoded outputs to be written in linear fashion for a framebuffer
    input          Input bitstream for decode, or Input .cfg file for encode (per test)
    output         Output decoded YUV file, or Output encoded bitstream file (per test)

Examples:
    # Basic help built into the executable
    vpu_multi_inst_test -h

    # AVC decode + HEVC encode, and write the decoded output to a single YUV file
    vpu_multi_inst_test --instance-num=2 -e 0,1 --codec=0,12 --enable-wtl=1 \
    --input /ti_fs/codec_test/bitstream/HistoryOfTI-480p.264,/ti_fs/codec_test/vpu/cfg/hevc_bg_8b_01.cfg \
    --output /ti_fs/codec_test/vpu/output/HistoryOfTI-480p.264-720x416.yuv,/ti_fs/codec_test/vpu/output/bg_8b_01.cfg.265

Notes:
    - This test is applicable only on J721S2 SoCs