4.1. Release notes - 08_02_00¶
4.1.1. Documentation¶
The documentation included with the PSDK QNX J7200 is specific to the PSDK QNX J7200 package.
PSDK RTOS J7200 package documentation (PSDK RTOS Components) must also be referenced, for full understanding of PSDK QNX J7200 support.
4.1.2. PSDK QNX J7200 Features¶
Note
Reference PSDK RTOS J7200 package documentation (LINK) for an extensive list of new and current features supported by PSDK QNX + PSDK RTOS. This section lists only the features that are PSDK QNX J7200 specific.
Note
For features & drivers enabled by the QNX BSP, please refer to BSP Documentation or contact QNX.
4.1.2.1. Enabled in this Release¶
Features enabled in this release, specific to PSDK QNX J7200 addon package are:
Support for dynamic IP and MAC configuration support added to CPSW5G driver
Support and validaiton with the PSDK RTOS release
Bug fixes
For additional new updates, please refer PSDK RTOS package documentation (PSDK RTOS Components).
4.1.2.2. Enabled in Previous Releases¶
Features enabled in previous release, specific to PSDK QNX addon package are:
Single core multicast support added to CPSW5G driver
HW-checksum offloading support added to CPSW5G driver
HW-checksum offloading support added to CPSW2G driver
Shared Memory Allocator Resource Manager
SCI-Client Resource Manager
UDMA Resource Manager
IPC Resource Manager
A72 CPSW2G Devnp driver
A72 CPSW9G Virtual Devnp driver that interact with EthFW Switch running on Main R5
SBL Boot flow support for QNX
K3conf utility
For additional new updates, please refer PSDK RTOS package documentation (PSDK RTOS Components).
4.1.2.3. Change Requests¶
None
4.1.2.4. Errata¶
Please refer release note in the PSDK RTOS J7200 package documentation (PSDK RTOS Components) for the complete errata list.
4.1.3. Software Dependencies¶
4.1.3.1. QNX Dependency¶
Note
The PSDK QNX addon package is dependent on installations from QNX Software Center. The below QNX packages were used for PSDK QNX 08_02_00 build and verification.
4.1.3.1.1. QNX SDP 7.1¶
QNX SDP 710 Package |
Build ID |
Package ID |
Package Version |
---|---|---|---|
QNX® Software Development Platform 7.1 |
472 |
com.qnx.sdp710 |
7.1.0.00472T202006132107S |
QNX® SDP7.1 BSP for Texas Instruments Jacinto 7 J7200 (DRA821) Evaluation Modules |
6 |
com.qnx.qnx710.bsp.ti_j7200_evm |
0.0.3.00006T202104291808L |
4.1.3.2. PSDK RTOS Dependency¶
The PSDK QNX package is an addon package to the PSDK RTOS release, as such the PSDK RTOS is required.
4.1.3.3. PSDK LINUX Dependency¶
If SPL boot mode is to be supported, downloading the PSDK LINUX 08_02_00 package is recommended for access to the pre-built binaries.
4.1.4. Device Support and Validation Information¶
SoC |
Build Host (OS) |
Run Target (OS) |
Test Platform |
---|---|---|---|
J7200 |
x86_64 (Linux Ubuntu 18.04) |
R5Fs running TI-RTOS A72 running QNX |
TI EVM with daughter cards |
PC emulation mode |
x86_64 (Linux Ubuntu 18.04) |
x86_64 (Linux Ubuntu 18.04) |
x86_64 (Linux Ubuntu 18.04) |
Note
Refer EVM Setup for J7200 for more details on the TI EVM support.
4.1.5. Known Issues¶
A list of key known issues with the PSDK QNX release is provided below.
Note
Refer to individual PSDK RTOS Components release notes for known issues in each component
Index |
Module |
Description |
---|---|---|
1 |
QNX BSP OSPI driver |
For SBL xSPI boot mode, the QNX OSPI flash driver is not loading properly. Suspect OSPI flash not getting re-initialized after SBL usage. |
2 |
QNX BSP SD driver |
For SBL xSPI boot mode, the QNX SD driver is encountering a segmentation fault. Suspect SD driver is not enabling power & clocks for MMCSD IP. |
4.1.6. Additional Reports¶
For additional reports like test report, traceability refer PSDK RTOS Additional Reports