14.10. Release notes version 08.05.00

14.10.1. New in this Release

  • Added DL-Inferer GStreamer plugin which can be called from gst-launch command

  • Added DL-postproc GStreamer plugin which handles text overlay, drawing boxes, lines etc. natively in NV12 format

  • Added perfOverlay GStreamer plugin which overlays CPU load, HWA load, DDR bandwidth on the post-processed image

  • Added multi platform support which detects underlying platform at runtime

  • Added split-output support in edgeai-gst-apps to channel post-processed output to both encode and display

  • DL-Inferer component in edgeai-gst-apps is migrated to separate repo supporting TFLite RT, ONNX-RT and NeoAI-DLR

14.10.2. Fixed in this Release

  • EDGEAI_ROBOTICS-818 - TVM Models when used with file input does not exit cleanly

  • EDGEAI_ROBOTICS-814 - addr[0] is INVALID error reported by edgeai-gst-apps infrequently

  • EDGEAI_ROBOTICS-730 - Performance Visualization Tool command typo/error

  • EDGEAI_ROBOTICS-666 - No valid frames found before end of stream for image file input and video file output

  • EDGEAI_ROBOTICS-639 - tiovx mosaic plugin throws error if the pixel ratio of input videos is different

  • EDGEAI_ROBOTICS-335 - Issue with running setup script on HOST due to ldconfig

14.10.3. Known Issues

  • EDGEAI_ROBOTICS-820 - Video container formats of .mp4 and .mov fails while writing in Docker

  • EDGEAI_ROBOTICS-819 - tiovxisp element infrequently throws error while exiting edgeai-gst-apps

  • EDGEAI_ROBOTICS-648 - tiovxdlcolorconvert fails when the image height/2 is not an even number

  • EDGEAI_ROBOTICS-642 - Mosaic element hangs when both instances of MSC are used in multi-input multi-inference usecase

  • EDGEAI_ROBOTICS-640 - LDC introduces image format while working with 1936 x 1096 resolution

14.10.4. Model Zoo

Models from edgeai-modelzoo are regressed with multiple input sources such as camera and video files. A list of unsupported models are as below,

  • Height/2 is odd, tiovxdlpreproc block fetch logic fails
    • TFL-CL-0100-efficientNet-edgeTPU-m

    • TFL-CL-0140-efficientNet-lite4

    • TFL-CL-0170-efficientNet-lite1

    • TFL-CL-0190-efficientNet-edgeTPU-l

  • High latency causes DSS underflow
    • ONR-SS-8730-deeplabv3-mobv3-lite-large-cocoseg21-512x512

  • Odd resolution, tiovxdlcolorconvert fails
    • TVM-CL-3430-gluoncv-mxnet-xception

    • TFL-CL-0040-InceptionNetV3

  • Human pose model with unsupported post processing
    • ONR-KD-7000-human-pose-ae-mobv2-fpn-spp-udp-512x512

    • ONR-KD-7010-human-pose-ae-res50v2-fpn-spp-udp-512x512

    • ONR-KD-7020-human-pose-ae-mobv2-pan-spp-udp-512x512

    • ONR-KD-7030-human-pose-ae-res50v2-pan-spp-udp-512x512

Note

Please also refer to edgeai-gst-plugins issues for more details on bugs filed on custom GStreamer plugins

14.10.5. Software components

List of software components used in this version

Componenet

Version

PSDKLA (filesystem, uboot)

08.05.00.08

PSDKRA (firmware)

08.05.00.11

Docker

19.03.8-ce

Ubuntu (Docker)

20.04.LTS

Python

3.8

OpenCV

4.1.0

GStreamer

1.16.3

Cmake

3.16.5

Ninja

1.10.0

Meson

0.53.2

Jupyterlab

3.0.14

NeoAI - DLR

1.10.0

Tensorflow

TIDL_PSDK_8.5

TFLite-runtime

TIDL_PSDK_8.5

ONNX-runtime

TIDL_PSDK_8.5

PyYAML

5.3.1

TI Model Zoo

8.5.0

edgeai-gst-plugins

0.8.0

edgeai-tiovx-modules

8.5

edgeai-dl-inferer

8.5

edgeai-tidl-tools

08_05_00_11