14.11. Release notes version 08.04.00

14.11.1. New in this Release

  • SDK comes pre-installed with required dependencies and demo applications

  • Enable zero-copy in between GStreamer and runtimes

  • Support DMABUF import for v4l2 raw camera sources using tiovxisp element

  • Cross compile support for all EdgeAI repos

  • Support for separately enabling or disabling DL runtime

  • Support for streaming the demo output over the network

  • Added scripts to report stats on core loading and GStreamer pipeline

  • Support for SDE and DOF GStreamer plugins

14.11.2. Fixed in this Release

  • ADASVISION-5635 - tiovxisp output is wrong with dmabuf-import when sensor resolution is not multiple of 64

  • ADASVISION-5584 - Edge AI demo: Image classification demo freezes around 98~99 frames

  • ADASVISION-5583 - Edge AI demo: file input in multi-output demo causes demo to freeze

  • ADASVISION-5494 - Add support for simultaneous use of RPi camera and Rpi extension header

  • ADASVISION-5475 - J7 SK: The setup_script.sh fails when the board is configured in AP mode, which is the default with WiFi only case

  • ADASVISION-5463 - ONR-OD-8000 model fails with IMX390 in CPP app due to 1200x1200 resolution

  • ADASVISION-5349 - Setup script fails building without internet connection

  • ADASVISION-4997 - Multi-input multi-inference demo freezes after long duration run

14.11.3. Known Issues

  • ADASVISION-5643 - Mosaic hangs in edge ai apps multi-input multi-inference when run with both instances of MSC

  • ADASVISION-5631 - tiovx mosaic doesn’t work if the pixel ratio of input videos is different

  • ADASVISION-5447 - Models failing due to tiovxdlcolorconvert limitation

  • ADASVISION-5420 - No valid frames found before end of stream Image Input -> Video File Write

14.11.4. Model Zoo

About 83 models from 8.4 model zoo are regressed with multiple input sources such as camera and video files. A list of unsupported models are as below,

  • Height/2 is odd, tiovxdlpreproc block fetch logic fails
    • TFL-CL-0100-efficientNet-edgeTPU-m

    • TFL-CL-0140-efficientNet-lite4

    • TFL-CL-0170-efficientNet-lite1

    • TFL-CL-0190-efficientNet-edgeTPU-l

  • High latency causes DSS underflow
    • ONR-SS-8730-deeplabv3-mobv3-lite-large-cocoseg21-512x512

  • Odd resolution, tiovxdlcolorconvert fails
    • TVM-CL-3430-gluoncv-mxnet-xception

    • TFL-CL-0040-InceptionNetV3

  • Human pose model with unsupported post processing
    • ONR-KD-7000-human-pose-ae-mobv2-fpn-spp-udp-512x512

    • ONR-KD-7010-human-pose-ae-res50v2-fpn-spp-udp-512x512

    • ONR-KD-7020-human-pose-ae-mobv2-pan-spp-udp-512x512

    • ONR-KD-7030-human-pose-ae-res50v2-pan-spp-udp-512x512

Note

Please also refer to edgeai-gst-plugins issues for more details on bugs filed on custom GStreamer plugins

14.11.5. Software components

List of software components used in this version

Componenet

Version

PSDKLA (filesystem, uboot)

08.04.00.11

PSDKRA (firmware)

08.04.00.06

Docker

19.03.8-ce

Ubuntu (Docker)

20.04.LTS

Python

3.8

OpenCV

4.5.1

GStreamer

1.16.2

Cmake

3.16.3

Ninja

1.10.0

Meson

0.57.2

Jupyterlab

3.0.14

NeoAI - DLR

1.8.0

Tensorflow

TIDL_PSDK_8.4

TFLite-runtime

TIDL_PSDK_8.4

ONNX-runtime

TIDL_PSDK_8.4

PyYAML

5.4.1

TI Model Zoo

8.4.0

edgeai-gst-plugins

0.7.1

edgeai-tiovx-modules

8.4.1

edgeai-tidl-tools

8.4.0.2