5.1.6. SDK File System Optimization/Customization

The purpose of this article is to explain the file system that is delivered as part of the Processor SDK Linux SK TDA4VM and how this file system can be modified to customize it for your use case. The tools discussed in this article are installed by default in the Processor SDK Linux SK TDA4VM file system for your convenience.

There are different filesystem tarball provided in the SDK. Refer Foundational_Components/Filesystems for more details. All of these filesystems contain the opkg package manager and can be used as a starting point for system optimization as discussed in the next sections.

5.1.6.1. The Basics of OPKG

5.1.6.1.1. List all available options of opkg

opkg is the package manager used in the SDK file system to install and remove packages. You can get a list of the full commands supported by opkg by running the following command on the target device:

root@<machine>:~# opkg

To check the version of opkg packaged in filesystem,

root@<machine>:~# opkg --version
opkg version 0.6.3 (libsolv 0.7.28)

5.1.6.1.2. Show all installed packages

To the list of packages are part of the file system and the version of each package you can run the following command on the target device:

root@<machine>:~# opkg list-installed

Important

This list only contains information about packages that were installed using the package manager. Applications that were built and copied to the file system and not installed as a .ipk package are not tracked by opkg

5.1.6.1.3. Show package contents

Sometimes it is useful to know what files a package has installed. To do this you can use the following command:

root@<machine>:~# opkg files <pkgname>

Where <pkgname> is the name of the package as given in the opkg list-installed output. This command will produce a list of all the files on the file system that belong to the given package.

5.1.6.1.4. Find a file owner

Sometimes you may find a file on the target file system that you want to remove, or just know where it came from. In this case you can use the following command:

root@<machine>:~# opkg search <file>

This command will find which package installed the given file. This may be useful later when you want to remove an particular file because this command can help you find the package to remove.

5.1.6.1.5. Show packages which require the package as dependency

Sometimes when you want to remove a package it is useful to find out what other packages depend on the package you are removing. While the opkg remove command will tell you the immediate dependencies you can find the longer list of dependencies using:

root@<machine>:~# opkg whatdepends <pkgname>

This command will print the list of packages the depend on the package you entered, as well as the packages that depend on those packages, and so forth.

5.1.6.1.6. Removing Packages or Deinstallation

One of the simplest ways to modify the contents of the file system is to use the opkg utility to remove packages (or install if you have pre-built packages). Removing a package is often as simple as:

root@<machine>:~# opkg remove <pkgname>

However, sometimes a package is a DEPENDENCY of another package. In this case you have the following options:

  • Use the --force-depends option

    • This option will force the removal of the package but will leave any packages that depend on this package installed. This can be useful in the case that you want to remove a particular package, but that package is depended on by some other package that you do not want removed.

  • Use the --force-removal-of-dependent-packages option

    • This option will go up the dependency list and remove all packages in the dependency chain. You should check all the packages being removed to make sure they are indeed packages you want to remove and do not contain other files you want.

  • Remove the individual packages that depend on this package first

    • This way you can control exactly which dependent packages are removed and which are left in place.

root@<machine>:~# opkg remove --force-removal-of-dependent-packages <pkgname>

Tip

opkg will print the packages that depend on the package being removed. It is usually a good idea to use the opkg files command for the packages that depend on the one being removed so that you can make sure that no files you really want to keep are going to be removed.

Tip

You can also use the whatdepends option discussed above to see the dependency list for a package

By using the opkg remove command in conjunction with the commands for listing packages, finding file owners, and listing package contents, you can quickly strip down a full file system into something smaller and more optimized for your use case. However, once a package is removed it cannot currently be re-installed without generating the .ipk file to install it.

5.1.6.1.7. Install local packages

In most cases installing additional applications can be as simple as copying the the binary executable to the file system. However, if you have built your own .ipk packages you can use opkg to install those ipks into the target file system.

One major advantage of using the package manager is the ability to track the package and it’s content with the opkg package manager. More details about how to build & install your own packages is available at Building the SDK with Yocto

To learn about Arago project, please visit Arago/TI-SDK distribution.