3.2.2.8. HyperBus and HyperFlash¶
3.2.2.8.1. Introduction¶
HyperBus is Low Signal Count, High Performance Double Data Rate (DDR) Bus interface between a host system master and one or more slave interfaces. Its a 8-bit data bus (DQ[7:0]) with Read-Write Data Strobe (RWDS) signal and either Single-ended clock(3.0V parts) or Differential clock (1.8V parts). It uses ChipSelect lines to select b/w multiple slaves. At bus level, it follows a separate protocol described in HyperBus specification.
HyperFlash is a NOR flash based device storage over HyperBus. HyperFlash follows CFI AMD/Fujitsu Extended Command Set (0x0002) similar to that of existing parallel NORs. Since Hyperbus is x8 DDR bus, its equivalent to x16 parallel NOR flash wrt bits per clk. But Hyperbus operates at much higher frequencies.
HyperFlash on TI’s J7 EVM is connected to HyperBus Memory Controller that supports memory mapped IO access to flash. HyperFlash is supported under kernel’s MTD framework.
Supported Devices
J7200 EVM
Note
On J7200 EVM, switch SW3.1 should be in ON position at the time of powering on the board to access HyperFlash.
3.2.2.8.2. Driver Architecture¶
Following diagram shows the HyperBus and HyperFlash driver stack:
![../../../../_images/hbmc-linux-arch.png](../../../../_images/hbmc-linux-arch.png)
Source Location
The source file for the HyperBus controller driver can be found at: drivers/mtd/hyperbus/hbmc-am654.c under Linux Kernel source tree.
HyperFlash command set is implementation is at: drivers/mtd/chips/cfi_cmdset0002.c
3.2.2.8.2.1. Kernel Configuration Options¶
The driver can be built into the kernel or can be compiled as module and loaded into the kernel dynamically.
Enabling HyperBus driver
Following configs are to be enabled for HyperBus and HyperFlash.
Note
HyperBus driver and their dependencies are enabled by default in the SDK images. So this section can be skipped in that case.
Start the Linux Kernel Configuration tool:
$ make menuconfig ARCH=arm64
Device Drivers --->
<*> Memory Technology Device (MTD) support --->
<*> HyperBus support --->
<*> HyperBus controller driver for AM65x SoC
Enabling UBIFS filesystem support:
File systems --->
[*] Miscellaneous filesystems --->
<*> UBIFS file system support
3.2.2.8.2.2. DT Configuration¶
Refer to Documentation/devicetree/bindings/mtd/ti,am654-hbmc.txt kernel source tree for HyperBus and HyperFlash documentation driver’s DT bindings and their usage. Example DT entry:
fss: system-controller@47000000 {
compatible = "syscon", "simple-mfd";
reg = <0x0 0x47000000 0x0 0x100>;
#address-cells = <2>;
#size-cells = <2>;
ranges;
hbmc_mux: hbmc-mux {
compatible = "mmio-mux";
#mux-control-cells = <1>;
mux-reg-masks = <0x4 0x2>; /* HBMC select */
};
hbmc: hyperbus@47034000 {
compatible = "ti,am654-hbmc";
reg = <0x0 0x47034000 0x0 0x100>,
<0x5 0x00000000 0x1 0x0000000>;
power-domains = <&k3_pds 102 TI_SCI_PD_EXCLUSIVE>;
clocks = <&k3_clks 102 0>;
assigned-clocks = <&k3_clks 102 5>;
assigned-clock-rates = <333333333>;
#address-cells = <2>;
#size-cells = <1>;
mux-controls = <&hbmc_mux 0>;
};
};
&hbmc {
pinctrl-names = "default";
pinctrl-0 = <&mcu_fss0_hpb0_pins_default>;
ranges = <0x0 0x0 0x5 0x00000000 0x4000000>, /* 64MB Flash on CS0 */
<0x1 0x0 0x5 0x04000000 0x800000>; /* 8MB RAM on CS1 */
flash@0,0 {
compatible = "cypress,hyperflash", "cfi-flash";
reg = <0x0 0x0 0x4000000>;
};
};
3.2.2.8.2.3. Driver Usage¶
HyperFlash is exposed to userspace as MTD character devices and /dev/mtdX (X = 0, 1, 2) entries are created for every partition defined in DT or via command line arguments. MTD abstracts all types of flashes and, To see all MTD partitions in the system run:
$cat /proc/mtd
Here is example for DT partitioning. Example for passing cmdline partition from U-Boot.
3.2.2.8.2.4. Testing¶
Since, HyperFlash is supported under MTD framework, usage is same as SPI NOR flashes such as OSPI/QSPI. HyperFlash also supports UBIFS as filesystem format. Note that, it is necessary to define at least one cmdline or DT partition to use UBIFS.
Refer to QSPI section for more testing.
Note
Currently, Linux has no support for HyperRAM.