3.2.2.14. PCIe Backplane

Introduction

PCIe backplane allows multiple hosts with RC ports to communicate and share data with each other.

../../../../../_images/j7-linux-pcie-backplane.png

PCIe backplane is implemented using multiple instances of multi-function endpoint controller. Each host should be connected to a separate endpoint controller instance and each host will enumerate the other host as an independent function.

PCIe uses NTB (non transparent bridge) for two hosts to communicate with each other. Though J721E doesn’t have an explicit NTB controller, NTB functionality can be achieved using multiple endpoint controller instances. And for PCIe backplane (to connect more than 2 hosts), aggregation of NTB controllers can be modeled using multiple instances of multi-function endpoint controller.

In the below diagram, PCI NTB function configures the SoC with multiple PCIe Endpoint (EP) instances in such a way that transaction from one EP controller is routed to the other EP controller. Once PCI NTB function configures the SoC with multiple EP instances, HOST1 and HOST2 can communicate with each other using SoC as a bridge.

   +-------------+                                   +-------------+
   |             |                                   |             |
   |    HOST1    |                                   |    HOST2    |
   |             |                                   |             |
   +------^------+                                   +------^------+
          |                                                 |
          |                                                 |
+---------|-------------------------------------------------|---------+
|  +------v------+                                   +------v------+  |
|  |             |                                   |             |  |
|  |     EP      |                                   |     EP      |  |
|  | CONTROLLER1 |                                   | CONTROLLER2 |  |
|  |             <----------------------------------->             |  |
|  |             |                                   |             |  |
|  |             |                                   |             |  |
|  |             |  SoC With Multiple EP Instances   |             |  |
|  |             |  (Configured using NTB Function)  |             |  |
|  +-------------+                                   +-------------+  |
+---------------------------------------------------------------------+

NTB SW Architecture

The SW architecture for NTB both on the host side and EP side is given below. The top half is the host side NTB architecture, and the bottom half is the endpoint side NTB architecture.

../../../../../_images/ntb_sw_architecture.png

Backplane Setup

The following picture shows J721E EVM connected to two DRA7 EVMs. Here the two DRA7x boards communicate with each other using J721E as backplane.

../../../../../_images/j7-backplane.jpg

Backplane Configuration

Backplane DTS Overlay File

The following DTS overlay file configures the PCIe controller in EP mode and also contains a device tree node to create a NTB function device:

arch/arm64/boot/dts/ti/k3-j721e-pcie-backplane.dtso

In order to apply the dts overlay file, the following command should be given in u-boot prompt:

#setenv name_overlays k3-j721e-pcie-backplane.dtbo

EP Side Configuration (J721E Backplane)

8.x SDK (5.10 Kernel)

The following set of steps is required only for 5.10 Kernel

Creating pci-epf-ntb device

PCI endpoint function device can be created using the configfs. To create pci-epf-ntb device, the following commands can be used:

# mount -t configfs none /sys/kernel/config
# cd /sys/kernel/config/pci_ep/
# mkdir functions/pci_epf_ntb/func1

The “mkdir func1” above creates the pci-epf-ntb function device that will be probed by pci_epf_ntb driver.

The PCI endpoint framework populates the directory with the following configurable fields

# ls functions/pci_epf_ntb/func1
baseclass_code    deviceid          msi_interrupts    pci-epf-ntb.0
progif_code       secondary         subsys_id         vendorid
cache_line_size   interrupt_pin     msix_interrupts   primary
revid             subclass_code     subsys_vendor_id

The PCI endpoint function driver populates these entries with default values when the device is bound to the driver. The pci-epf-ntb driver populates vendorid with 0xffff and interrupt_pin with 0x0001

# cat functions/pci_epf_ntb/func1/vendorid
0xffff
# cat functions/pci_epf_ntb/func1/interrupt_pin
0x0001

Configuring pci-epf-ntb Device

The user can configure the pci-epf-ntb device using its configfs entry. In order to change the vendorid and the deviceid, the following commands can be used

# echo 0x104c > functions/pci_epf_ntb/func1/vendorid
# echo 0xb00d > functions/pci_epf_ntb/func1/deviceid

In order to configure NTB specific attributes, a new sub-directory to func1 should be created

# mkdir functions/pci_epf_ntb/func1/pci_epf_ntb.0/

The NTB function driver will populate this directory with various attributes that can be configured by the user

# ls functions/pci_epf_ntb/func1/pci_epf_ntb.0/
db_count    mw1         mw2         mw3         mw4         num_mws
spad_count

A sample configuration for NTB function is given below

# echo 4 > functions/pci_epf_ntb/func1/pci_epf_ntb.0/db_count
# echo 128 > functions/pci_epf_ntb/func1/pci_epf_ntb.0/spad_count
# echo 2 > functions/pci_epf_ntb/func1/pci_epf_ntb.0/num_mws
# echo 0x100000 > functions/pci_epf_ntb/func1/pci_epf_ntb.0/mw1
# echo 0x100000 > functions/pci_epf_ntb/func1/pci_epf_ntb.0/mw2

Binding pci-epf-ntb Device to EP Controller

NTB function device should be attached to two PCI endpoint controllers connected to the two hosts. Use the ‘primary’ and ‘secondary’ entries inside NTB function device to attach one PCI endpoint controller to primary interface and the other PCI endpoint controller to the secondary interface

# ln -s controllers/2900000.pcie-ep/ functions/pci-epf-ntb/func1/primary
# ln -s controllers/2910000.pcie-ep/ functions/pci-epf-ntb/func1/secondary

Once the above step is completed, both the PCI endpoint controllers are ready to establish a link with the host.

Start the Link: 7.x and 8.x SDK (5.4 and 5.10 Kernel)

In order for the endpoint device to establish a link with the host, the _start_ field should be populated with ‘1’. For NTB, both the PCI endpoint controllers should establish link with the host

# echo 1 > controllers/2900000.pcie-ep/start
# echo 1 > controllers/2910000.pcie-ep/start

(PCIe2 can also be configured for NTB, but that is not tested yet).

RC Side Configuration

The hosts that have to communicate with each other can be bought up in any order after EP has been brought up. Once the host boots up, the below steps have to be done in each of the hosts.

Since the same vendor ID and device ID are used for multiple function drivers (pci-endpoint-test and ntb_hw_epf), the device should be first ubound from existing driver.

echo 0000:01:00.0 > /sys/bus/pci/devices/0000\:01\:00.0/driver/unbind

After unbinding from existing driver, it should be bound to ntb_hw_epf driver.

echo 0000:01:00.0 > /sys/bus/pci/drivers/ntb_hw_epf/bind

Then bind one of the NTB application driver. Here ntb_netdev is bound to emulate ethernet over PCIe. This will create a new ethernet interface for each of the hosts.

modprobe ntb_transport
modprobe ntb_netdev

Kernel Configs

EP Side (J721E Backplane)

CONFIG_PCI_ENDPOINT=y
CONFIG_PCI_ENDPOINT_CONFIGFS=y
CONFIG_PCI_EPF_NTB=y
CONFIG_PCI_J721E=y
CONFIG_PCIE_CADENCE=y
CONFIG_PCIE_CADENCE_EP=y

Host Side

CONFIG_PCI=y
CONFIG_PCI_MSI=y
CONFIG_NTB=m
CONFIG_NTB_EPF=m
CONFIG_NTB_TRANSPORT=m
CONFIG_NTB_NETDEV=m
RC controller configs

Additional Information

For additional information, please refer to:

<Processor_SDK_install_dir>/board-support/linux-[ver]/Documentation/PCI/endpoint/pci-test-ntb.txt