3.2.2.22. UBIFS
Introduction
Unsorted Block Image File System is a file system specifically designed for flash memory devices. It’s built on top of the UBI layer, which handles low-level flash management tasks like wear-leveling and bad block management by dividing it into Logical Erase Blocks (LEBs).
Using UBIFS on flash
Flash devices can be divided into multiple partitions, including a rootfs partition dedicated for the root file system. The rootfs partition can be formatted with the UBIFS and the volume can be mounted as the root file system during boot.
Required Software for UBI image creation
Building a UBI File System requires two applications, ubinize and
mkfs.ubifs. Both are both provided by mtd-utils package.
$ sudo apt-get install mtd-utils
Building a UBI File System image
Step 1
Create a directory containing the root file system. It is important that the
directory size is smaller than the rootfs partition in the flash. Users can
download the default/tiny image for specific SoC.
Note
Download and extract tisdk-default-image-*-evm.rootfs.tar.xz for
QSPI/OSPI/GPMC NAND.
Download and extract tisdk-tiny-image-*-evm.rootfs.tar.xz for QSPI/OSPI
NOR.
The rootfs partition information
OSPI NOR
# EVM Linux $ mtdinfo /dev/mtd5 mtd5 Name: ospi.rootfs Type: nor Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 223 (58458112 bytes, 55.7 MiB) Minimum input/output unit size: 16 bytes Sub-page size: 16 bytes Character device major/minor: 90:10 Bad blocks are allowed: false Device is writable: trueOSPI NAND
# EVM Linux $ mtdinfo /dev/mtd5 mtd5 Name: ospi_nand.rootfs Type: nand Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 383 (100401152 bytes, 95.7 MiB) Minimum input/output unit size: 4096 bytes Sub-page size: 4096 bytes OOB size: 128 bytes Character device major/minor: 90:10 Bad blocks are allowed: true Device is writable: trueGPMC NAND
# EVM Linux $ mtdinfo /dev/mtd7 mtd7 Name: NAND.file-system Type: nand Eraseblock size: 262144 bytes, 256.0 KiB Amount of eraseblocks: 4054 (1062731776 bytes, 1013.5 MiB) Minimum input/output unit size: 4096 bytes Sub-page size: 1024 bytes OOB size: 256 bytes Character device major/minor: 90:14 Bad blocks are allowed: true Device is writable: true
Step 2
Create a file named ubinize.cfg and add the contents below. Note that
this configuration file can be outside the root directory.
[ubifs]
mode=ubi
image=rootfs.ubifs
vol_id=0
vol_type=dynamic
vol_name=rootfs
vol_flags=autoresize
Step 3
mkfs.ubifs is used to create UBI File System image, which is specifically generated for a flash memory device, like Serial NOR, NAND and Parallel NAND.
Syntax
mkfs.ubifs -r <root_dir> -o <output_image> [options]
Some key options to use:
-m <min_io_size>: specifies the minimum I/O size (in bytes) of the flash device.The 'Minimum input/output unit size' value in mtdinfo.
-e <leb_size>: specifies the logical eraseblock (LEB) size, which is the usable portion of an eraseblock in UBI.Logical Erase Block size = Physical Erase block size - UBI overhead Here, a. Physical Erase block size is the 'Eraseblock size' value in mtdinfo. b. UBI overhead = ALIGN((VID Header offset + sizeof(struct ubi_vid_hdr)), Minimum input/output unit size) Here, -> ALIGN(x,a) expands to (((x) + ((a) - 1)) & ~((a) - 1)) -> sizeof(struct ubi_vid_hdr) is 64 -> Minimum input/output unit size is the 'Minimum input/output unit size' value in mtdinfoFor VID Header offset, refer 4th option, here.
-c <max_leb>: specifies the maximum number of logical eraseblocks (LEBs) the filesystem can use.The 'Amount of eraseblocks' value in mtdinfo.
-x <compression>: specifies the compression method to use. Default is ‘zlib’.-F: used to force the filesystem to “fixup” all the free space which it is going to use. Note, this flag makes the first mount very slow, because the “free space fixup” procedure takes time.
For more details:
mkfs.ubifs --help
Step 4
ubinize is used to create UBI image for one or more UBIFS images.
ubinize [options] -o <output_image> <configuration_file>
Some key options to use:
-m <min_io_size>: specifies the minimum I/O size (in bytes) of the flash device.The 'Minimum input/output unit size' value in mtdinfo.
-p <peb_size>: specifies the physical eraseblock size, which is the total size of an eraseblock in the flash device.The 'Eraseblock size' value in mtdinfo.
-s <sub_page_size>: specifies the sub-page size. Usually equivalent to the minimum I/O size.The 'Sub-page size' value in mtdinfo.
-O <vid_hdr_offset>: specifies the offset of the VID (Volume Identifier) header within the physical eraseblock.VID Header offset = ALIGN((sizeof(struct ubi_ec_hdr)), Headers Minimum input/output unit size) Here, a. ALIGN(x,a) expands to (((x) + ((a) - 1)) & ~((a) - 1)) b. sizeof(struct ubi_ec_hdr) is 64 c. Headers Minimum input/output unit size = Minimum input/output unit size >> Sub Page shift Here, -> Minimum input/output unit size is the 'Minimum input/output unit size' value in mtdinfo -> Sub Page shift is zero for Serial flashes and [0,2] for Parallel flashes
For more details:
ubinize --help
Example:
To generate .ubifs image
$ mkfs.ubifs -r /path/to/directory -o rootfs.ubifs <MKUBIFS ARGS>
To generate .ubi image
$ ubinize -o rootfs.ubi <UBINIZE ARGS> ubinize.cfg
For GPMC NAND:
To generate .ubifs image
$ mkfs.ubifs -r /path/to/directory -o rootfs.ubifs <MKUBIFS ARGS>To generate .ubi image
$ ubinize -o rootfs.ubi <UBINIZE ARGS> ubinize.cfg
Board Name
MKUBIFS Args
UBINIZE Args
AM335X GP EVM
-F -m 2048 -e 126976 -c 5600
-m 2048 -p 128KiB -s 512 -O 2048
AM437x GP EVM
-F -m 4096 -e 253952 -c 2650
-m 4096 -p 256KiB -s 4096 -O 4096
K2E EVM
-F -m 2048 -e 126976 -c 3856
-m 2048 -p 128KiB -s 2048 -O 2048
K2L EVM
-F -m 4096 -e 253952 -c 1926
-m 4096 -p 256KiB -s 4096 -O 4096
K2G EVM
-F -m 4096 -e 253952 -c 1926
-m 4096 -p 256KiB -s 4096 -O 4096
DRA71x EVM
-F -m 2048 -e 126976 -c 8192
-m 2048 -p 128KiB -s 512 -O 2048
AM64 GP EVM
-F -m 4096 -e 258048 -c 3970
-m 4096 -p 256KiB -s 1024 -O 1024
AM62 LP SK
-F -m 4096 -e 258048 -c 3970
-m 4096 -p 256KiB -s 1024 -O 1024
Table: Table of Parameters to use for Building UBI filesystem image
Step 5
Flash rootfs.ubi to rootfs partition
# EVM Linux
$ ubiformat -f rootfs.ubi /dev/mtdX