3.1.2.11. DDR

3.1.2.11.1. Overview

The DDR subsystem (DDRSS) comprises DDR controller, DDR PHY and wrapper logic to integrate these blocks in the device. The K3 DDRSS driver (drivers/ram/k3-ddrss/k3-ddrss.c) runs during the R5 SPL stage and is responsible for initializing and configuring the DDR subsystem.

3.1.2.11.2. DDR Initialization

The driver utilizes an auto-generated configuration file containing the necessary settings for the DDR. It configures the frequency, timing parameters, training algorithms etc. for DDR initialization. The configuration DTSI can be generated using the Sysconfig tool and selecting the software product as “DDR Configuration for *” as well as the required device.

3.1.2.11.3. DDR Temperature Monitoring

For enabling temperature polling in the DDR subsystem, the configuration DTSI (see DDR Initialization) must be regenerated after selecting ‘Yes’ for LPDDR > DDRSS x > Enable DRAM Temperature Polling and also changing the DRAM Timing Parameters as prompted by the tool.

The kernel DDR driver utilizes this polling feature to provide base support for dynamic DDR refresh rate changes (see Using the DDR Temperature Monitoring)

3.1.2.11.4. Inline ECC

Note

Inline ECC is currently not tested and supported for J721E and J7200

For SDRAM data integrity, the DDRSS bridge supports inline ECC on the data written to or read from the SDRAM. ECC is stored together with the data so that a dedicated SDRAM device for ECC is not required. The 8-bit single error correction double error detection (SECDED) ECC data is calculated over 64-bit data quanta. For every 256-byte data block 32 bytes of ECC is stored inline. Thus, 1/9th of the total SDRAM space is used for ECC storage and the remaining 8/9th of the SDRAM data space are seen as consecutive byte addresses. Even if there are non-ECC protected regions the previously described 1/9th-8/9th rule still applies and consecutive byte addresses are seen from system point of view. J721E supports up to 3 ECC protected non-overlapping memory ranges. The current U-Boot release supports a single region covering the entire SDRAM space.

ECC is calculated for all accesses that are within the address ranges protected by it. 1-bit error is correctable by ECC, but multi-bit and multiple 1-bit errors are not correctable and will be treated as an uncorrectable error. Any uncorrectable error will cause a bus abort.

3.1.2.11.4.1. ECC Handling

Note

The inline ECC feature of DDRSS is not enabled by default in U-Boot.

3.1.2.11.4.1.1. Enabling inline ECC

The inline ECC feature of DDRSS can be enabled by adding the CONFIG_K3_INLINE_ECC config to the R5 defconfig:

# u-boot/configs/*_r5_defconfig

CONFIG_PINCTRL_SINGLE=y
CONFIG_POWER_DOMAIN=y
CONFIG_TI_POWER_DOMAIN=y
CONFIG_K3_INLINE_ECC=y
CONFIG_K3_SYSTEM_CONTROLLER=y
CONFIG_REMOTEPROC_TI_K3_ARM64=y
CONFIG_RESET_TI_SCI=y

This enables inline ECC for the entire region of the DDR.

3.1.2.11.4.1.2. Priming with BIST Engine

The bootloader has the responsibility to pre-load the ECC protected region with known data before functional reads and writes are performed. During the ECC initialization, the R5 SPL fills the entire memory with zeros using the BIST engine in the DDR controller. The BIST engine method allows priming the entire region with zeros in much less time.

3.1.2.11.4.1.3. Enabling inline ECC for a partial region of the DDR

Instead of defaulting to enable inline ECC for the entire DDR region, a partial range can also be selected.

In this case, the DDRSS driver expects such a node within the memory node, in the absence of which it resorts to enabling for the entire DDR region:

inline_ecc: protected@9e780000 {
   device_type = "ecc";
   reg = <0x9e780000 0x0080000>;
   bootph-all;
};