3.2.2.20. DM TIMER
This guide covers a general overview on DM Timer, it supports DM Timers found on TI’s Jacinto 7 SoC.
Each timer comes with dedicated pins that can be used as timer capture inputs or as timer PWM outputs, please check the device TRM for more information.
Each timer contains a free-running upward counter with autoreload capability on overflow. Each timer includes compare logic to allow an interrupt event on a programmable counter matching value. A dedicated output signal can be pulsed/toggled on an overflow or a match event. This offers time-stamp trigger signaling or PWM signal sources. A dedicated input signal can be used to trigger an automatic timer counter capture or an interrupt event on a programmable input signal transition.
For more detailed information on timers, please refer to the:
Peripherals/Timer Modules/Timerssection of the device specific TRM.
3.2.2.20.1. Driver Sources
Driver source location:
drivers/clocksource/ti,timer-dm.cBinding source location:
Documentation/device-tree/bindings/timer/ti,timer-dm.yaml
Enabling PWM output signals:
Driver source location:
drivers/pwm/pwm-omap-dmtimer.cBinding source location:
Documentation/devicetree/bindings/pwm/pwm-omap-dmtimer.txt
3.2.2.20.2. Kernel Configuration
Configs to be enabled in Linux Kernel:
Enabling PWM output signals:
DTS node for DM Timer
In this example, we take am62x SK DT node as an example. In general all the timer nodes should be described in its appropriate voltage domain .dtsi file, for example the following node can be found in k3-am62-main.dtsi:
main_timer3: timer@2430000 {
compatible = "ti,am654-timer";
reg = <0x00 0x2430000 0x00 0x400>;
interrupts = <GIC_SPI 123 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&k3_clks 39 2>;
clock-names = "fck";
assigned-clocks = <&k3_clks 39 2>;
assigned-clock-parents = <&k3_clks 39 3>;
power-domains = <&k3_pds 39 TI_SCI_PD_EXCLUSIVE>;
ti,timer-pwm;
};
Enabling PWM output signals:
The “ti,timer-pwm” DT attribute is required in the DM Timer node in order to enable PWM output signals.
An additional DT node is required in order to enable PWM output signals as shown below. The
main_timer3_pins_default is also required and not listed here, use sysconfig tool to get
pinumux configuration.
main_pwm3: dmtimer-main-pwm-3 {
compatible = "ti,omap-dmtimer-pwm";
#pwm-cells = <3>;
ti,timers = <&main_timer3>;
pinctrl-names = "default";
pinctrl-0 = <&main_timer3_pins_default>;
};
3.2.2.20.3. Driver Usage
For information on using DM timer as a counter, please refer to the detailed descriptions
in the TRM Timers Functional Description and Low-Level Programming Models under
Peripherals/Timers Modules/Timers.
Note
Currently there is no sysfs interface to interact with the DM Timer as a counter via userspace.
Timers in “Timer” mode should be enabled by default in Linux DT.
Enabling PWM output signals:
If the PWM node exists in DT using a DM TIMER, the PWM device is probed and exposed as a
PWM device by Linux Kernel to be used by userspace in /sys/class/pwm.
For controlling the PWM chip via sysfs interface please refer to the official Linux documentation: here or go to Using-PWM-with-sysfs.
3.2.2.20.4. Examples
To enable DM timer PWM output signals, there is an example DT overlay found in
arch/arm64/boot/dts/ti/k3-am62x-sk-dmtimer-pwm.dtso that applies for am62x
family devices and can be referenced for other K3 devices.