3.6.6. OpenGL ES

The OpenGL|reg| ES and EGL|reg| libraries are packaged with the Processor SDK Linux J721e and are used by graphics stacks such as Wayland/Weston. The drivers run on an ARM core and programs the firmware running inside a GPU core with rendering commands submitted by the user applications.

For more information about OpenGL|reg| ES and EGL|reg| extensions see: