1.2. Processor SDK RTOS
Processor SDK RTOS is a companion SDK to Processor SDK Linux on the Jacinto 7 family of devices. In order to use some SoC features from the core running Linux, one needs to download and install the PSDK RTOS package.
Refer to the PSDK RTOS top level user guide online or after downloading the installer at ${PSDK_RTOS_PATH}/index.html, for more details.
Features provided by PSDK RTOS that can be accessed from Linux A72 core on Jacinto 7 family of devices are listed below:
TIDL on C7x
Vision pre/post processing functions on C6x
Vision HW accelerators (VPAC/DMPAC) on R5F
CSI2RX on R5F
Remote display on R5F
Ethernet switch on R5F
MCU/AutoSAR MCAL on R5F
OpenVX on Linux A72 and RTOS C6x, C7x, R5F
Deep learning demos on Linux A72
Surround view demos on Linux A72
Important
This package is NOT included in PSDK Linux installer and needs to be downloaded separately.