2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) for Linux provides a fundamental software platform for development, deployment and execution of Linux based applications and includes the following:
- Bootloaders, Linux Kernel & Filesystem
- SDK installer
- Setup scripts
- Demo applications
- Documentation
Note
For building some of the RTOS-based demonstrations, you should also download Processor SDK RTOS installer. For more information, refer to <PSDKRA install path>/index.html.
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below. In addition, see Processor SDK Linux GPLv3 Disclaimer.
2.1.3. Documentation¶
- Processor SDK Linux Software Developer’s Guide: Provides information on features, functions, delivery package and, compile tools for the Processor SDK Linux release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Processor SDK Linux Getting Started Guide: Provides information on getting the software and running examples/demonstrations bundled in the SDK.
- Software Manifest: Provides license information on software
included in the SDK release. This document is in the release at
[INSTALL-DIR]/docs. - EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Supported Platforms¶
See here for a list of supported platforms and links to more information.
2.1.5. Release 08.05.00¶
Released December 2022
What’s New
Processor SDK 8.5 Release supports the following platforms:
- J721E
- J7200
- J721S2
- J784S4
Processor SDK 8.5 Release has following new features:
- Adds support for the J784S4 device family
- JPEG Decode support on J721E
- Authentication of firmware
- Proper support for poweroff command
- McSPI slave support
- J7AEP stability progress (mostly Graphics)
2.1.6. Build Information¶
2.1.6.1. U-Boot¶
2.1.6.2. Kernel¶
Linux Kernel
Real Time (RT) Linux Kernel
Note:
2.1.6.3. Yocto¶
meta-ti
meta-arago
meta-psdkla
2.1.7. Issues Tracker¶
2.1.7.1. Issues opened in previous releases that were closed on this release¶
| Record ID | Title | Platform |
|---|---|---|
| LCPD-28510 | VDEC: Decoder gives cmalloc errors | j721e-idk-gw |
| LCPD-28625 | J7AHP: Add the missing UART instances clock/dev data | j784s4-evm |
| LCPD-28243 | core-image-minimal build fails for j7200-evm with rm_work enabled | j7200-evm |
| LCPD-28108 | J7200: cadence-mhdp-fw recipe should be machine dependent on j721e-evm only | j7200-evm |
| LCPD-28509 | WAVE5: MultiStream Decode/Encode > 2 channel fails | j721s2-evm,j784s4-evm |
| LCPD-28256 | Wave5: H264/265 Encoded file produces extra green garbage data on width | j721s2-evm |
| LCPD-28255 | Wave5: Decode fails for Dynamic resolution change in input stream | j721s2-evm |
| LCPD-28254 | Wave5: Decode deosnot work for videotestsrc with pattern source | j721s2-evm |
| LCPD-25332 | J721e Failing Video test | j721e-idk-gw |
| LCPD-28325 | kernel crashes if CONFIG_DEBUG_FS is not set | am62xx-hsevm,am62xx-sk,am64xx-evm,am64xx-hsevm,am64xx-sk,am654x-evm,am654x-idk,am654x-hsevm,j7am-evm,j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j721s2-evm,j721s2-hsevm,j7200-evm,j7200-hsevm |
| LCPD-24142 | J721e: Issue with OSPI probe in kernel when booting from OSPI boot mode | j721e-evm,j721e-hsevm,j721e-idk-gw |
| LCPD-28387 | J721e/J7200/J721s2: Add the missing UART instances clock/dev data | j721e-evm,j721s2-evm,j7200-evm |
| LCPD-28349 | j721s2-evm: no support in k3conf | j721s2-evm |
| LCPD-28246 | J7200/J7VCL: Linux crash when we cat pinctrl debugfs node | j7200-evm |
| LCPD-26728 | J721e: Watchdog reset fails on newer SoMs | j721e-idk-gw,j721e-sk |
| LCPD-25670 | tisdk-tiny-image does not boot for J721S2/J784S4 | j721s2-evm,j784s4-evm |
| LCPD-25317 | A72 SPL: A72 SPL memcpy sluggish with 8.0/8.1 SDK | j721e-idk-gw |
| LCPD-25075 | J721E: revE8 SoM board doesn’t boot consistently | j721e-idk-gw |
| LCPD-28502 | MMC I/O latency is causing audio UNDERRUN issues | j721e-idk-gw |
| LCPD-24125 | j721e-idk-gw all LE play + record tests fail (Impact 7.0) | j721e-idk-gw |
| LCPD-16911 | Linux performance guide: Crypto benchmark numbers: fix unit and accompanying description | j721e-evm,j721e-idk-gw |
| LCPD-28259 | Wave5: V4l2 driver Multi stream support | j721s2-evm |
| LCPD-28257 | Wave5: Video looping does not work with H264/265 Decoder | j721s2-evm |
| LCPD-28465 | Automated test failure - KICKSYNC SYNCCONTEXTLOOP failed due to change in command line arguments | j721s2-evm,j721s2-hsevm |
| LCPD-16366 | RGX kick test fails when 32 sync dependencies are set for each command | j721e-evm,j721e-evm-ivi,j721e-idk-gw |
| LCPD-28403 | SDK: Crypto node cleanup across TI SOCs | am64xx-evm,am654x-evm,j721e-evm,j721s2-evm,j7200-evm,j784s4-evm |
| LCPD-27948 | TSN: PTP test fails with J7200 in switch mode (acting as a transparent clock) | j7200-evm |
| LCPD-25564 | J721s2-evm: CPSW2g: interface goes up and down sporadically | am62xx-sk,j721s2-evm |
| LCPD-25469 | j721e USB OTG HOST regressions on eptf126 | j721e-idk-gw |
| LCPD-24677 | j721e-idk-gw PCI WIFI Tests Fail due to iperf issues(Impact 1) | am62xx-sk,j721e-idk-gw |
| LCPD-28206 | j721: sdhci0: Capabilities offered in U-Boot Vs Kernel dts are different | j721e-idk-gw |
| LCPD-24511 | ARM: A72/53 L1 data cache and L2 cache set counts wrong | am64xx-evm,am64xx-hsevm,am64xx-sk,j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j7200-evm,j7200-hsevm |
| LCPD-22861 | Missing documentation for HS devices | j721e-hsevm |
| LCPD-28258 | Wave5: Kernel crash during encode usecase | j721s2-evm |
2.1.7.2. Issues found and closed on this release that may be applicable to prior releases¶
| Record ID | Title | Platform |
|---|---|---|
| LCPD-29625 | j721e hangs during boot after IPC tests reconfigures firmware | j721e-idk-gw |
| LCPD-28795 | J7AHP : xSPI boot enable DMA | j784s4-evm |
| LCPD-28663 | Pauses in video being displayed when input video is read from SD card | j721e-idk-gw |
| LCPD-29696 | SERDES driver not being probed in U-Boot | j721e-evm,j7200-evm |
| LCPD-29302 | J721S2: CSI2RX: stream broken with update in DPHY Common module reset logic | j721s2-evm |
| LCPD-28927 | J7200: MCSPI: Data mismatch between the master & slave(J7200) when cpu is heavily loaded | j7200-evm |
| LCPD-28889 | j721s2: GPIO Interrupts are broken | j721s2-evm |
| LCPD-29639 | DSS tests failing due to FPS mismatch | j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j721e-sk |
| LCPD-28762 | GLMark2 visual errors around fragmentation shader tests | am62xx-hsevm,am62xx-sk,j721e-evm,j721e-hsevm,j721s2-evm,j721s2-hsevm,j784s4-evm,j784s4-hsevm |
| LCPD-29732 | SDK: MDIO: DaVinci driver probe incorrectly deferred | j784s4-evm,j784s4-hsevm |
| LCPD-29477 | j721e-idk-gw PCI WIFI Tests Fail due to iperf issues(Impact 1) | am62xx-sk,j721e-idk-gw |
| LCPD-29419 | J721s2-evm: u-boot: CPSW2g: interface goes up and down sporadically | am62xx-sk,j721s2-evm |
| LCPD-28756 | J7AHP - Enable ultra high speed mode for SDIO/MMC | j784s4-evm |
| LCPD-29534 | kernels in arago-dunfell RT directory are not an RT-Kernels | am62xx-hsevm,am62xx-lp-sk,am62xx-sk,am64xx-sk,j721e-evm,j721e-hsevm,j721s2-evm,j721s2-hsevm,j7200-evm,j7200-hsevm,j784s4-evm,j784s4-hsevm |
| LCPD-29524 | j721: sdhci0: Capabilities offered in U-Boot Vs Kernel dts are different | j721e-idk-gw |
| LCPD-29284 | Fix ti,sci-inta, ti,sci-intr and mmc dtbs_check | am62xx-sk,am64xx-evm,j721e-idk-gw,j721s2-evm |
| LCPD-28765 | J7200: U-boot R5 SPL build triggers warning due to duplicate config definitions | j7200-evm |
2.1.7.3. Errata Workarounds Available in this Release¶
| Record ID | Platform | Title |
|---|---|---|
| LCPD-19965 | am64xx-evm,am654x-idk,j721e-idk-gw,j7200-evm | OSPI PHY Controller Bug Affecting Read Transactions |
| LCPD-19047 | j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw | USB: Race condition while reading TRB from system memory in device mode |
| LCPD-17220 | j721e-idk-gw | U-Boot Hyperbus: Hyperflash reads limited to 125MHz max. frequency |
| LCPD-16605 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | MMC: MMC1/2 Speed Issue |
| LCPD-22544 | j7200-evm | DDR: LPDDR4 should be configured to 2666 MT/S |
| LCPD-19068 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | DSS: Disabling a layer connected to Overlay may result in synclost during the next frame |
2.1.7.4. U-Boot Known Issues¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-29402 | am64xx-evm,j7200-evm | tftp download in U-Boot fails on am64xx-evm1@eptf124 | |
| LCPD-25263 | j721s2-evm | j721s2-evm: U-Boot USBHOST: Superspeed test is failing | |
| LCPD-22512 | j721e-evm,j7200-evm | Update dfu_alt_info_ospi to include flashing of PHY tuning data | |
| LCPD-17789 | j721e-idk-gw | UBOOT J7: Could not see UFS device by scsi scan | |
| LCPD-24824 | j7200-evm | J7200/VCL: u-boot SPL code configuring the SOC DDR PLL (PLL12) incorrectly. Desired boot frequency is 27.5 MHz | |
| LCPD-22904 | j721e-idk-gw,j7200-evm | U-boot: Update EMIFtool for i2244:DDR: Valid stop value must be defined for write DQ VREF training | |
| LCPD-17523 | j721e-evm,j721e-idk-gw,j7200-evm | A72-SPL - Support to dump EEPROM to shared memory | |
| LCPD-29743 | j721e-evm,j721s2-evm,j7200-evm | u-boot ums does not work stably | |
| LCPD-24108 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | U-Boot: TISCI config ring fail traces seen in OSPI boot mode on J721E | |
| LCPD-29852 | j784s4-evm | j784s4-evm: SD card not recognized in U-Boot when booting over UART |
2.1.7.5. Linux Known Issues¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-29636 | j784s4-evm | TDA4VH: multi thread mutex usage causes kernel crash | |
| LCPD-28142 | am62xx-sk,j784s4-evm | Automated performance testing - spec2k6 benchmark test broken | |
| LCPD-28317 | j721e-evm,j721e-hsevm | GStreamer pipeline with decoder and fakesink causes kernel crash | |
| LCPD-27522 | j721e-idk-gw | Multi Stream decode fails | |
| LCPD-25598 | j721s2-evm | Wave5: Dynamic SRAM configuration in upstream driver | |
| LCPD-29521 | j721e-evm,j784s4-evm | R5 remote proc load does’nt guarentee CPU0 vs CPU1 sequencing | |
| LCPD-28791 | j784s4-evm,j784s4-hsevm | AHP GFX performance regression compaired to AEP | |
| LCPD-28511 | j721e-evm,j721e-hsevm,j721s2-evm,j721s2-hsevm,j784s4-evm,j784s4-hsevm | GPU cache coherency issues | |
| LCPD-24589 | am335x-evm,am57xx-evm,j721e-idk-gw | no new usb reported on host after g_multi | |
| LCPD-19497 | j7200-evm | J7200: CPSW2g: interface goes up and down sporadically | Seen only on very few EVMs. No workaround. |
| LCPD-17814 | j721e-idk-gw | Kingston 16G card could not boot to uboot prompt | |
| LCPD-29737 | j7200-evm | J7200: Watchdog reset test fails | |
| LCPD-29714 | j721e-idk-gw | iperf hangs during crypto performance testing | |
| LCPD-29705 | j7200-evm | J7200: DT compile time warnings | |
| LCPD-29554 | j721e-idk-gw,j7200-evm | EEPROM Header Unidentified Board | |
| LCPD-29525 | j7200-evm,j7200-hsevm | Documentation for MCAN missing in the SDK | |
| LCPD-28645 | j721e-idk-gw | k3conf wrong frequencies | |
| LCPD-29599 | j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm | Stream_1 benchmark executable missing | |
| LCPD-24720 | j721e-idk-gw | Order 4 SR1.1 j721e-idk-boards and replace SR1.0 boards in the farm | |
| LCPD-24686 | j721e-idk-gw | j721e-idk-gw: ETH-CPSW2G test fail due to wrong return code | |
| LCPD-24648 | am335x-evm,am572x-idk,am64xx-evm,dra71x-evm,j721e-evm,j7200-evm | Move dma-heaps-test and ion-tests to TI repositories | |
| LCPD-24629 | j721e-idk-gw | j721e-idk-gw Weston Keyboard Test Capability Gap NR (Impact 1) | |
| LCPD-24597 | j721e-idk-gw | j721e-idk-gw PCI_PERF tests report bad numbers (Impact 2) | |
| LCPD-20331 | am64xx-evm,am64xx-sk,j7200-evm | Farm: j7200-evm/k3-am642-evm/k3-am642-sk DT blob has to be passed manually | |
| LCPD-17398 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | J7 Beta board hangs and cannot power cycle via automation interface | |
| LCPD-16909 | dra7xx-evm,j721e-evm,j721e-idk-gw | Linux performance guide: CPU load is not captured, incorrect throughput numbers for ethernet | |
| LCPD-24619 | j721e-idk-gw | Bitbake fails in different timezone | |
| LCPD-29721 | j721e-evm,j721e-idk-gw | SDK: Linux: Kernel crashes with Intel PCIe WiFi Card | |
| LCPD-29680 | j721e-evm,j721e-evm-ivi,j721e-idk-gw,j7200-evm | vxe_enc_probe warning observed while booting with debug options enabled | |
| LCPD-29634 | j721s2-evm | Need to include codec maximum capabilities in SDK documentation | |
| LCPD-29320 | j721e-idk-gw | The H.264 profile in the IMG video encoder driver is hardcoded to Base profile. | |
| LCPD-25619 | j721s2-evm | Wave5: Encoded output, mplayer warnings | |
| LCPD-24475 | j721e-idk-gw | Performance of H.265 decoder is poor | |
| LCPD-17138 | j721e-idk-gw | Kernel warning reported during h264 video encode operations | |
| LCPD-28946 | j721e-evm,j7200-evm | remoteproc hangs during booting sporadically | |
| LCPD-25322 | j7200-evm | Docs: J7200: Improve the IPC chapter for ti-rpmsg-char | |
| LCPD-25321 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | Docs: J721E: Improve the IPC chapter for ti-rpmsg-char | |
| LCPD-24456 | am335x-evm,am335x-hsevm,am335x-ice,am335x-sk,am43xx-epos,am43xx-gpevm,am43xx-hsevm,am437x-idk,am437x-sk,am571x-idk,am572x-idk,am574x-idk,am574x-hsidk,am57xx-evm,am57xx-beagle-x15,am57xx-hsevm,am62axx-sk,am62xx-hsevm,am62xx-sk,am62xx-vlab,am62xx-zebu,am64xx-evm,am64xx-hsevm,am64xx-sk,am654x-evm,am654x-idk,am654x-hsevm,beaglebone,bbai,beaglebone-black,dra71x-evm,dra71x-hsevm,dra72x-evm,dra72x-hsevm,dra76x-evm,dra76x-hsevm,dra7xx-evm,dra7xx-hsevm,j7ae-evm,j7ae-zebu,j7aep-zebu,j7am-evm,j7am-vlab,j7am-zebu,j7amp-vlab,j7amp-zebu,j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j721e-sk,j721e-vlab,j721s2-evm,j721s2-hsevm,j7200-evm,j7200-hsevm,j7amp-evm,k2e-evm,k2e-hsevm,k2g-evm,k2g-hsevm,k2g-ice,k2hk-evm,k2hk-hsevm,k2l-evm,k2l-hsevm,omapl138-lcdk | Move IPC validation source from github to git.ti.com | |
| LCPD-17284 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | remoteproc/k3-r5: Cores are started out-of-order when core 0 file size >> core 1 file size | |
| LCPD-16545 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | remoteproc/k3-r5f: PDK IPC echo_test image fails to boot up in remoteproc mode on second run | |
| LCPD-16535 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | remoteproc/k3-dsp: PDK IPC echo test binaries fails to do IPC in remoteproc mode on second run | |
| LCPD-25662 | am62xx-sk,j721e-evm,j7200-evm | Remove SGX PVR tools from KS3 devices | |
| LCPD-25221 | j721e-idk-gw |
|
|
| LCPD-22972 | j721e-idk-gw | j721e-idk-gw GLBenchmark GLB25_EgyptTestStandardOffscreen_inherited test | |
| LCPD-22921 | j721e-idk-gw | j721e PVR profiling with PVRPerfServer test is failing | |
| LCPD-19894 | j721e-idk-gw,j721s2-evm,j784s4-evm | UYVY texture test fails due to internal data stream error | |
| LCPD-19716 | j721e-idk-gw | GFX_XS_FUNC_UYVY_TEXTURE test fails | |
| LCPD-24127 | am654x-evm,j721e-idk-gw | AM654x IPSEC Software Crypto tests fail (Impact 4) | |
| LCPD-28485 | j7200-evm | j7200: Segmentation fault during reload PCIe driver. | |
| LCPD-28433 | j721s2-evm | PCIe EP: DMA test fail | |
| LCPD-28087 | j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw | emmc: using RPMB panicks the TA on High speed mode | |
| LCPD-25304 | j721s2-evm | J7AEP: USB: USB 3.0 devices not getting enumerated in high speed | |
| LCPD-25112 | am64xx-evm,j721e-idk-gw | Ethernet driver not gating its clock when interface is down | |
| LCPD-24798 | am654x-evm,am654x-idk,j721e-idk-gw,j7200-evm | j721e-idk-gw, j7200-evm UART tests fail (Impact 3.0) | |
| LCPD-24725 | j721e-idk-gw | PCIE RC Link fails when linux prints are made quiet | |
| LCPD-24690 | am62xx-sk,am64xx-evm,am64xx-sk,j721s2-evm,j7200-evm | Kernel: SDK: Set HIGH_SPEED_EN for MMC1 instance | |
| LCPD-24595 | am64xx-evm,am64xx-sk,j721e-idk-gw,j721e-sk,j7200-evm | j721e-idk-gw USB Suspend/Resume with RTC Wakeup fail (Impact 1) | |
| LCPD-24491 | j721e-evm,j721e-evm-ivi,j721e-idk-gw,j7200-evm | Docs: MMC/SD supported modes not documented properly for J721E/J7200 | |
| LCPD-22905 | am654x-evm,j721e-idk-gw | UDMA: TR15 hangs if ICNT0 is less than 64 bytes | |
| LCPD-22413 | j7200-evm | Hyperflash tests fail ~50% of the time on j7200 | |
| LCPD-20240 | j721e-idk-gw,j721e-sk | MMC Modular testcase regression | |
| LCPD-19659 | j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j7200-evm,j7200-hsevm | Doc: PCIe: Update documentation to indicate how to move to compliance mode | |
| LCPD-19499 | j7200-evm,j7200-hsevm | Kernel: OSPI write throughput is less than 1MB/s | |
| LCPD-19084 | j721e-idk-gw | Few SD cards not enumerating in Kernel with Alpha EVM | |
| LCPD-17794 | j721e-idk-gw | ext4write failed to write firmware to SD card | |
| LCPD-17421 | j721e-idk-gw | CPSW9G: Can’t bring up interface over NFS | |
| LCPD-17172 | j721e-idk-gw | Uboot USBhost: Sandisk Extreme USB 3.0 msc stick could not be detected at second time | |
| LCPD-17171 | j721e-idk-gw | Uboot dhcp occasionally failed | |
| LCPD-17113 | j721e-idk-gw | [Cpsw9g][VirtualDriver][VirtualMAC] rpmsg_kdrv_switch is not autoloaded | |
| LCPD-16640 | j721e-idk-gw | PCIe RC: GIC ITS misbehaves when more than 4 devices use it simultaneously | |
| LCPD-16396 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | J721E: RC: Unsupported request in configuration completion packets results in an abort | Workaround for Multifunction: Configure all the physical functions supported by the endpoint. For configuring all the 6 functions of PCIe controller instance ‘1’ in J721E, the following can be used. mount -t configfs none /sys/kernel/config; cd /sys/kernel/config/pci_ep/; mkdir functions/pci_epf_test/func1; echo 0x104c > functions/pci_epf_test/func1/vendorid; echo 0xb00d > functions/pci_epf_test/func1/deviceid; echo 1 > functions/pci_epf_test/func1/msi_interrupts; echo 16 > functions/pci_epf_test/func1/msix_interrupts; ln -s functions/pci_epf_test/func1 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func2; echo 0x104c > functions/pci_epf_test/func2/vendorid; echo 0xb00d > functions/pci_epf_test/func2/deviceid; echo 1 > functions/pci_epf_test/func2/msi_interrupts; echo 16 > functions/pci_epf_test/func2/msix_interrupts; ln -s functions/pci_epf_test/func2 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func3; echo 0x104c > functions/pci_epf_test/func3/vendorid; echo 0xb00d > functions/pci_epf_test/func3/deviceid; echo 1 > functions/pci_epf_test/func3/msi_interrupts; echo 16 > functions/pci_epf_test/func3/msix_interrupts; ln -s functions/pci_epf_test/func3 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func4; echo 0x104c > functions/pci_epf_test/func4/vendorid; echo 0xb00d > functions/pci_epf_test/func4/deviceid; echo 1 > functions/pci_epf_test/func4/msi_interrupts; echo 16 > functions/pci_epf_test/func4/msix_interrupts; ln -s functions/pci_epf_test/func4 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func5; echo 0x104c > functions/pci_epf_test/func5/vendorid; echo 0xb00d > functions/pci_epf_test/func5/deviceid; echo 1 > functions/pci_epf_test/func5/msi_interrupts; echo 16 > functions/pci_epf_test/func5/msix_interrupts; ln -s functions/pci_epf_test/func5 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func6; echo 0x104c > functions/pci_epf_test/func6/vendorid; echo 0xb00d > functions/pci_epf_test/func6/deviceid; echo 1 > functions/pci_epf_test/func6/msi_interrupts; echo 16 > functions/pci_epf_test/func6/msix_interrupts; ln -s functions/pci_epf_test/func6 controllers/d800000.pcie-ep/; echo 1 > controllers/d800000.pcie-ep/start; echo 1 > /sys/bus/pci/devices/0000:00:00.0/remove; echo 1 > /sys/bus/pci/rescan; Workaround for switch card: No workarounds available. |
| LCPD-16031 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | J721e: PCIe: Legacy interrupts do not work | |
| LCPD-29740 | j721e-idk-gw | j721e-idk-gw: EMMC_DD_RW_500M test fail | |
| LCPD-29729 | j721e-idk-gw,j7200-evm | j721e-idk-gw, j7200-evm MMC_M_MODULAR_SDHC_MULTI tests fail | |
| LCPD-29648 | j7200-evm | Failure logs during boot: Failed unmounting /var/lib & /var/volatile | |
| LCPD-29647 | j7200-evm | Non-fatal failure logs seen during system boot up | |
| LCPD-29646 | am62xx-sk,j721e-idk-gw | Failure logs during boot: Failed to get MSI domain | |
| LCPD-29645 | j784s4-evm | MMC: SD Card doesn’t go into SDR104 mode | |
| LCPD-29644 | j784s4-evm | MMC: SD Card doesn’t go into DDR50 mode | |
| LCPD-29528 | am62xx-sk,am64xx-evm,am64xx-hsevm,am64xx-sk,am64xx-hssk,j721e-idk-gw,j721s2-evm,j721s2-hsevm,j7200-evm,j7200-hsevm,j784s4-evm | k3: integration: sdk: missing tag info for optee and atf projects | |
| LCPD-28861 | j721e-evm,j7200-evm | J721e/j7200: MCU/WKUP UART as console. The output gets garbled after sysfw/dm load | |
| LCPD-28250 | j721s2-evm | J7AEP: QSPI Write corrupted when the first operation after powerup is erase | |
| LCPD-25692 | j721s2-evm,j721s2-hsevm | linux needs to identify J7ES PG1.1 correctly | |
| LCPD-25686 | j721s2-evm,j721s2-hsevm | k3conf needs to identify J7ES PG1.1 correctly | |
| LCPD-25262 | j721s2-evm | j721s2-evm : cpuhotplug06 fails | |
| LCPD-25195 | j721s2-evm | j721s2-evm: audio device is not found | |
| LCPD-23010 | j721e-idk-gw | j721e-idk-gw stress boot test files | |
| LCPD-22715 | j721e-idk-gw,j7200-evm,j721s2-evm,am62xx-evm | i2232: DDR: Controller postpones more than allowed refreshes after frequency change | Workaround 1: Disable dynamic frequency change by programing DFS_ENABLE = 0
Workaround 2: If switching frequency, program the register field values as follows: if (old_freq/new_freq >= 7) {
if (PBR_EN==1) { // Per-bank refresh is enabled
AREF_HIGH_THRESHOLD = 19
AREF_NORM_THRESHOLD = 18
AREF_PBR_CONT_EN_THRESHOLD = 1
AREF_CMD_MAX_PER_TREF = 8
}
else { // Per-bank refresh is disabled
AREF_HIGH_THRESHOLD = 18
AREF_NORM_THRESHOLD = 17
AREF_CMD_MAX_PER_TREF = 8
}
} else {
AREF_HIGH_THRESHOLD = 21
AREF_CMD_MAX_PER_TREF = 8
}
|
| LCPD-22319 | am64xx-evm,j7200-evm | OpenSSL performance test data out of bounds | |
| LCPD-20653 | am335x-evm,am43xx-gpevm,am654x-idk,j721e-idk-gw | ltp: kernel syscall tests fail | |
| LCPD-19792 | j721e-idk-gw | j721e boot fails sometimes due to EL1 exception | |
| LCPD-18860 | am654x-evm,am654x-idk,j721e-idk-gw,j7200-evm | isolcpus in the command line is not honored | |
| LCPD-18684 | am57xx-evm,am654x-evm,j721e-idk-gw | syscalls sync failures: fdatasync03, fsync04, sync03, syncfs01, sync_file_range02 | |
| LCPD-18258 | am654x-evm,j721e-idk-gw | IPSEC perfomance failures | |
| LCPD-17798 | am654x-evm,am654x-idk,j7am-evm,j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j721e-vlab,j7200-evm,j7200-hsevm | 2020 LTS: INTA/INTR smp_affinity failure and IRQ allocation issues. | |
| LCPD-17543 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | Some cpuhotplug tests failed | |
| LCPD-24502 | j721e-evm-ivi,j721e-idk-gw | j721e-evm-ivi Universal Planes fails (Impact 1) | |
| LCPD-19068 | j721e-evm,j721e-evm-ivi,j721e-idk-gw | DSS: Disabling a layer connected to Overlay may result in synclost during the next frame | |
| LCPD-17017 | j721e-evm-ivi,j721e-idk-gw | J7: DSS underflows seen on various use cases | |
| LCPD-25583 | j721e-idk-gw | H264 Encode followed by decode not working for all resolutions in Gstreamer | |
| LCPD-16531 | j721e-idk-gw | video decode: vxd_dec warnings displayed at end of gstreamer hevc playback to kmssink for certain video | |
| LCPD-25663 | am62xx-sk,j721e-evm,j721s2-evm,j784s4-evm | Remove old IMG demo binaries | |
| LCPD-22513 | j721e-evm,j7200-evm | Update SDK doc to include OSPI flashing instruction using dfu-util | |
| LCPD-18790 | j721e-idk-gw | eMMC tests failed on J7 rev E2 EVM | |
| LCPD-29755 | j721e-idk-gw | j721e-idk-gw : Can Transmission and Reception Tests Fail | |
| LCPD-29596 | j721e-idk-gw | J721E: USBHOST: All boot attempts failed | |
| LCPD-19743 | j7200-evm,j7200-hsevm | Packages.gz is missing | |
| LCPD-19739 | am654x-idk,j7200-evm | AM65 shutdown error | |
| LCPD-29781 | j721s2-evm | CPU is hitting 100% when using gst-launch for both encode and decode | |
| LCPD-29620 | j721e-idk-gw | IMG Decoder not passing ITU-T Streams | |
| LCPD-26692 | am335x-evm,am43xx-gpevm,am57xx-evm,am64xx-evm,j721e-idk-gw | Hardware + Software IPSec Performance Test Failures | |
| LCPD-22339 | j721e-idk-gw,j7200-evm | PCI-E USBCARD, ETHCARD don’t indicate 2-lane support with lspci | |
| LCPD-29699 | j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j721e-sk | J721E tidss fails to keep in sync with displays requesting resolutions > 2k |
2.1.7.6. Linux RT Kernel Known Issues¶
There are no known issues in this release in the Linux RT Kernel.
2.1.8. Change Requests¶
2.1.8.1. SDK features scope change for 8.5 release¶
| ID | Head Line |
|---|---|
| JACINTOREQ-4994 | Video Codec Memory Optimization Scope Change |
2.1.8.2. SDK features descoped from 8.4 release¶
| ID | Head Line | Original Fix Version | New Fix Version |
|---|---|---|---|
| JACINTOREQ-4930 | k3conf Doc and Test Modify | 08.04.00 | 08.05.00 |
2.1.8.3. SDK features descoped from 8.0 release¶
| ID | Head Line | Original Fix Version | New Fix Version |
|---|---|---|---|
| JACINTOREQ-1559 | Linux H264 decoder support | 08.00.00 | 08.01.00 |
| JACINTOREQ-1485 | Linux writeback pipeline support | 08.00.00 | None |
| JACINTOREQ-1444 | Vision apps inclusion in yocto build | 08.00.00 | None |
2.1.8.4. SDK features present in 7.0 that were descoped in 7.1¶
| Feature | Comments |
|---|---|
| HS support | Restored in 7.3 |
| SPL/Uboot boot modes restricted to SD card boot mode | Restored in 7.3 |
| 1s Linux boot | |
| Descope for support of native H264 encode/decode | Use R5F based driver with OpenVX as interface. H.264 decoder support restored in 7.3 |
| GPU compression | |
| SA2UL driver optimization | |
| Display Sharing | Display sharing demo available in SDK v6.1 |
| Virtualization (Jailhouse hypervisor/IPC virtualization/CPSW9G virtualization) | Does not affect 3P virtualization solutions. Basic Jailhouse demo can be seen in SDK 7.0 |
2.1.9. Installation and Usage¶
The Software Developer’s Guide provides instructions on how to setup your Linux development environment, install the SDK and start your development. It also includes User’s Guides for various Example Applications.