3.1.1.4. NAND

Note

NAND is not supported on J721E platform.

This section documents how to write files to the NAND device and use it to load and then boot the Linux Kernel using a root filesystem also found on NAND.

3.1.1.4.1. Erasing, Reading and Writing to/from NAND partitions

Listing NAND partitions

Below command is used to see the list of mtd devices enabled in U-boot

mtdparts

Example output on DRA71x EVM:

device nand0 <nand.0>, # parts = 10
 #: name                size            offset          mask_flags
 0: NAND.SPL            0x00020000      0x00000000      0
 1: NAND.SPL.backup1    0x00020000      0x00020000      0
 2: NAND.SPL.backup2    0x00020000      0x00040000      0
 3: NAND.SPL.backup3    0x00020000      0x00060000      0
 4: NAND.u-boot-spl-os  0x00040000      0x00080000      0
 5: NAND.u-boot         0x00100000      0x000c0000      0
 6: NAND.u-boot-env     0x00020000      0x001c0000      0
 7: NAND.u-boot-env.backup10x00020000   0x001e0000      0
 8: NAND.kernel         0x00800000      0x00200000      0
 9: NAND.file-system    0x0f600000      0x00a00000      0

Note: In later sections the <partition name> symbol should be replaced with the partition name seen when executing the mtdparts command.

Erasing Partition

nand erase.part <partition name>

Writing to Partition

When writing to NAND partition the file to be written must have previously been copied to memory.

nand write <ddr address> <partition name> <file size>

The symbol <ddr address> refers to the location in memory that a file was read into DDR memory. The symbol <file size> represents the amount of bytes (in hex) of the file to write into the NAND partition. Note: When reading a file into DDR, U-boot by default sets the value of environment variable “filesize” to the number of bytes (in hex) that was read via the last read/load command.


As an example below shows the process of writing a kernel (zImage) into the NAND’s kernel partition. The zImage to be written is loaded from the SD card’s rootfs (2nd) partition. Loading zImage from MMC to DDR memory
U-Boot # mmc dev 0;
U-Boot # setenv devnum 0
U-Boot # setenv devtype mmc
U-Boot # mmc rescan
U-Boot # load ${devtype} 1:2 ${loadaddr} /boot/zImage

Now that zImage is loaded into memory time to write it into the NAND partition

U-Boot # nand erase.part NAND.kernel
U-Boot # nand write ${loadaddr} NAND.kernel ${filesize}

Reading from Partition

nand read <ddr address> <partition name>

The symbol <ddr address> should be replaced with the location in DDR that you want the contents of the NAND partition to be copied to. The symbol <partition name> contains the NAND partition name you want to read from.


3.1.1.4.2. Writing to NAND via DFU

Currently in boards that support using DFU, the default build supports writing to NAND, so no custom build is required. To see the list of available places to write to (in DFU terms, altsettings) use the mtdparts command to list the known MTD partitions and printenv dfu_alt_settings to see how they are mapped and exposed to dfu-util.

U-Boot # mtdparts

device nand0 <nand0>, # parts = 8
 #: name                size            offset          mask_flags
 0: NAND.SPL            0x00020000      0x00000000      0
 1: NAND.SPL.backup1    0x00020000      0x00020000      0
 2: NAND.SPL.backup2    0x00020000      0x00040000      0
 3: NAND.SPL.backup3    0x00020000      0x00060000      0
 4: NAND.u-boot         0x001e0000      0x00080000      0
 5: NAND.u-boot-env     0x00020000      0x00260000      0
 6: NAND.kernel         0x00500000      0x00280000      0
 7: NAND.file-system    0x0f880000      0x00780000      0

active partition: nand0,0 - (SPL) 0x00080000 @ 0x00000000
U-Boot # printenv dfu_alt_info_nand
dfu_alt_info=NAND.SPL part 0 1;NAND.SPL.backup1 part 0 2;NAND.SPL.backup2 part 0 3;NAND.SPL.backup3 part 0 4;NAND.u-boot part 0 5;NAND.kernel part 0 7;NAND.file-system part 0 8

This means that you can tell dfu-util to write anything to any of:

  • NAND.SPL
  • NAND.SPL.backup1
  • NAND.SPL.backup2
  • NAND.SPL.backup3
  • NAND.u-boot
  • NAND.kernel
  • NAND.file-system

Before writing you must erase at least the area to be written to. Then to start DFU on the target on the first NAND device:

U-Boot # nand erase.chip
U-Boot # setenv dfu_alt_info ${dfu_alt_info_nand}
U-Boot # dfu 0 nand 0

Then on the host PC to write MLO to the first SPL partition:

$ sudo dfu-util -D MLO -a NAND.SPL

3.1.1.4.3. NAND Boot

If you want to load and run U-Boot from NAND the first step is insuring that the appropriate U-boot files are loaded in the correct partition. For AM335x, AM437x, DRA7x devices this means writing the file MLO to the NAND’s SPL partition. For OMAP-L138 device, write the .ais image to the NAND’s partition. For all devices this requires writing u-boot.img to the NAND’s U-Boot partition.

Note

The NAND partition of OMAP-L138 is different from other devices, please use the following commands to program the NAND

=> setenv ipaddr <EVM_IPADDR>
=> setenv serverip <TFTP_SERVER_IPADDR>
=> tftp ${loadaddr} ${serverip}:u-boot-omapl138-lcdk.ais
=> print filesize
=> nand erase 0x20000 <hex_len>
=> nand write ${loadaddr} 0x20000 <hex_len>
* hex_len is next sector boundary of the filesize. The sector size is 0x10000.
set dip switch to NAND boot and power cycle the EVM

Once the file(s) have been written to NAND the board should then be powered off. Next evm’s boot switches need to be configured for NAND booting. To understand the appropriate boot switches settings please see the evm’s hardware setup guide.


3.1.1.4.4. Booting Kernel and Filesystem from NAND

If a user wants to use NAND as their primary storage then the NAND flash must have individual partitions for all the critical software needed to boot the kernel. At a minimum this includes kernel, dtb, file system. Some SoCs require additional files and firmware which also need to be stored in different NAND partitions.

Similar to booting the kernel from any interface the user must insure that all required files needed for booting are loaded in DDR memory. The only exception is the filesystem which will be loaded by the kernel via the bootargs parameters. Bootargs contains information passed to the kernel including where and how to mount the file system.

The below contains example bootargs used by DRA7x evm for using a ubifs filesystem

setenv bootargs console=${console} ${optargs} root=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048 rootfstype=ubifs rootwait=1

In the above example bootargs, “rootfs” stands for the value specified by in the “vol_name” parameter defined in the ubinize.cfg file. In ubi.mtd “NAND.file-system” and “2048” represents the name of the partition that contains the ubifs and page size. Rootfstype simply tells the kernel what type of file system to use.

By default for our evms properly loading, setting bootargs and booting the kernel is handled by running “run nandboot” in U-boot. Information on creating a UBIFS can be found here.