3.2.2.12. PCIe Root Complex

Introduction

The PCI Express (PCIe) module is a multi-lane I/O interconnect providing low pin count, high reliability, and high-speed data transfer at rates of up to 8.0 Gbps per lane per direction. It is a 3rd Generation I/O Interconnect technology succeeding ISA and PCI bus that is designed to be used as a general-purpose serial I/O interconnect in multiple market segments, including desktop, mobile, server, storage and embedded communications.

Features of J7ES

There are four instances of the PCIe subsystem. Following are some of the main features:

  • Each instance can be configured to operate in Root Complex mode or End Point mode
  • One or two lane configuration, capable up to 8.0 Gbps/lane (Gen3)
  • Support for Legacy, MSI and MSI-X Interrupt
  • There can be 32 different address mappings in outbound address translation unit. The mappings can be from regions reserved for each PCIe instance.
    • For instance PCIE0 and PCIE1, there are two regions in SoC Memory Map:
      • 128 MB region with address in lower 32 bits
      • 4 GB region with address above 32 bits
    • For instance PCIE2 and PCIE3, there are two regions in SoC Memory Map:
      • 128 MB region with address above 32 bits
      • 4 GB region with address above 32 bits

Capabilities of J721E EVM

There are three instances of the PCIe subsystem on the EVM. Following are some of the details for each instance:

Instance Supported lanes Supported Connector
PCIE0 1 lane Standard female connector
PCIE1 2 lane Standard female connector
PCIE2 2 lane m.2 connector keyed for SSD (M key)

Hardware Setup Details

J721E is, by default, intended to be operated in Root Complex mode.

For End Point mode, PCIE_1L_MODE_SEL (switch 5) and PCIE_2L_MODE_SEL (switch 6) should be set to ‘0’.

../../../../../_images/dip-switch.png

RC Software Architecture

Following is the software architecture for Root Complex mode:

../../../../../_images/Linux_PCIe_subsystem.png

Following is a brief explanation of layers shown in the diagram:

  • There are different drivers for the connected PCIe devices like pci_endpoint_test, tg-3, r8169, xhci-pci, ahci, etc. It could be vendor-specific like most of the ethernet cards (tg3, r8169) or class-specific like xhci-pci and ahci. Each of these drivers will also interact with it’s own domain-specific stack. For example, tg3 will interface with network stack, and xhci-pci will interface with USB stack.
  • The PCI core layer scans the PCIe bus to identify and detect any PCIe devices. It also binds the driver from the layer above, for the PCIe device, based on vendorid, deviceid and class.
  • The PCI BIOS layer handles resource management. For example, allocation of memory resources for BARs.
  • The bottom-most layer consists of the PCIe platform drivers like pcie-cadence, pcie-designware, etc. pci-j721e and pci-dra7xx are TI’s wrappers over these drivers. They configure platform-specific controllers and perform actual register writes.

RC Device Configuration

DTS Modification

The default dts for J721E is configured to be used in root complex mode.

Linux Driver Configuration

The following config options have to be enabled in order to configure the PCI controller to be used in Root Complex mode.

CONFIG_SOCIONEXT_SYNQUACER_PREITS=y
CONFIG_PCI=y
CONFIG_PCI_MSI=y
CONFIG_PCI_J721E=y
CONFIG_PCIE_CADENCE=y
CONFIG_PCIE_CADENCE_HOST=y

Testing Details

The RC should enumerate any off-the-shelf PCIe cards. It has been tested with Ethernet cards, NVMe cards, PCIe USB card, PCIe WiFi card, PCIe SATA card and also to J721E in loopback mode.

In order to see if the connected card is detected, lspci utility should be used. Different utilities can be used depending on the cards.

Following are the outputs for some of them:

  • Loopback mode (J721E EVM to J721E EVM)

    Two J721E EVMs can be connected in loopback mode by following the steps explained in End Point (EP) Device Configuration section for End Point (EP) and HOST Device Configuration section for Root Complex (RC) in PCIe End Point documentation. The pci-epf-test driver will be configured for End Point(EP) using those steps.

    The lspci output on the Root Complex (RC) device is as follows:

    root@j7-evm:~# lspci
    0000:00:00.0 PCI bridge: Texas Instruments Device b00d
    0000:01:00.0 Unassigned class [ff00]: Texas Instruments Device b00d
    0000:01:00.1 Unassigned class [ff00]: Texas Instruments Device b00d
    0000:01:00.2 Unassigned class [ff00]: Texas Instruments Device b00d
    0000:01:00.3 Unassigned class [ff00]: Texas Instruments Device b00d
    0000:01:00.4 Unassigned class [ff00]: Texas Instruments Device b00d
    0000:01:00.5 Unassigned class [ff00]: Texas Instruments Device b00d
    0001:00:00.0 PCI bridge: Texas Instruments Device b00d
    0002:00:00.0 PCI bridge: Texas Instruments Device b00d
    
  • WiFi card

    • lspci output
    root@j7-evm:~# lspci
    0000:00:00.0 PCI bridge: Texas Instruments Device b00d
    0000:01:00.0 Network controller: Intel Corporation Wireless 3160 (rev 6b)
    0001:00:00.0 PCI bridge: Texas Instruments Device b00d
    0002:00:00.0 PCI bridge: Texas Instruments Device b00d
    
    • Test using ping
    root@j7-evm:~# ping 192.168.10.1 -w 10|
    PING 192.168.10.1 (192.168.10.1): 56 data bytes
    64 bytes from 192.168.10.1: seq=0 ttl=64 time=176.985 ms
    64 bytes from 192.168.10.1: seq=1 ttl=64 time=49.840 ms
    64 bytes from 192.168.10.1: seq=2 ttl=64 time=32.125 ms
    64 bytes from 192.168.10.1: seq=3 ttl=64 time=4.652 ms
    64 bytes from 192.168.10.1: seq=4 ttl=64 time=70.805 ms
    64 bytes from 192.168.10.1: seq=6 ttl=64 time=195.564 ms
    64 bytes from 192.168.10.1: seq=7 ttl=64 time=9.321 ms
    64 bytes from 192.168.10.1: seq=8 ttl=64 time=5.784 ms
    64 bytes from 192.168.10.1: seq=9 ttl=64 time=18.015 ms
    
  • NVMe SSD

    • lspci output
    root@j7-evm:~# lspci -vv
    0000:00:00.0 PCI bridge: Texas Instruments Device b00d (prog-if 00 [Normal decode])
        Control: I/O- Mem- BusMaster- SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx-
        Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
        Interrupt: pin A routed to IRQ 0
        Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
        I/O behind bridge: None
        Memory behind bridge: None
        Prefetchable memory behind bridge: None
        Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
        BridgeCtl: Parity- SERR- NoISA- VGA- VGA16- MAbort- >Reset- FastB2B-
            PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
        Capabilities: [80] Power Management version 3
            Flags: PMEClk- DSI- D1+ D2- AuxCurrent=0mA PME(D0+,D1+,D2-,D3hot+,D3cold-)
            Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
        Capabilities: [90] MSI: Enable- Count=1/1 Maskable+ 64bit+
            Address: 0000000000000000  Data: 0000
            Masking: 00000000  Pending: 00000000
        Capabilities: [b0] MSI-X: Enable- Count=1 Masked-
            Vector table: BAR=0 offset=00000000
            PBA: BAR=0 offset=00000008
        Capabilities: [c0] Express (v2) Root Port (Slot+), MSI 00
            DevCap:     MaxPayload 256 bytes, PhantFunc 0
                ExtTag- RBE+
            DevCtl:     CorrErr- NonFatalErr- FatalErr- UnsupReq-
                RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                MaxPayload 128 bytes, MaxReadReq 512 bytes
            DevSta:     CorrErr- NonFatalErr- FatalErr- UnsupReq- AuxPwr- TransPend-
            LnkCap:     Port #0, Speed 8GT/s, Width x1, ASPM L1, Exit Latency L1 <8us
                ClockPM- Surprise- LLActRep- BwNot+ ASPMOptComp+
            LnkCtl:     ASPM Disabled; RCB 64 bytes Disabled- CommClk-
                ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
            LnkSta:     Speed 2.5GT/s (downgraded), Width x2 (strange)
                TrErr- Train- SlotClk- DLActive- BWMgmt- ABWMgmt-
            SltCap:     AttnBtn- PwrCtrl- MRL- AttnInd- PwrInd- HotPlug- Surprise-
                Slot #0, PowerLimit 0.000W; Interlock- NoCompl-
            SltCtl:     Enable: AttnBtn- PwrFlt- MRL- PresDet- CmdCplt- HPIrq- LinkChg-
                Control: AttnInd Off, PwrInd Off, Power+ Interlock-
            SltSta:     Status: AttnBtn- PowerFlt- MRL+ CmdCplt- PresDet- Interlock-
                Changed: MRL- PresDet- LinkState-
            RootCtl: ErrCorrectable- ErrNon-Fatal- ErrFatal- PMEIntEna- CRSVisible-
            RootCap: CRSVisible-
            RootSta: PME ReqID 0000, PMEStatus- PMEPending-
            DevCap2: Completion Timeout: Range B, TimeoutDis+, LTR+, OBFF Not Supported ARIFwd+
                AtomicOpsCap: Routing- 32bit- 64bit- 128bitCAS-
            DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled ARIFwd-
                AtomicOpsCtl: ReqEn- EgressBlck-
            LnkCtl2: Target Link Speed: 8GT/s, EnterCompliance- SpeedDis-
                Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                Compliance De-emphasis: -6dB
            LnkSta2: Current De-emphasis Level: -3.5dB, EqualizationComplete-, EqualizationPhase1-
                EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
        Capabilities: [100 v2] Advanced Error Reporting
            UESta:      DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
            UEMsk:      DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
            UESvrt:     DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
            CESta:      RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr-
            CEMsk:      RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
            AERCap:     First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
                MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
            HeaderLog: 00000000 00000000 00000000 00000000
            RootCmd: CERptEn- NFERptEn- FERptEn-
            RootSta: CERcvd- MultCERcvd- UERcvd- MultUERcvd-
                FirstFatal- NonFatalMsg- FatalMsg- IntMsg 0
            ErrorSrc: ERR_COR: 0000 ERR_FATAL/NONFATAL: 0000
        Capabilities: [150 v1] Device Serial Number 00-00-00-00-00-00-00-00
        Capabilities: [300 v1] Secondary PCI Express <?>
        Capabilities: [4c0 v1] Virtual Channel
            Caps:       LPEVC=0 RefClk=100ns PATEntryBits=1
            Arb:        Fixed- WRR32- WRR64- WRR128-
            Ctrl:       ArbSelect=Fixed
            Status:     InProgress-
            VC0:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
                Status: NegoPending- InProgress-
            VC1:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable- ID=1 ArbSelect=Fixed TC/VC=00
                Status: NegoPending- InProgress-
            VC2:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable- ID=2 ArbSelect=Fixed TC/VC=00
                Status: NegoPending- InProgress-
            VC3:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable- ID=3 ArbSelect=Fixed TC/VC=00
                Status: NegoPending- InProgress-
        Capabilities: [5c0 v1] Address Translation Service (ATS)
            ATSCap:     Invalidate Queue Depth: 01
            ATSCtl:     Enable-, Smallest Translation Unit: 00
        Capabilities: [640 v1] Page Request Interface (PRI)
            PRICtl: Enable- Reset-
            PRISta: RF- UPRGI- Stopped+
            Page Request Capacity: 00000001, Page Request Allocation: 00000000
        Capabilities: [900 v1] L1 PM Substates
            L1SubCap: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2+ ASPM_L1.1+ L1_PM_Substates+
                PortCommonModeRestoreTime=255us PortTPowerOnTime=26us
            L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
                T_CommonMode=0us LTR1.2_Threshold=0ns
            L1SubCtl2: T_PwrOn=10us
        Kernel modules: pci_endpoint_test, ntb_hw_epf
    
    0001:00:00.0 PCI bridge: Texas Instruments Device b00d (prog-if 00 [Normal decode])
        Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx-
        Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
        Latency: 0
        Interrupt: pin A routed to IRQ 0
        Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
        I/O behind bridge: None
        Memory behind bridge: 18100000-181fffff [size=1M]
        Prefetchable memory behind bridge: None
        Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
        BridgeCtl: Parity- SERR- NoISA- VGA- VGA16- MAbort- >Reset- FastB2B-
            PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
        Capabilities: [80] Power Management version 3
            Flags: PMEClk- DSI- D1+ D2- AuxCurrent=0mA PME(D0+,D1+,D2-,D3hot+,D3cold-)
            Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
        Capabilities: [90] MSI: Enable- Count=1/1 Maskable+ 64bit+
            Address: 0000000000000000  Data: 0000
            Masking: 00000000  Pending: 00000000
        Capabilities: [b0] MSI-X: Enable- Count=1 Masked-
            Vector table: BAR=0 offset=00000000
            PBA: BAR=0 offset=00000008
        Capabilities: [c0] Express (v2) Root Port (Slot+), MSI 00
            DevCap:     MaxPayload 256 bytes, PhantFunc 0
                ExtTag- RBE+
            DevCtl:     CorrErr- NonFatalErr- FatalErr- UnsupReq-
                RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                MaxPayload 128 bytes, MaxReadReq 512 bytes
            DevSta:     CorrErr- NonFatalErr- FatalErr- UnsupReq- AuxPwr- TransPend-
            LnkCap:     Port #0, Speed 8GT/s, Width x2, ASPM L1, Exit Latency L1 <8us
                ClockPM- Surprise- LLActRep- BwNot+ ASPMOptComp+
            LnkCtl:     ASPM Disabled; RCB 64 bytes Disabled- CommClk-
                ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
            LnkSta:     Speed 8GT/s (ok), Width x2 (ok)
                TrErr- Train- SlotClk- DLActive- BWMgmt- ABWMgmt+
            SltCap:     AttnBtn- PwrCtrl- MRL- AttnInd- PwrInd- HotPlug- Surprise-
                Slot #0, PowerLimit 0.000W; Interlock- NoCompl-
            SltCtl:     Enable: AttnBtn- PwrFlt- MRL- PresDet- CmdCplt- HPIrq- LinkChg-
                Control: AttnInd Off, PwrInd Off, Power+ Interlock-
            SltSta:     Status: AttnBtn- PowerFlt- MRL+ CmdCplt- PresDet- Interlock-
                Changed: MRL- PresDet- LinkState-
            RootCtl: ErrCorrectable- ErrNon-Fatal- ErrFatal- PMEIntEna- CRSVisible-
            RootCap: CRSVisible-
            RootSta: PME ReqID 0000, PMEStatus- PMEPending-
            DevCap2: Completion Timeout: Range B, TimeoutDis+, LTR+, OBFF Not Supported ARIFwd+
                AtomicOpsCap: Routing- 32bit- 64bit- 128bitCAS-
            DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled ARIFwd+
                AtomicOpsCtl: ReqEn- EgressBlck-
            LnkCtl2: Target Link Speed: 8GT/s, EnterCompliance- SpeedDis-
                Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                Compliance De-emphasis: -6dB
            LnkSta2: Current De-emphasis Level: -6dB, EqualizationComplete+, EqualizationPhase1+
                EqualizationPhase2+, EqualizationPhase3+, LinkEqualizationRequest-
        Capabilities: [100 v2] Advanced Error Reporting
            UESta:      DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
            UEMsk:      DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
            UESvrt:     DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
            CESta:      RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr-
            CEMsk:      RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
            AERCap:     First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
                MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
            HeaderLog: 00000000 00000000 00000000 00000000
            RootCmd: CERptEn- NFERptEn- FERptEn-
            RootSta: CERcvd- MultCERcvd- UERcvd- MultUERcvd-
                FirstFatal- NonFatalMsg- FatalMsg- IntMsg 0
            ErrorSrc: ERR_COR: 0000 ERR_FATAL/NONFATAL: 0000
        Capabilities: [150 v1] Device Serial Number 00-00-00-00-00-00-00-00
        Capabilities: [300 v1] Secondary PCI Express <?>
        Capabilities: [4c0 v1] Virtual Channel
            Caps:       LPEVC=0 RefClk=100ns PATEntryBits=1
            Arb:        Fixed- WRR32- WRR64- WRR128-
            Ctrl:       ArbSelect=Fixed
            Status:     InProgress-
            VC0:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
                Status: NegoPending- InProgress-
            VC1:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable- ID=1 ArbSelect=Fixed TC/VC=00
                Status: NegoPending- InProgress-
            VC2:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable- ID=2 ArbSelect=Fixed TC/VC=00
                Status: NegoPending- InProgress-
            VC3:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable- ID=3 ArbSelect=Fixed TC/VC=00
                Status: NegoPending- InProgress-
        Capabilities: [5c0 v1] Address Translation Service (ATS)
            ATSCap:     Invalidate Queue Depth: 01
            ATSCtl:     Enable-, Smallest Translation Unit: 00
        Capabilities: [640 v1] Page Request Interface (PRI)
            PRICtl: Enable- Reset-
            PRISta: RF- UPRGI- Stopped+
            Page Request Capacity: 00000001, Page Request Allocation: 00000000
        Capabilities: [900 v1] L1 PM Substates
            L1SubCap: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2+ ASPM_L1.1+ L1_PM_Substates+
                PortCommonModeRestoreTime=255us PortTPowerOnTime=26us
            L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
                T_CommonMode=0us LTR1.2_Threshold=0ns
            L1SubCtl2: T_PwrOn=10us
        Kernel modules: pci_endpoint_test, ntb_hw_epf
    
    0001:01:00.0 Non-Volatile memory controller: Lite-On Technology Corporation M8Pe Series NVMe SSD (rev 01) (prog-if 02 [NVM Express])
        Subsystem: Marvell Technology Group Ltd. M8Pe Series NVMe SSD
        Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx+
        Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
        Latency: 0
        Interrupt: pin A routed to IRQ 0
        Region 0: Memory at 18120000 (64-bit, non-prefetchable) [size=16K]
        Expansion ROM at 18100000 [size=128K]
        Capabilities: [40] Power Management version 3
            Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
            Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
        Capabilities: [50] MSI: Enable- Count=1/1 Maskable+ 64bit+
            Address: 0000000000000000  Data: 0000
            Masking: 00000000  Pending: 00000000
        Capabilities: [70] Express (v2) Endpoint, MSI 00
            DevCap:     MaxPayload 128 bytes, PhantFunc 0, Latency L0s unlimited, L1 unlimited
                ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset+ SlotPowerLimit 0.000W
            DevCtl:     CorrErr- NonFatalErr- FatalErr- UnsupReq-
                RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop- FLReset-
                MaxPayload 128 bytes, MaxReadReq 512 bytes
            DevSta:     CorrErr- NonFatalErr- FatalErr- UnsupReq- AuxPwr- TransPend-
            LnkCap:     Port #0, Speed 8GT/s, Width x4, ASPM L1, Exit Latency L1 <64us
                ClockPM+ Surprise- LLActRep- BwNot- ASPMOptComp+
            LnkCtl:     ASPM Disabled; RCB 64 bytes Disabled- CommClk-
                ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
            LnkSta:     Speed 8GT/s (ok), Width x2 (downgraded)
                TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
            DevCap2: Completion Timeout: Not Supported, TimeoutDis+, LTR+, OBFF Via message
                AtomicOpsCap: 32bit- 64bit- 128bitCAS-
            DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled
                AtomicOpsCtl: ReqEn-
            LnkCtl2: Target Link Speed: 8GT/s, EnterCompliance- SpeedDis-
                Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                Compliance De-emphasis: -6dB
            LnkSta2: Current De-emphasis Level: -6dB, EqualizationComplete+, EqualizationPhase1+
                EqualizationPhase2+, EqualizationPhase3+, LinkEqualizationRequest-
        Capabilities: [b0] MSI-X: Enable+ Count=19 Masked-
            Vector table: BAR=0 offset=00002000
            PBA: BAR=0 offset=00003000
        Capabilities: [100 v2] Advanced Error Reporting
            UESta:      DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
            UEMsk:      DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
            UESvrt:     DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
            CESta:      RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr-
            CEMsk:      RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
            AERCap:     First Error Pointer: 00, ECRCGenCap+ ECRCGenEn+ ECRCChkCap+ ECRCChkEn+
                MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
            HeaderLog: 00000000 00000000 00000000 00000000
        Capabilities: [148 v1] Device Serial Number 00-00-00-00-00-00-00-00
        Capabilities: [158 v1] Power Budgeting <?>
        Capabilities: [168 v1] Alternative Routing-ID Interpretation (ARI)
            ARICap:     MFVC- ACS-, Next Function: 0
            ARICtl:     MFVC- ACS-, Function Group: 0
        Capabilities: [178 v1] Secondary PCI Express <?>
        Capabilities: [2b8 v1] Latency Tolerance Reporting
            Max snoop latency: 0ns
            Max no snoop latency: 0ns
        Capabilities: [2c0 v1] L1 PM Substates
            L1SubCap: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2+ ASPM_L1.1+ L1_PM_Substates+
                PortCommonModeRestoreTime=10us PortTPowerOnTime=10us
            L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
                T_CommonMode=0us LTR1.2_Threshold=0ns
            L1SubCtl2: T_PwrOn=10us
        Kernel driver in use: nvme
        Kernel modules: nvme
    
    0002:00:00.0 PCI bridge: Texas Instruments Device b00d (prog-if 00 [Normal decode])
        Control: I/O- Mem- BusMaster- SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx-
        Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
        Interrupt: pin A routed to IRQ 0
        Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
        I/O behind bridge: None
        Memory behind bridge: None
        Prefetchable memory behind bridge: None
        Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
        BridgeCtl: Parity- SERR- NoISA- VGA- VGA16- MAbort- >Reset- FastB2B-
            PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
        Capabilities: [80] Power Management version 3
            Flags: PMEClk- DSI- D1+ D2- AuxCurrent=0mA PME(D0+,D1+,D2-,D3hot+,D3cold-)
            Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
        Capabilities: [90] MSI: Enable- Count=1/1 Maskable+ 64bit+
            Address: 0000000000000000  Data: 0000
            Masking: 00000000  Pending: 00000000
        Capabilities: [b0] MSI-X: Enable- Count=1 Masked-
            Vector table: BAR=0 offset=00000000
            PBA: BAR=0 offset=00000008
        Capabilities: [c0] Express (v2) Root Port (Slot+), MSI 00
            DevCap:     MaxPayload 256 bytes, PhantFunc 0
                ExtTag- RBE+
            DevCtl:     CorrErr- NonFatalErr- FatalErr- UnsupReq-
                RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                MaxPayload 128 bytes, MaxReadReq 512 bytes
            DevSta:     CorrErr- NonFatalErr- FatalErr- UnsupReq- AuxPwr- TransPend-
            LnkCap:     Port #0, Speed 8GT/s, Width x2, ASPM L1, Exit Latency L1 <8us
                ClockPM- Surprise- LLActRep- BwNot+ ASPMOptComp+
            LnkCtl:     ASPM Disabled; RCB 64 bytes Disabled- CommClk-
                ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
            LnkSta:     Speed 2.5GT/s (downgraded), Width x2 (ok)
                TrErr- Train- SlotClk- DLActive- BWMgmt- ABWMgmt-
            SltCap:     AttnBtn- PwrCtrl- MRL- AttnInd- PwrInd- HotPlug- Surprise-
                Slot #0, PowerLimit 0.000W; Interlock- NoCompl-
            SltCtl:     Enable: AttnBtn- PwrFlt- MRL- PresDet- CmdCplt- HPIrq- LinkChg-
                Control: AttnInd Off, PwrInd Off, Power+ Interlock-
            SltSta:     Status: AttnBtn- PowerFlt- MRL+ CmdCplt- PresDet- Interlock-
                Changed: MRL- PresDet- LinkState-
            RootCtl: ErrCorrectable- ErrNon-Fatal- ErrFatal- PMEIntEna- CRSVisible-
            RootCap: CRSVisible-
            RootSta: PME ReqID 0000, PMEStatus- PMEPending-
            DevCap2: Completion Timeout: Range B, TimeoutDis+, LTR+, OBFF Not Supported ARIFwd+
                AtomicOpsCap: Routing- 32bit- 64bit- 128bitCAS-
            DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled ARIFwd-
                AtomicOpsCtl: ReqEn- EgressBlck-
            LnkCtl2: Target Link Speed: 8GT/s, EnterCompliance- SpeedDis-
                Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                Compliance De-emphasis: -6dB
            LnkSta2: Current De-emphasis Level: -3.5dB, EqualizationComplete-, EqualizationPhase1-
                EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
        Capabilities: [100 v2] Advanced Error Reporting
            UESta:      DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
            UEMsk:      DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
            UESvrt:     DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
            CESta:      RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr-
            CEMsk:      RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
            AERCap:     First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
                MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
            HeaderLog: 00000000 00000000 00000000 00000000
            RootCmd: CERptEn- NFERptEn- FERptEn-
            RootSta: CERcvd- MultCERcvd- UERcvd- MultUERcvd-
                FirstFatal- NonFatalMsg- FatalMsg- IntMsg 0
            ErrorSrc: ERR_COR: 0000 ERR_FATAL/NONFATAL: 0000
        Capabilities: [150 v1] Device Serial Number 00-00-00-00-00-00-00-00
        Capabilities: [300 v1] Secondary PCI Express <?>
        Capabilities: [4c0 v1] Virtual Channel
            Caps:       LPEVC=0 RefClk=100ns PATEntryBits=1
            Arb:        Fixed- WRR32- WRR64- WRR128-
            Ctrl:       ArbSelect=Fixed
            Status:     InProgress-
            VC0:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
                Status: NegoPending- InProgress-
            VC1:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable- ID=1 ArbSelect=Fixed TC/VC=00
                Status: NegoPending- InProgress-
            VC2:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable- ID=2 ArbSelect=Fixed TC/VC=00
                Status: NegoPending- InProgress-
            VC3:        Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                Ctrl:   Enable- ID=3 ArbSelect=Fixed TC/VC=00
                Status: NegoPending- InProgress-
        Capabilities: [5c0 v1] Address Translation Service (ATS)
            ATSCap:     Invalidate Queue Depth: 01
            ATSCtl:     Enable-, Smallest Translation Unit: 00
        Capabilities: [640 v1] Page Request Interface (PRI)
            PRICtl: Enable- Reset-
            PRISta: RF- UPRGI- Stopped+
            Page Request Capacity: 00000001, Page Request Allocation: 00000000
        Capabilities: [900 v1] L1 PM Substates
            L1SubCap: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2+ ASPM_L1.1+ L1_PM_Substates+
                PortCommonModeRestoreTime=255us PortTPowerOnTime=26us
            L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
                T_CommonMode=0us LTR1.2_Threshold=0ns
            L1SubCtl2: T_PwrOn=10us
        Kernel modules: pci_endpoint_test, ntb_hw_epf
    
    • Test using hdparm
    root@j7-evm:~# hdparm -tT /dev/nvme0n1
    
    /dev/nvme0n1:
    Timing cached reads: 3678 MB in 2.00 seconds = 1840.32 MB/sec
    Timing buffered disk reads: 2252 MB in 3.00 seconds = 750.34 MB/sec
    
    • Test using dd
    root@j7-evm:~# time dd if=/dev/urandom of=/home/root/srctest_file_pci_2199 bs=1M count=10|
    10+0 records in
    10+0 records out
    real        0m 0.17s
    user        0m 0.00s
    sys     0m 0.08s
    

J7200 Testing Details

PCIe and QSGMII uses the same SERDES in J7200. The default SDK is enabled for QSGMII. In order to test PCIe, Ethfw firmware shouldn’t be loaded and PCIe overlay file should be applied.

The simplest way to avoid ethfw from being loaded is to link j7200-main-r5f0_0-fw to IPC firmware.

root@j7200-evm:~# rm /lib/firmware/j7200-main-r5f0_0-fw
root@j7200-evm:~# ln -s /lib/firmware/pdk-ipc/ipc_echo_test_mcu2_0_release_strip.xer5f /lib/firmware/j7200-main-r5f0_0-fw

The following Device Tree Overlay should be applied for testing J7200 RC.

https://git.ti.com/cgit/ti-linux-kernel/ti-upstream-tools/tree/arch/arm64/boot/dts/ti/system_test/pcie/pcie_ep/k3-j7200-common-proc-board-pcie.dtso?h=ti-linux-5.4.y

The following command should be given in u-boot to apply overlay

=> setenv name_overlays k3-j7200-common-proc-board-pcie.dtbo