2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) for Linux provides a fundamental software platform for development, deployment and execution of Linux based applications and includes the following:
- Bootloaders, Linux Kernel & Filesystem
- SDK installer
- Setup scripts
- Demo applications
- Documentation
Note
For building some of the RTOS-based demonstrations, you should also download Processor SDK RTOS installer. For more information, refer to <PSDKRA install path>/index.html.
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below. In addition, see Processor SDK Linux GPLv3 Disclaimer.
2.1.3. Documentation¶
- Processor SDK Linux Software Developer’s Guide: Provides information on features, functions, delivery package and, compile tools for the Processor SDK Linux release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Processor SDK Linux Getting Started Guide: Provides information on getting the software and running examples/demonstrations bundled in the SDK.
- Software Manifest: Provides license information on software
included in the SDK release. This document is in the release at
[INSTALL-DIR]/docs. - EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Supported Platforms¶
See here for a list of supported platforms and links to more information.
2.1.5. Release 08.00.00¶
Released August 2021
What’s New
Processor SDK 8.0 Release has following new features:
- First release on 2021 LTS 5.10 kernel, 2021.01 U-Boot
- J7200, J721E: HSM bootloader re-arch
- J721E HS Boot
- AM64, J7200, J721E: Unified DDR driver
- ATF 2.5, OPTEE 3.12
2.1.6. Build Information¶
2.1.6.1. U-Boot¶
2.1.6.2. Kernel¶
Linux Kernel
Real Time (RT) Linux Kernel
Generic Kernel Release Notes
2.1.6.3. Yocto¶
meta-ti
meta-arago
2.1.7. Issues Tracker¶
2.1.7.1. Issues opened in previous releases that were closed on this release¶
| Record ID | Summary |
|---|---|
| LCPD-20229 | U-Boot : HS Boot post Rearch for J721E |
| LCPD-21334 | Convert ti,j721e-gpio to yaml |
| LCPD-20389 | DDR Frequency requested(4266 MHz) & the value set(3200 MHz) are different(SDK 7.1/7.2) |
| LCPD-20741 | j721e PCIe backplane test fails to load the dtb overlay |
| LCPD-20622 | J721e-ivi-evm DSS CRTC0 sync lost error |
| LCPD-21297 | Upstream: remoteproc/pru: Fix multiple issues in firmware event mapping |
| LCPD-18935 | IPC tests failed on j721e in 07.00 rc5 |
| LCPD-18673 | IPSEC fails to establish connection when using HW crypto |
| LCPD-19822 | ARM benchmark testcases returning lower than expected performance |
| LCPD-20700 | Direction for MCU_RGMII1_TXC pin in for u-boot and Kernel DTB don’t match Pinmux tool’s output |
2.1.7.2. Issues found and closed on this release that may be applicable to prior releases¶
| Record ID | Summary |
|---|---|
| LCPD-22208 | J7ES: Linux not using the latest RM Boardcfg from the sysconfig tool leading to inconsistency with PDK |
| LCPD-23003 | IPC: when pdk-ipc fw loaded from u-boot it breaks j721e boot and ethfw |
| LCPD-22979 | firmware links are missing in /lib/firmware directory for K3 |
| LCPD-22097 | Kernel crash for video file based demo |
| LCPD-22914 | HS EVMs fail to boot |
| LCPD-22300 | /dev/hwrng missing on K3 platforms |
| LCPD-22242 | Kernel: UBIFS test failing on J721E |
| LCPD-22207 | SDK: j7*-*evm fails to build after 5.10 kernel migration |
| LCPD-22209 | J7ES: OSPI boot: TISCI config ring fail error with SDK7.3 |
| LCPD-22048 | U-Boot: J7/AM64: DDR driver size is bloated up |
| LCPD-22188 | j721e and am65 hs fails to build on 2021.01 uboot |
| LCPD-22792 | EFI is disabled |
| LCPD-22859 | j721e PCE-EP tests fail |
| LCPD-22488 | AM64 inconsistent promiscuous mode visibility |
| LCPD-22358 | U-Boot: am642/am654/j72xx: ethernet address fixup is broken |
| LCPD-22345 | U-Boot: Main R5F clusters are incorrectly in LockStep mode |
| LCPD-22349 | Displayport playback test fails: cannot find tidss device |
| LCPD-22344 | crypto: sa2ul: crypto self-tests fail to allocate des3 algos |
| LCPD-22342 | crypto: sa2ul: Fix a number of leaks in failure paths in probe |
| LCPD-22318 | CRYPTO_S_PERF testcases are missing CONFIG_CRYPTO_DEV_SA2UL arg in 2021.00 |
| LCPD-22282 | U-Boot: reset to default env fails in 2021 LTS |
| LCPD-22889 | U-Boot: k3-ddrss driver generates a build warning |
| LCPD-22285 | HS200 MMC speeds aren’t being achieved in kernel |
| LCPD-22816 | Update documentation to mention that CPSW 2G PPS support is disabled |
2.1.7.3. Errata workarounds¶
| Record ID | Summary | Workaround | ErrataID |
|---|---|---|---|
| LCPD-19068 | DSS: Disabling a layer connected to Overlay may result in synclost during the next frame | i2097 | |
| LCPD-19047 | USB: Race condition while reading TRB from system memory in device mode | i2067 | |
| LCPD-19965 | OSPI PHY Controller Bug Affecting Read Transactions | i2189 | |
| LCPD-17220 | U-Boot Hyperbus: Hyperflash reads limited to 125MHz max. frequency | i2088 | |
| LCPD-16605 | MMC: MMC1/2 Speed Issue | i2090 |
2.1.7.4. SDK Known Issues¶
| Record ID | Summary | Workaround |
|---|---|---|
| LCPD-22973 | GFX_XS_FUNC_GPU_MEM2MEM test fails due to a change in the expected output | |
| LCPD-22972 | j721e-idk-gw GLBenchmark GLB25_EgyptTestStandardOffscreen_inherited test | |
| LCPD-22921 | j721e PVR profiling with PVRPerfServer test is failing | |
| LCPD-22549 | v4l2h264dec : application hangs when setting the pipeline to null | |
| LCPD-22542 | v4l2h264dec is giving high latency compared to SW decoder | |
| LCPD-21298 | Frame Buffer Decompression does not show expected improvement | |
| LCPD-20620 | J721e: Gstreamer warning seen with video decoder mjpeg test | |
| LCPD-19948 | Yocto: stream recipe is incorrect | |
| LCPD-19894 | UYVY texture test fails due to internal data stream error | |
| LCPD-19858 | OE: OPTEE label used in SDK is old and wrong | |
| LCPD-19819 | KMS ALPHABLEND tests fail due to no attribute ‘get_default_mode’ | |
| LCPD-19716 | GFX_XS_FUNC_UYVY_TEXTURE test fails | |
| LCPD-18270 | Ivi shell test fails. Lib ivi-controller.so and other components are missing from the file system | |
| LCPD-17387 | Underflow and CRTC SYNC LOST observed while running GLMark2 (1x1080p + 1x4k) | |
| LCPD-16531 | video decode: vxd_dec warnings displayed at end of gstreamer hevc playback to kmssink for certain video | |
| LCPD-16366 | RGX kick test fails when 32 sync dependencies are set for each command | |
| LCPD-16130 | Exception triggered by drm_dev_unregister during poweroff |
2.1.7.5. U-Boot Known Issues¶
| Record ID | Summary | Workaround |
|---|---|---|
| LCPD-22967 | U-Boot: PLL PostDiv1 and PostDiv2 divider clock rates are computed incorrectly | |
| LCPD-19636 | J7: HS: OSPI Boot broken | |
| LCPD-22964 | U-Boot: PLL POSTDIV1 and POSTDIV2 clock parenting is reversed | |
| LCPD-22904 | U-boot: Update EMIFtool for i2244:DDR: Valid stop value must be defined for write DQ VREF training | |
| LCPD-22841 | j7200 Watchdog Timer test is failing | |
| LCPD-22451 | Documentation on J7ES Boot flow refers to AM65xx Boot flow in the u-boot user guide | |
| LCPD-20737 | Documentation: u-boot documentation issues | |
| LCPD-19776 | j7: uboot: some socketed evms fail to boot | |
| LCPD-17770 | U-Boot: Fix order of MCU R5 shutdown depending on cluster mode | |
| LCPD-17523 | A72-SPL - Support to dump EEPROM to shared memory | |
| LCPD-22512 | Update dfu_alt_info_ospi to include flashing of PHY tuning data | |
| LCPD-22246 | j721e Uboot DFU tests are failing | |
| LCPD-21986 | j721e U-Boot DDR50 mode cannot be tested using the default image | |
| LCPD-20131 | Uboot fails to enumerate devices attached to a usb hub on the first ‘usb reset’ call | Re-run usb reset command |
| LCPD-17789 | UBOOT J7: Could not see UFS device by scsi scan | |
| LCPD-19871 | U-boot: Documentation: Combined Boot flow and SPL Rearch | |
| LCPD-22452 | u-boot README doesn’t have eMMC specific documentation for J7ES |
2.1.7.6. Linux Kernel Known Issues¶
| Record ID | Summary | Workaround |
|---|---|---|
| LCPD-22913 | USBDEV ACM NCM enumeration fails on the device side | |
| LCPD-22278 | PCI-E USB devices fail to enumerate after power cycling | |
| LCPD-20653 | ltp: kernel syscall tests fail | |
| LCPD-17284 | remoteproc/k3-r5: Cores are started out-of-order when core 0 file size >> core 1 file size | |
| LCPD-16545 | remoteproc/k3-r5f: PDK IPC echo_test image fails to boot up in remoteproc mode on second run | |
| LCPD-16535 | remoteproc/k3-dsp: PDK IPC echo test binaries fails to do IPC in remoteproc mode on second run | |
| LCPD-22976 | omap-spi.txt convert to yaml | |
| LCPD-22487 | USB: usb0 doesn’t work properly in host only mode | |
| LCPD-20240 | MMC Modular testcase regression | |
| LCPD-19659 | Doc: PCIe: Update documentation to indicate how to move to compliance mode | |
| LCPD-19084 | Few SD cards not enumerating in Kernel with Alpha EVM | |
| LCPD-17814 | Kingston 16G card could not boot to uboot prompt | |
| LCPD-17794 | ext4write failed to write firmware to SD card | |
| LCPD-17421 | CPSW9G: Can’t bring up interface over NFS | |
| LCPD-17172 | Uboot USBhost: Sandisk Extreme USB 3.0 msc stick could not be detected at second time | |
| LCPD-17171 | Uboot dhcp occasionally failed | |
| LCPD-16640 | PCIe RC: GIC ITS misbehaves when more than 4 devices use it simultaneously | |
| LCPD-16628 | Could not enumerate PLEXTOR pcie SSD | |
| LCPD-16591 | PCIe wifi ping stress test failed | |
| LCPD-16396 | J721E: RC: Unsupported request in configuration completion packets results in an abort | Workaround for Multifunction: Configure all the physical functions supported by the endpoint. For configuring all the 6 functions of PCIe controller instance ‘1’ in J721E, the following can be used. mount -t configfs none /sys/kernel/config; cd /sys/kernel/config/pci_ep/; mkdir functions/pci_epf_test/func1; echo 0x104c > functions/pci_epf_test/func1/vendorid; echo 0xb00d > functions/pci_epf_test/func1/deviceid; echo 1 > functions/pci_epf_test/func1/msi_interrupts; echo 16 > functions/pci_epf_test/func1/msix_interrupts; ln -s functions/pci_epf_test/func1 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func2; echo 0x104c > functions/pci_epf_test/func2/vendorid; echo 0xb00d > functions/pci_epf_test/func2/deviceid; echo 1 > functions/pci_epf_test/func2/msi_interrupts; echo 16 > functions/pci_epf_test/func2/msix_interrupts; ln -s functions/pci_epf_test/func2 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func3; echo 0x104c > functions/pci_epf_test/func3/vendorid; echo 0xb00d > functions/pci_epf_test/func3/deviceid; echo 1 > functions/pci_epf_test/func3/msi_interrupts; echo 16 > functions/pci_epf_test/func3/msix_interrupts; ln -s functions/pci_epf_test/func3 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func4; echo 0x104c > functions/pci_epf_test/func4/vendorid; echo 0xb00d > functions/pci_epf_test/func4/deviceid; echo 1 > functions/pci_epf_test/func4/msi_interrupts; echo 16 > functions/pci_epf_test/func4/msix_interrupts; ln -s functions/pci_epf_test/func4 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func5; echo 0x104c > functions/pci_epf_test/func5/vendorid; echo 0xb00d > functions/pci_epf_test/func5/deviceid; echo 1 > functions/pci_epf_test/func5/msi_interrupts; echo 16 > functions/pci_epf_test/func5/msix_interrupts; ln -s functions/pci_epf_test/func5 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func6; echo 0x104c > functions/pci_epf_test/func6/vendorid; echo 0xb00d > functions/pci_epf_test/func6/deviceid; echo 1 > functions/pci_epf_test/func6/msi_interrupts; echo 16 > functions/pci_epf_test/func6/msix_interrupts; ln -s functions/pci_epf_test/func6 controllers/d800000.pcie-ep/; echo 1 > controllers/d800000.pcie-ep/start; echo 1 > /sys/bus/pci/devices/0000:00:00.0/remove; echo 1 > /sys/bus/pci/rescan; Workaround for switch card: No workarounds available. |
| LCPD-23010 | j721e-idk-gw stress boot test files | |
| LCPD-22861 | Missing documentation for HS devices | |
| LCPD-22760 | k3conf: Register read leads to kernel crash | |
| LCPD-22715 | i2232: DDR: Controller postpones more than allowed refreshes after frequency change | Workaround 1: Disable dynamic frequency change by programing DFS_ENABLE = 0 Workaround 2: If switching frequency, program the register field values as follows:
} |
| LCPD-22534 | Ipsec aes128 TCP test failure | |
| LCPD-19792 | j721e boot fails sometimes due to EL1 exception | |
| LCPD-18860 | isolcpus in the command line is not honored | |
| LCPD-18684 | syscalls sync failures: fdatasync03, fsync04, sync03, syncfs01, sync_file_range02 | |
| LCPD-18258 | IPSEC perfomance failures | |
| LCPD-17798 | 2020 LTS: INTA/INTR smp_affinity failure and IRQ allocation issues. | |
| LCPD-17673 | No software documentation for the Timer module | |
| LCPD-17543 | Some cpuhotplug tests failed | |
| LCPD-16505 | Wrong clock rate is reported for 157:400, 157:401 (HSDIVIDER after PLL4 and 15) | |
| LCPD-22831 | Application takes 10-15 seconds to come up in some cases | |
| LCPD-22362 | ALSA sampling format capture/loopback test - arecord failure | |
| LCPD-19068 | DSS: Disabling a layer connected to Overlay may result in synclost during the next frame | |
| LCPD-17387 | Underflow and CRTC SYNC LOST observed while running GLMark2 (1x1080p + 1x4k) | |
| LCPD-17006 | 4k DP Display Shows Blank Screen sometimes when booting | |
| LCPD-16836 | DP: GeChic display EDID read failures with custom DP cable | |
| LCPD-16616 | Jailhouse: Failure in mhdp probe while restarting the Linux VM | |
| LCPD-16208 | FIFO Underflows during video playback on 4k panel | |
| LCPD-22513 | Update SDK doc to include OSPI flashing instruction using dfu-util | |
| LCPD-20290 | CPSW Performance regression on j721e-idk-gw | |
| LCPD-18790 | eMMC tests failed on J7 rev E2 EVM | |
| LCPD-23057 | J721e: DFU boot test fails | |
| LCPD-22339 | PCI-E USBCARD, ETHCARD don’t indicate 2-lane support with lspci | |
| LCPD-23018 | j721e-idk-gw IPC tests fail on some EVMs |
2.1.7.7. RT Linux Kernel Known Issues¶
| Record ID | Summary | Workaround |
|---|---|---|
| LCPD-6663 | [RT] Kmemleak is buggy and boot is crashed randomly | |
| LCPD-22238 | RT linux build sometimes fails to boot - might be related to remoteproc2 |
2.1.8. Change Requests¶
2.1.8.1. SDK features descoped from 8.0 release¶
| ID | Head Line | Original Fix Version | New Fix Version |
|---|---|---|---|
| JACINTOREQ-1559 | Linux H264 decoder support | 08.00.00 | 08.01.00 |
| JACINTOREQ-1485 | Linux writeback pipeline support | 08.00.00 | None |
| JACINTOREQ-1444 | Vision apps inclusion in yocto build | 08.00.00 | None |
2.1.8.2. SDK features present in 7.0 that were descoped in 7.1¶
| Feature | Comments |
|---|---|
| HS support | Restored in 7.3 |
| SPL/Uboot boot modes restricted to SD card boot mode | Restored in 7.3 |
| 1s Linux boot | |
| Descope for support of native H264 encode/decode | Use R5F based driver with OpenVX as interface. H.264 decoder support restored in 7.3 |
| GPU compression | |
| SA2UL driver optimization | |
| Display Sharing | Display sharing demo available in SDK v6.1 |
| Virtualization (Jailhouse hypervisor/IPC virtualization/CPSW9G virtualization) | Does not affect 3P virtualization solutions. Basic Jailhouse demo can be seen in SDK 7.0 |
2.1.9. Installation and Usage¶
The Software Developer’s Guide provides instructions on how to setup your Linux development environment, install the SDK and start your development. It also includes User’s Guides for various Example Applications.