3.8.2. TensorFlow Lite¶
3.8.2.1. Introduction¶
TensorFlow Lite is an open source library for deep learning models. TensorFlow Lite runs on Jacinto Arm cores.
3.8.2.2. Supported version¶
- TensorFlow Lite 1.15
3.8.2.3. TensorFlow Lite example applications¶
TensoreFlow Lite example applications are installed on filesystem at /usr/share/tensorflow-lite/examples. One TensorFlow Lite model (mobilenet_v1_1.0_224_quant.tflite) is also installed at the same place for demonstration. To use other TensorFlow Lite models, such as TensorFlow Lite Hosted Models, please download those models and then copy them to the target.
root@am57xx-evm:/usr/share/tensorflow-lite/examples# ls -l
total 8356
-rwxr-xr-x 1 root root 2423336 Aug 28 08:27 benchmark_model
-rw-r--r-- 1 root root 940650 Aug 28 07:56 grace_hopper.bmp
-rwxr-xr-x 1 root root 2288600 Aug 28 08:27 label_image
-rw-r--r-- 1 root root 10484 Aug 28 07:56 labels.txt
-rwxr-xr-x 1 root root 2251048 Aug 28 08:27 minimal
-rw-r--r-- 1 root root 4276352 Aug 28 07:56 mobilenet_v1_1.0_224_quant.tflite
-rwxr-xr-x 1 root root 2152 Aug 28 07:56 tflite-benchmark.she
3.8.2.3.1. Running benchmark_model¶
The benchmark_model binary performs computation benchmarking for Tensorflow Lite models. Usage of benchmark_model:
usage: ./benchmark_model
Flags:
--num_runs=50 int32 number of runs
--run_delay=-1 float delay between runs in seconds
--num_threads=1 int32 number of threads
--benchmark_name= string benchmark name
--output_prefix= string benchmark output prefix
--warmup_runs=1 int32 how many runs to initialize model
--graph= string graph file name
--input_layer= string input layer names
--input_layer_shape= string input layer shape
--use_nnapi=false bool use nnapi api
Example of running benchmark_model on target using the pre-installed mobilenet_v1_1.0_224_quant.tflite model:
# cd /usr/share/tensorflow-lite/examples
# ./benchmark_model --graph=mobilenet_v1_1.0_224_quant.tflite
STARTING!
Min num runs: [50]
Min runs duration (seconds): [1]
Max runs duration (seconds): [150]
Inter-run delay (seconds): [-1]
Num threads: [1]
Benchmark name: []
Output prefix: []
Min warmup runs: [1]
Min warmup runs duration (seconds): [0.5]
Graph: [mobilenet_v1_1.0_224_quant.tflite]
Input layers: []
Input shapes: []
Use nnapi : [0]
Use legacy nnapi : [0]
Use gpu : [0]
Allow fp16 : [0]
Require full delegation : [0]
Enable op profiling: [0]
Max profiling buffer entries: [1024]
Loaded model mobilenet_v1_1.0_224_quant.tflite
resolved reporter
Initialized session in 126.941ms
Running benchmark for at least 1 iterations and at least 0.5 seconds but termin.
count=7 first=80936 curr=73720 min=73663 max=80936 avg=74766.3 std=2519
3.8.2.3.2. Running label_image example¶
The label_image provides an image classification example using TensorFlow Lite. Options for label_image:
--accelerated, -a: [0|1], use Android NNAPI or not
--count, -c: loop interpreter->Invoke() for certain times
--input_mean, -b: input mean
--input_std, -s: input standard deviation
--image, -i: image_name.bmp
--labels, -l: labels for the model
--tflite_model, -m: model_name.tflite
--profiling, -p: [0|1], profiling or not
--num_results, -r: number of results to show
--threads, -t: number of threads
--verbose, -v: [0|1] print more information
Example of running label_image on target, using the pre-installed mobilenet_v1_1.0_224_quant.tflite model, grace_hopper.bmp, and labels.txt.
# cd /usr/share/tensorflow-lite/examples
# ./label_image -i grace_hopper.bmp -l labels.txt -m mobilenet_v1_1.0_224_quant.tflite
Loaded model mobilenet_v1_1.0_224_quant.tflite
resolved reporter
invoked
average time: 164.164 ms
0.780392: 653 military uniform
0.105882: 907 Windsor tie
0.0156863: 458 bow tie
0.0117647: 466 bulletproof vest
0.00784314: 835 suit