1.1.4. Creating SD card on Linux¶
1.1.4.1. Overview¶
The Linux SDK includes a script in the <SDK INSTALL DIR>/bin directory named mksdboot.sh. The purpose of this script is to create bootable SD cards by partitioning and formatting them so that target can boot using the boot images and filesystem.
1.1.4.2. Partitioning SD card¶
No matter which use case above that you are creating an SD card for the following steps are the same.
The mksdboot.sh script can be run from any location but must be run with root permissions. This usually means using the sudo command to start execution of the script. For example:
sudo <SDK INSTALL DIR>/bin/mksdboot.sh --device /dev/sdX --sdk <SDK INSTALL DIR>
#Replace the /dev/sdX with appropriate device name
If you fail to execute the script without root permissions you will receive a message that root permissions are required and the script will exit.
1.1.4.3. Select the SD Card Device¶
The first step before running the script is to select the drive representing the SD card that you want to format. In most cases your host root file system drive has been masked off to prevent damage to the host system. You can run sudo fdisk -l to find out the device name for the SD card you want to format. Example output looks like this:
Disk /dev/sda: 931.5 GiB, 1000204886016 bytes, 1953525168 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes
Disklabel type: dos
Disk identifier: 0x2addf736
Device Boot Start End Sectors Size Id Type
/dev/sda1 2048 614402047 614400000 293G 83 Linux
/dev/sda2 614402048 1228802047 614400000 293G 83 Linux
/dev/sda3 1228802048 1953523711 724721664 345.6G 83 Linux
Disk /dev/sdd: 14.9 GiB, 15931539456 bytes, 31116288 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: dos
Disk identifier: 0xda7cb208
Device Boot Start End Sectors Size Id Type
/dev/sdd1 * 2048 129023 126976 62M c W95 FAT32 (LBA)
/dev/sdd2 129024 8517631 8388608 4G 83 Linux
/dev/sdd3 8517632 31116287 22598656 10.8G 83 Linux
You should choose the device where the partition sizes match with the SD card you want to partition.