3.1.2.14. HSM M4F Loading

Some K3 SoCs like J721S2 and J784S4 have a High Security Module (HSM) M4F core in the Wakeup Voltage Domain. The HSM M4 core is loaded at R5 SPL stage. Boot flow for HSM M4 core is different than the general purpose M4F cores, and is described as below:

  • Request control of HSM M4F remote processor.

  • Assert Reset on the HSM M4F remote processor.

  • Load firmware into HSM M4F core’s SRAM memory region.
    • For HS devices, request TIFS to authenticate and load the firmware.

    • For GP devices, load the firmware manually into HSM SRAM.

  • Deassert Reset on the HSM M4F remote processor.

  • Release control of HSM M4F remote processor.

This User Guide documents how to enable HSM core loading.

3.1.2.14.1. How to enable HSM M4F Loading

By default, only the HSM demo firmware for HS-SE device type is packed in tispl.bin FIT image. See How to build U-Boot with custom HSM firmware section to change the default firmware for other device types.

R5 SPL supports loading of HSM M4 core for all device types, i.e., HS-SE, HS-FS, GP. However, This feature is disabled by default in SDK. To enable HSM loading, set the CONFIG_K3_HSM_FW config in both <soc>_evm_r5_defconfig and <soc>_evm_a72_defconfig files.

For example, to enable HSM loading on J721S2 device, make the following changes:

diff --git a/configs/j721s2_evm_r5_defconfig b/configs/j721s2_evm_r5_defconfig
index 806c97792f6..ebe100c2278 100644
--- a/configs/j721s2_evm_r5_defconfig
+++ b/configs/j721s2_evm_r5_defconfig
@@ -187,3 +187,4 @@ CONFIG_FS_FAT_MAX_CLUSTSIZE=16384
 CONFIG_PANIC_HANG=y
 CONFIG_LIB_RATIONAL=y
 CONFIG_SPL_LIB_RATIONAL=y
+CONFIG_K3_HSM_FW=y
diff --git a/configs/j721s2_evm_a72_defconfig b/configs/j721s2_evm_a72_defconfig
index 6db41cb457e..a07e6d63270 100644
--- a/configs/j721s2_evm_a72_defconfig
+++ b/configs/j721s2_evm_a72_defconfig
@@ -198,3 +198,4 @@ CONFIG_UFS=y
 CONFIG_CADENCE_UFS=y
 CONFIG_TI_J721E_UFS=y
 CONFIG_TI_COMMON_CMD_OPTIONS=y
+CONFIG_K3_HSM_FW=y

Proceed to build U-Boot (tiboot3.bin and tispl.bin). One can verify if the HSM binary is packed inside tispl.bin FIT image by using following command:

mkimage -l <output directory>/a72/tispl.bin
<...>
Image 2 (hsm)
 Description:  HSM binary
 Created:      Thu Mar 20 13:26:16 2025
 Type:         Standalone Program
 Compression:  uncompressed
 Data Size:    132694 Bytes = 129.58 KiB = 0.13 MiB
 Architecture: Unknown Architecture
 Load Address: 0x82000000
 Entry point:  0x82000000
<...>

The HSM core loading can be verified by checking for the following log at R5 SPL stage: ‘Successfully booted HSM core’.

U-Boot SPL 2025.01-00391-ga7a25e886202-dirty (Mar 20 2025 - 11:04:05 +0530)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.9--v11.00.09+ (Fancy Rat)')
Initialized 4 DRAM controllers
SPL initial stack usage: 13456 bytes
Trying to boot from MMC2
Authentication passed
Authentication passed
Authentication passed
Loading Environment from nowhere... OK
Successfully booted HSM core
Authentication passed
Authentication passed
Starting ATF on ARM64 core...

3.1.2.14.2. How to build U-Boot with custom HSM firmware

To pack the firmware for any other device type, one can update the path in the SoC binman template to point to the custom binary and re-build U-Boot images (tispl.bin).

arch/arm/dts/k3-<soc>-binman.dtsi

hsm {
   hsm: blob-ext {
      filename = <path_to_custom_binary>;
   };
};

For example, To pack the HSM demo firmware for J784S4 HS-FS device type, make following changes to arch/arm/dts/k3-j784s4-binman.dtsi

hsm {
   hsm: blob-ext {
      filename = "ti-hsm/hsm-demo-firmware-j784s4-hs-fs.bin";
   };
};

A list of all HSM demo firmwares can be found in ti-linux-firmware repository.