3.2.2.22. UBIFS

Introduction

Unsorted Block Image File System is a file system specifically designed for flash memory devices. It’s built on top of the UBI layer, which handles low-level flash management tasks like wear-leveling and bad block management by dividing it into Logical Erase Blocks (LEBs).

Using UBIFS on flash

Flash devices can be divided into multiple partitions, including a rootfs partition dedicated for the root file system. The rootfs partition can be formatted with the UBIFS and the volume can be mounted as the root file system during boot.

Required Software for UBI image creation

Building a UBI File System requires two applications, ubinize and mkfs.ubifs. Both are both provided by mtd-utils package.

$ sudo apt-get install mtd-utils

Building a UBI File System image

Step 1

Create a directory containing the root file system. It is important that the directory size is smaller than the rootfs partition in the flash. Users can download the default/tiny image for specific SoC.

Note

Download and extract tisdk-default-image-*-evm.rootfs.tar.xz for QSPI/OSPI/GPMC NAND.

Download and extract tisdk-tiny-image-*-evm.rootfs.tar.xz for QSPI/OSPI NOR.

The rootfs partition information

OSPI NOR

# EVM Linux

$ mtdinfo /dev/mtd5
mtd5
Name:                           ospi.rootfs
Type:                           nor
Eraseblock size:                262144 bytes, 256.0 KiB
Amount of eraseblocks:          223 (58458112 bytes, 55.7 MiB)
Minimum input/output unit size: 16 bytes
Sub-page size:                  16 bytes
Character device major/minor:   90:10
Bad blocks are allowed:         false
Device is writable:             true

OSPI NAND

# EVM Linux

$ mtdinfo /dev/mtd5
mtd5
Name:                           ospi_nand.rootfs
Type:                           nand
Eraseblock size:                262144 bytes, 256.0 KiB
Amount of eraseblocks:          383 (100401152 bytes, 95.7 MiB)
Minimum input/output unit size: 4096 bytes
Sub-page size:                  4096 bytes
OOB size:                       128 bytes
Character device major/minor:   90:10
Bad blocks are allowed:         true
Device is writable:             true

GPMC NAND

# EVM Linux

$ mtdinfo /dev/mtd7
mtd7
Name:                           NAND.file-system
Type:                           nand
Eraseblock size:                262144 bytes, 256.0 KiB
Amount of eraseblocks:          4054 (1062731776 bytes, 1013.5 MiB)
Minimum input/output unit size: 4096 bytes
Sub-page size:                  1024 bytes
OOB size:                       256 bytes
Character device major/minor:   90:14
Bad blocks are allowed:         true
Device is writable:             true

Step 2

Create a file named ubinize.cfg and add the contents below. Note that this configuration file can be outside the root directory.

[ubifs]
mode=ubi
image=rootfs.ubifs
vol_id=0
vol_type=dynamic
vol_name=rootfs
vol_flags=autoresize

Step 3

mkfs.ubifs is used to create UBI File System image, which is specifically generated for a flash memory device, like Serial NOR, NAND and Parallel NAND.

Syntax

mkfs.ubifs -r <root_dir> -o <output_image> [options]

Some key options to use:

  1. -m <min_io_size>: specifies the minimum I/O size (in bytes) of the flash device.

    The 'Minimum input/output unit size' value in mtdinfo.
    
  2. -e <leb_size>: specifies the logical eraseblock (LEB) size, which is the usable portion of an eraseblock in UBI.

    Logical Erase Block size = Physical Erase block size - UBI overhead
    
       Here,
       a. Physical Erase block size is the 'Eraseblock size' value in mtdinfo.
       b. UBI overhead = ALIGN((VID Header offset + sizeof(struct ubi_vid_hdr)), Minimum input/output unit size)
    
          Here,
          -> ALIGN(x,a) expands to (((x) + ((a) - 1)) & ~((a) - 1))
          -> sizeof(struct ubi_vid_hdr) is 64
          -> Minimum input/output unit size is the 'Minimum input/output unit
          size' value in mtdinfo
    

    For VID Header offset, refer 4th option, here.

  3. -c <max_leb>: specifies the maximum number of logical eraseblocks (LEBs) the filesystem can use.

    The 'Amount of eraseblocks' value in mtdinfo.
    
  4. -x <compression>: specifies the compression method to use. Default is ‘zlib’.

  5. -F: used to force the filesystem to “fixup” all the free space which it is going to use. Note, this flag makes the first mount very slow, because the “free space fixup” procedure takes time.

For more details:

mkfs.ubifs --help

Step 4

ubinize is used to create UBI image for one or more UBIFS images.

ubinize [options] -o <output_image> <configuration_file>

Some key options to use:

  1. -m <min_io_size>: specifies the minimum I/O size (in bytes) of the flash device.

    The 'Minimum input/output unit size' value in mtdinfo.
    
  2. -p <peb_size>: specifies the physical eraseblock size, which is the total size of an eraseblock in the flash device.

    The 'Eraseblock size' value in mtdinfo.
    
  3. -s <sub_page_size>: specifies the sub-page size. Usually equivalent to the minimum I/O size.

    The 'Sub-page size' value in mtdinfo.
    
  4. -O <vid_hdr_offset>: specifies the offset of the VID (Volume Identifier) header within the physical eraseblock.

    VID Header offset = ALIGN((sizeof(struct ubi_ec_hdr)), Headers Minimum input/output unit size)
    
       Here,
       a. ALIGN(x,a) expands to (((x) + ((a) - 1)) & ~((a) - 1))
       b. sizeof(struct ubi_ec_hdr) is 64
       c. Headers Minimum input/output unit size = Minimum input/output unit size >> Sub Page shift
    
          Here,
          -> Minimum input/output unit size is the 'Minimum input/output unit
          size' value in mtdinfo
          -> Sub Page shift is zero for Serial flashes and [0,2] for Parallel
          flashes
    

For more details:

ubinize --help

Example:

To generate .ubifs image

For OSPI NOR:

$ mkfs.ubifs -r /path/to/directory -o rootfs.ubifs -m 16 -e 262016 -c 219

For OSPI NAND:

$ mkfs.ubifs -r /path/to/directory -o rootfs.ubifs -m 4096 -e 253952 -c 369

To generate .ubi image

For OSPI NOR:

$ ubinize -o rootfs.ubi -m 16 -p 262144 -s 16 -O 64 ubinize.cfg

For OSPI NAND:

$ ubinize -o rootfs.ubi -m 16 -p 262144 -s 4096 -O 4096 ubinize.cfg

For GPMC NAND:

To generate .ubifs image

$ mkfs.ubifs -r /path/to/directory -o rootfs.ubifs <MKUBIFS ARGS>

To generate .ubi image

$ ubinize -o rootfs.ubi <UBINIZE ARGS> ubinize.cfg

Board Name

MKUBIFS Args

UBINIZE Args

AM335X GP EVM

-F -m 2048 -e 126976 -c 5600

-m 2048 -p 128KiB -s 512 -O 2048

AM437x GP EVM

-F -m 4096 -e 253952 -c 2650

-m 4096 -p 256KiB -s 4096 -O 4096

K2E EVM

-F -m 2048 -e 126976 -c 3856

-m 2048 -p 128KiB -s 2048 -O 2048

K2L EVM

-F -m 4096 -e 253952 -c 1926

-m 4096 -p 256KiB -s 4096 -O 4096

K2G EVM

-F -m 4096 -e 253952 -c 1926

-m 4096 -p 256KiB -s 4096 -O 4096

DRA71x EVM

-F -m 2048 -e 126976 -c 8192

-m 2048 -p 128KiB -s 512 -O 2048

AM64 GP EVM

-F -m 4096 -e 258048 -c 3970

-m 4096 -p 256KiB -s 1024 -O 1024

AM62 LP SK

-F -m 4096 -e 258048 -c 3970

-m 4096 -p 256KiB -s 1024 -O 1024

Table: Table of Parameters to use for Building UBI filesystem image

Step 5

Flash rootfs.ubi to rootfs partition

# EVM Linux

$ ubiformat -f rootfs.ubi /dev/mtdX