4.1.13. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux J784s4?¶
If users have a need to move to a different component version (older or newer) because of an existing bug, feature limitations or other reasons, TI will not support the version migration. As a reference, TI provides the list of a few recipes that were updated while integrating the components to the Processor SDK Linux J784s4.
├── QT5:
│ ├──Baseline:
│ │ └──meta-qt5:recipes-qt/qt5/: recipes and patches from community
│ │
│ └──Arago (TI) updates:
│ ├──meta-arago:
│ │ ├──meta-arago-distro/recipes-qt/qt5: recipes update and additional patches
│ │ ├──meta-arago-extra/recipes-qt/examples:local qt5 examples
│ │ ├──meta-arago-distro/recipes-qt/examples:local qt5 examples recipe update and patches
│ │ ├──meta-arago-distro/recipes-core/packagegroups: no changes are expected
│ │ │ ├──packagegroup-arago-qte.bb
│ │ │ ├──packagegroup-arago-tisdk-qte.bb
│ │ │ └──packagegroup-arago-tisdk-qte-sdk-host.bb
│ │ ├──meta-arago-extras\recipes-core\packagegroups: no changes are expected
│ │ │ └──packagegroup-arago-qte-toolchain-target.bb
│ │ │
│ │ ├──meta-arago-distro/conf/layer.conf: No changes needed for QT configurations
│ │ └──meta-arago-distro/conf/distro/arago.conf
│ └──meta-processor-sdk:
│ └──recipes-qt/qt5: additional recipe updates and patches
├──Wayland/Weston:
│ ├──Baseline:
│ │ └──oe-core/meta/recipes-graphics/wayland: recipes and patches from community
│ │
│ └──Arago (TI) updates:
│ ├──meta-arago:
│ │ ├──meta-arago-distro/recipes-graphics/wayland: recipes update and additional patches
│ │ ├──meta-arago-extras/recipes-graphics/wayland/wayland-protocols
│ │ ├──meta-arago-distro/recipes-graphics/wayland/wayland-ivi-extension: wayland-ivi recipes
│ │ ├──meta-arago-distro/recipes-graphics/wayland/weston-conf: weston configuration
│ │ └──meta-arago-distro/conf/distro/arago.conf: DISTRO_FEATURES
Note: There are many modules that depend on wayland. For example: chromium-wayland, qt5/qtwayland, gstreamer1.0-plugins-bad(waylandsink), glmark2 and gtk+3
├──SGX (Not recommended to modify):
│ ├──Baseline:
│ │
│ ├──meta-ti:
│ │ ├──recipes-graphics/libgles/ti-sgx-ddk-um_<version>
│ │ └──recipes-bsp/powervr-drivers/ti-sgx-ddk-km_<version>
│ │
│ ├──meta-arago:
│ │ ├──meta-arago-extras/recipes-graphics/img-pvr-sdk
│ │ ├──meta-arago-distro/recipes-tisdk/ti-tisdk-makefile/ti-tisdk-makefile/Makefile_ti-sgx-ddk-km
│ │ └──meta-arago-distro/conf/distro/include/arago-prefs.inc: define virtual/egl, virtual/libgles1 and virtual/libgles2
│ │
│ │ Note: There are many modules that depend on sgx, but that does not affect sgx update.
│ │
│ └──Arago (TI) updates:
│ └──meta-processor-sdk:
│ └──recipes-graphics/libgles/ti-sgx-ddk-um_version: for non-sgx build only
├──Gstreamer:
│ ├──Baseline:
│ │
│ ├──meta-openembedded:
│ │ └──meta-multimedia/recipes-multimedia/gstreamer-0.10: recipes and patches from community
│ │
│ │
│ ├──oe-core:
│ │ └──meta/recipes-multimedia/gstreamer: recipes and patches from community
│ │ ├──gstreamer1.0-plugins-base
│ │ ├──gstreamer1.0-plugins-bad
│ │ ├──gstreamer1.0-plugins-good
│ │ ├──gstreamer1.0-plugins-ugly
│ │ └──gstreamer1.0-libav
│ │
│ └──Arago (TI) updates:
│ └──meta-arago:
│ ├──meta-arago-extras/recipes-multimedia/gst-plugins-ti: TI-specific recipes for TI plugins
│ ├──meta-arago-extras/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad: recipes update and additional patches
│ ├──meta-arago-distro/conf/distro/arago.conf: configuration
│ └──meta-arago-distro/recipes-core/packagegroups/packagegroup-arago-tisdk-multimedia-sdk-target.bb: package
If users wish to learn more about Yocto project or Arago build, please refer to the below video link and the documentation on Building Processor SDK Linux through Yocto.