2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) for Linux provides a fundamental software platform for development, deployment and execution of Linux based applications and includes the following:
- Bootloaders, Linux Kernel & Filesystem
- SDK installer & Prebuilt Binaries
- Setup scripts
- Demo applications
- Documentation
Note
For building some of the RTOS-based demonstrations, you should also download Processor SDK RTOS installer. For more information, refer to <PSDKRA install path>/index.html.
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below. In addition, see Processor SDK Linux GPLv3 Disclaimer.
2.1.3. Documentation¶
- Processor SDK Linux Software Developer’s Guide: Provides information on features, functions, delivery package and, compile tools for the Processor SDK Linux release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Processor SDK Linux Getting Started Guide: Provides information on getting the software and running examples/demonstrations bundled in the SDK.
- Software Manifest: Provides license information on software
included in the SDK release. This document is in the release at
[INSTALL-DIR]/docs. - EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Supported Platforms¶
See here for a list of supported platforms and links to more information.
2.1.5. Release 08.06.01¶
This is a patch release on top of 8.6 Release.
Released April 2023
What’s New
Processor SDK 8.6.1 Release supports the following platforms:
- J721E
- J7200
- J721S2
- J784S4
Processor SDK 8.6.1 Release has following new bug fixes:
- U-Boot fix to avoid race condition
- Firmware updates for J721S2/J784S4 to Enable read access of SA3UL MMR region for HSM core
Processor SDK 8.6 Release supports the following platforms:
- J721E
- J7200
- J721S2
- J784S4
- AM68A
- AM69A
Processor SDK 8.6 Release has following new features:
- AM68A-sk and AM69A-sk HS-FS support
- Fusion 1 board for supporting multi-camera capture for Edge AI applications
- Replay Protected Memory Block (RPMB) access in OP-TEE userspace through eMMC RPMB
- SPI Master/Slave
- J7200 stability improvements
2.1.6. Build Information¶
2.1.6.1. U-Boot¶
Note:
Note:
2.1.6.2. Kernel¶
Linux Kernel
Real Time (RT) Linux Kernel
Note:
2.1.6.3. Yocto¶
meta-ti
meta-arago
meta-psdkla
2.1.7. Issues Tracker¶
2.1.7.1. Issues opened in previous releases that were closed on this release¶
| Record ID | Title | Platform |
|---|---|---|
| LCPD-29636 | TDA4VH: multi thread mutex usage causes kernel crash | j784s4-evm |
| LCPD-28317 | GStreamer pipeline with decoder and fakesink causes kernel crash | j721e-evm,j721e-hsevm |
| LCPD-28256 | Wave5: H264/265 Encoded file produces extra green garbage data on width | j721s2-evm |
| LCPD-28255 | Wave5: Decode fails for Dynamic resolution change in input stream | j721s2-evm |
| LCPD-25598 | Wave5: Dynamic SRAM configuration in upstream driver | j721s2-evm |
| LCPD-25332 | J721e Failing Video test | j721e-idk-gw |
| LCPD-28432 | DRA821: PCIe: Segmentation fault | j7200-evm |
| LCPD-29714 | iperf hangs during crypto performance testing | j721e-idk-gw |
| LCPD-29696 | SERDES driver not being probed in U-Boot | j721e-evm,j7200-evm |
| LCPD-29554 | EEPROM Header Unidentified Board | j721e-idk-gw,j7200-evm |
| LCPD-29402 | tftp download in U-Boot fails on am64xx-evm1@eptf124 | am64xx-evm,j721e-idk-gw,j7200-evm |
| LCPD-28889 | j721s2: GPIO Interrupts are broken | j721s2-evm |
| LCPD-26728 | J721e: Watchdog reset fails on newer SoMs | j721e-idk-gw,j721e-sk |
| LCPD-29599 | Stream_1 benchmark executable missing | j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm |
| LCPD-28259 | Wave5: V4l2 driver Multi stream support | j721s2-evm |
| LCPD-28257 | Wave5: Video looping does not work with H264/265 Decoder | j721s2-evm |
| LCPD-22972 | j721e-idk-gw GLBenchmark GLB25_EgyptTestStandardOffscreen_inherited test | j721e-idk-gw |
| LCPD-28756 | J7AHP - Enable ultra high speed mode for SDIO/MMC | j784s4-evm |
| LCPD-28485 | j7200: Segmentation fault during reload PCIe driver. | j7200-evm |
| LCPD-28433 | PCIe EP: DMA test fail | j721s2-evm |
| LCPD-25263 | j721s2-evm: U-Boot USBHOST: Superspeed test is failing | j721s2-evm |
| LCPD-25112 | Ethernet driver not gating its clock when interface is down | am64xx-evm,j721e-idk-gw |
| LCPD-22413 | Hyperflash tests fail ~50% of the time on j7200 | j7200-evm |
| LCPD-17113 | [Cpsw9g][VirtualDriver][VirtualMAC] rpmsg_kdrv_switch is not autoloaded | j721e-idk-gw |
| LCPD-29694 | gpio-line-names is limited to 100. it should be ti,ngpios | am62axx_sk-fs,am62xx-sk,am64xx-sk,am654x-idk,dra71x-evm,dra7xx-evm,j784s4-evm |
| LCPD-29646 | Failure logs during boot: Failed to get MSI domain | am62xx-sk,j721e-idk-gw |
| LCPD-29645 | MMC: SD Card doesn’t go into SDR104 mode | j784s4-evm |
| LCPD-29528 | k3: integration: sdk: missing tag info for optee and atf projects | am62xx-sk,am64xx-evm,am64xx-hsevm,am64xx-sk,am64xx-hssk,j721e-idk-gw,j721s2-evm,j721s2-hsevm,j7200-evm,j7200-hsevm,j784s4-evm |
| LCPD-29524 | j721: sdhci0: Capabilities offered in U-Boot Vs Kernel dts are different | j721e-idk-gw |
| LCPD-27886 | USART: Erroneous clear/trigger of timeout interrupt | am62axx_sk-fs,am62xx-sk,am64xx-evm,j721e-idk-gw,j7200-evm,j784s4-evm,j784s4-hsevm |
| LCPD-18860 | isolcpus in the command line is not honored | am654x-evm,am654x-idk,j721e-idk-gw,j7200-evm |
| LCPD-22954 | DRM Stress Test fails | am62xx-lp-sk,am62xx_lp_sk-fs,am62xx-sk,am654x-evm,j721e-idk-gw,j721s2-evm,j721s2-hsevm,j784s4-evm |
| LCPD-25663 | Remove old IMG demo binaries | am62xx-sk,j721e-evm,j721s2-evm,j784s4-evm |
2.1.7.2. Issues found and closed on this release that may be applicable to prior releases¶
| Record ID | Title | Platform |
|---|---|---|
| LCPD-32462 | Documentation: List of supported Ubuntu versions link is broken | j721e-evm-ivi,j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm |
| LCPD-32335 | SDK: J784S4: Kernel crashes when am65_cpts_disable() is invoked for MAIN CPSW CPTS | j784s4-evm,j784s4-hsevm |
| LCPD-29931 | Missing CPSWnG Native Driver Section in User Guide | j721e-evm-ivi,j721e-idk-gw,j721e-sk,j7200-evm |
| LCPD-32460 | J7200/J7VCL: Linux crash when we cat pinctrl debugfs node | j7200-evm |
| LCPD-32292 | Docs: J784S4: No information on Linux boot flow | j784s4-evm |
| LCPD-29894 | Interrupt Values for adc are incorrect in dts | j721s2-evm,j784s4-evm |
| LCPD-29737 | J7200: Watchdog reset test fails | j7200-evm |
| LCPD-32515 | OV5640: LI OV5640 module fails to probe | am68_sk-fs,am69_sk-fs,j721e-sk,j721s2-evm,j784s4-evm |
| LCPD-32703 | Fusion, CSI Camera overlays missing in rootfs for J7200, J721E, J721S2 | j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm |
| LCPD-32692 | J7200: am65xx: CPSW Checksum Offload Support: Test skipped | j7200-evm |
| LCPD-32493 | J7200: USB CDC ECM class device fails | j7200-evm |
| LCPD-32472 | J7200: CPSW5G Virtual Eth PING Tests fail | j7200-evm,j7200-hsevm |
| LCPD-29885 | Fix DTC Warnings: J784S4 USXGMII Overlays | j784s4-evm,j784s4-hsevm |
| LCPD-29732 | SDK: MDIO: DaVinci driver probe incorrectly deferred | j784s4-evm,j784s4-hsevm |
| LCPD-32654 | uboot watchdog, ESM, PMIC test tracing RC4 | j7200-evm |
| LCPD-32557 | MCSPI Test failing due to missing configs | j7200-evm |
| LCPD-32494 | J7200: U-boot shows multiple ti_sci message not acknowledged warnings | j7200-evm |
| LCPD-29900 | k3: allmod config fails to build due to ti sci kconfig | am62xx-sk,am64xx-evm,am64xx-sk,j721e-idk-gw |
| LCPD-29740 | j721e-idk-gw: EMMC_DD_RW_500M test fail | j721e-idk-gw,j7200-evm |
| LCPD-29729 | j721e-idk-gw, j7200-evm MMC_M_MODULAR_SDHC_MULTI tests fail | j721e-idk-gw,j7200-evm |
| LCPD-32467 | tidss: Incorrect pixel format definitions | am62xx-lp-sk,am62xx_lp_sk-fs,am62xx-sk,j721e-idk-gw,j721s2-evm,j721s2-hsevm,j784s4-evm,j784s4-hsevm |
| LCPD-29883 | Test to update bootloader in mmc using dfu failing | j721s2-evm |
| LCPD-29866 | j721e-idk-gw: MMC_M_FUNC_SDHC_EXT2_DD_RW_1G Failing | j721e-idk-gw |
2.1.7.3. Errata Workarounds Available in this Release¶
| Record ID | Title | Platform |
|---|---|---|
| LCPD-19965 | OSPI PHY Controller Bug Affecting Read Transactions | am64xx-evm,am654x-idk,j721e-idk-gw,j7200-evm |
| LCPD-19047 | USB: Race condition while reading TRB from system memory in device mode | j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw |
| LCPD-17220 | U-Boot Hyperbus: Hyperflash reads limited to 125MHz max. frequency | j721e-idk-gw |
| LCPD-16605 | MMC: MMC1/2 Speed Issue | j721e-evm,j721e-evm-ivi,j721e-idk-gw |
| LCPD-27886 | USART: Erroneous clear/trigger of timeout interrupt | am62axx_sk-fs,am62xx-sk,am64xx-evm,j721e-idk-gw,j7200-evm,j784s4-evm,j784s4-hsevm |
| LCPD-22544 | DDR: LPDDR4 should be configured to 2666 MT/S | j7200-evm |
| LCPD-19068 | DSS: Disabling a layer connected to Overlay may result in synclost during the next frame | j721e-evm,j721e-evm-ivi,j721e-idk-gw |
2.1.7.4. U-Boot Known Issues¶
| Record ID | Title | Platform | Workaround |
|---|---|---|---|
| LCPD-32697 | Failed to get DHCP address in U-Boot | j784s4-evm | |
| LCPD-29852 | j784s4-evm: SD card not recognized in U-Boot when booting over UART | j784s4-evm | |
| LCPD-29891 | u-boot: USB storage device detection failed on j7200 | j7200-evm | |
| LCPD-22512 | Update dfu_alt_info_ospi to include flashing of PHY tuning data | j721e-evm,j7200-evm | |
| LCPD-17789 | UBOOT J7: Could not see UFS device by scsi scan | j721e-idk-gw | |
| LCPD-24824 | J7200/VCL: u-boot SPL code configuring the SOC DDR PLL (PLL12) incorrectly. Desired boot frequency is 27.5 MHz | j7200-evm | Hardcode desired DDR freq in function k3_ddrss_init_freq of u-boot |
| LCPD-22904 | U-boot: Update EMIFtool for i2244:DDR: Valid stop value must be defined for write DQ VREF training | j721e-idk-gw,j7200-evm | |
| LCPD-17523 | A72-SPL - Support to dump EEPROM to shared memory | j721e-evm,j721e-idk-gw,j7200-evm | |
| LCPD-32695 | J784S4 : U-boot : Mass storage tests failure | j784s4-evm | |
| LCPD-32726 | Test: U-Boot: Support Octal SPI(OSPI) flash devices (AHP) RC 6 SDK 8.6 | j784s4-evm | |
| LCPD-24108 | U-Boot: TISCI config ring fail traces seen in OSPI boot mode on J721E | j721e-evm,j721e-evm-ivi,j721e-idk-gw | |
| LCPD-32721 | U-boot DFU mode is not functional | j7200-evm | |
| LCPD-32660 | J721S2: U-boot shows a ti_sci message not acknowledged warning. | j721s2-evm,j721s2-hsevm |
2.1.7.5. Linux Known Issues¶
| Record ID | Title | Platform | Workaround |
|---|---|---|---|
| LCPD-32580 | J7200: System benchmarking tests are failing | j7200-evm | |
| LCPD-27522 | Multi Stream decode fails | j721e-idk-gw | |
| LCPD-29521 | R5 remote proc load does’nt guarentee CPU0 vs CPU1 sequencing | j721e-evm,j784s4-evm | |
| LCPD-28791 | AHP GFX performance regression compaired to AEP | j784s4-evm,j784s4-hsevm | |
| LCPD-28511 | GPU cache coherency issues | j721e-evm,j721e-hsevm,j721s2-evm,j721s2-hsevm,j784s4-evm,j784s4-hsevm | |
| LCPD-32430 | OpenSSL Crypto Perf Intermittent Failure | j784s4-evm | |
| LCPD-19497 | J7200: CPSW2g: interface goes up and down sporadically | j7200-evm | Seen only on very few EVMs. No workaround. |
| LCPD-17814 | Kingston 16G card could not boot to uboot prompt | j721e-idk-gw | |
| LCPD-32794 | j7200: wkup_pmx: Offsets of the pinctrl nodes under the wkup_pmx2 are wrong | j7200-evm | |
| LCPD-32365 | J7200: Audit pinmux node for correct sizes | j7200-evm | |
| LCPD-32363 | ATF: Address ARM Errata 854172 | j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j7200-evm,j7200-hsevm,j784s4-evm,j784s4-hsevm | |
| LCPD-29949 | [PROD STOP]I2c operations at 100KHz is broken | am62xx-sk,am62xx_sk-fs,am62xx_sk-se,j721e-idk-gw | |
| LCPD-29705 | J7200: DT compile time warnings | j7200-evm | |
| LCPD-32609 | J784S4: Sync flip test fails for resolution>2k | j784s4-evm | |
| LCPD-32448 | j721s2: display: eDP mode fails colorbar test | j721s2-evm | |
| LCPD-29525 | Documentation for MCAN missing in the SDK | j7200-evm,j7200-hsevm | |
| LCPD-28645 | K3conf wrong frequencies | j721e-idk-gw | |
| LCPD-29721 | SDK: Linux: Kernel crashes with Intel PCIe WiFi Card | j721e-evm,j721e-idk-gw | |
| LCPD-32468 | CMA allocation in higher memory (32bit+) fails | j721e-idk-gw,j721s2-evm,j784s4-evm | |
| LCPD-29680 | vxe_enc_probe warning observed while booting with debug options enabled | j721e-evm,j721e-evm-ivi,j721e-idk-gw,j7200-evm | |
| LCPD-29634 | Need to include codec maximum capabilities in SDK documentation | j721s2-evm | |
| LCPD-29620 | IMG Decoder not passing ITU-T Streams | j721e-idk-gw | |
| LCPD-29320 | The H.264 profile in the IMG video encoder driver is hardcoded to Base profile. | j721e-idk-gw | The following 2 patches enables the user to provide user defined profile for the video encoding using Gstreamer. Board: J721e (TDA4VM) SDK Version: 8.4 Patch-1: To be applied to Gstreamer plugin. Patch file Name: 0001-Added-H264-profiles-support-to-Gstreamer-Plugin-for-.patch In order to apply the patch, the user needs to have a Yocto setup and for setting up Yocto, please refer to SDK Documentation. Once the Yocto build is ready, the Gstreamer plugin is found at the location: <path-to-J721e-8.4-sdk>/yocto-build/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/gstreamer1.0-plugins-good/1.16.3-r0.0.arago3_psdkla_0/gst-plugins-good-1.16.3 The patch can be applied from this folder and changes are made to the files: ./sys/v4l2/gstv4l2h264enc.c and ./sys/v4l2/gstv4l2h264enc.h Patch-2: To be applied to Linux Kernel Patch file name: 0001-Added-H264-Profiles-Support-to-IMG-Video-encode-driv.patch Location of Linux Kernel: ./ti-processor-sdk-linux-j7-evm-08_04_00_11/board-support/linux-5.10+gitAUTOINC+95b90aa828-g95b90aa828 Apply the patch from this folder and changes are made to the file: ./drivers/media/platform/vxe-vxd/encoder/vxe_v4l2.c ./drivers/media/platform/vxe-vxd/encoder/vxe_enc.c Once both the patches are applied, the driver can be verified by the below command. Use profile=0 for Base, profile=2 for Main, profile=4 for High. For any other value, default Base profile is set. $ gst-launch-1.0 videotestsrc pattern=ball do-timestamp=true num-buffers=100 ! video/x-raw, format=NV12, width=852, height=480, framerate=30/1 ! v4l2h264enc profile=2 ! h264parse ! mp4mux ! filesink location=demo_main.mp4 Profile of the file can be verified using ffmpeg |
| LCPD-25619 | Wave5: Encoded output, mplayer warnings | j721s2-evm | |
| LCPD-17138 | Kernel warning reported during h264 video encode operations | j721e-idk-gw | |
| LCPD-25322 | Docs: J7200: Improve the IPC chapter for ti-rpmsg-char | j7200-evm | |
| LCPD-25321 | Docs: J721E: Improve the IPC chapter for ti-rpmsg-char | j721e-evm,j721e-evm-ivi,j721e-idk-gw | |
| LCPD-24456 | Move IPC validation source from github to git.ti.com | am335x-evm,am335x-hsevm,am335x-ice,am335x-sk,am43xx-epos,am43xx-gpevm,am43xx-hsevm,am437x-idk,am437x-sk,am571x-idk,am572x-idk,am574x-idk,am574x-hsidk,am57xx-evm,am57xx-beagle-x15,am57xx-hsevm,am62axx_sk-fs,am62xx-sk,am62xx_sk-fs,am62xx_sk-se,am62xx-vlab,am62xx-zebu,am64xx-evm,am64xx-hsevm,am64xx-sk,am654x-evm,am654x-idk,am654x-hsevm,beaglebone,bbai,beaglebone-black,dra71x-evm,dra71x-hsevm,dra72x-evm,dra72x-hsevm,dra76x-evm,dra76x-hsevm,dra7xx-evm,dra7xx-hsevm,j7ae-evm,j7ae-zebu,j7aep-zebu,j7am-evm,j7am-vlab,j7am-zebu,j7amp-vlab,j7amp-zebu,j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j721e-sk,j721e-vlab,j721s2-evm,j721s2-hsevm,j7200-evm,j7200-hsevm,j7amp-evm,k2e-evm,k2e-hsevm,k2g-evm,k2g-hsevm,k2g-ice,k2hk-evm,k2hk-hsevm,k2l-evm,k2l-hsevm,omapl138-lcdk | |
| LCPD-17284 | remoteproc/k3-r5: Cores are started out-of-order when core 0 file size >> core 1 file size | j721e-evm,j721e-evm-ivi,j721e-idk-gw | |
| LCPD-16545 | remoteproc/k3-r5f: PDK IPC echo_test image fails to boot up in remoteproc mode on second run | j721e-evm,j721e-evm-ivi,j721e-idk-gw | |
| LCPD-16535 | remoteproc/k3-dsp: PDK IPC echo test binaries fails to do IPC in remoteproc mode on second run | j721e-evm,j721e-evm-ivi,j721e-idk-gw | |
| LCPD-25662 | Remove SGX PVR tools from KS3 devices | am62xx-sk,am62xx_sk-fs,am62xx_sk-se,j721e-evm,j7200-evm | |
| LCPD-25221 |
|
j721e-idk-gw | |
| LCPD-22921 | j721e PVR profiling with PVRPerfServer test is failing | j721e-idk-gw | |
| LCPD-19894 | UYVY texture test fails due to internal data stream error | j721e-idk-gw,j721s2-evm,j784s4-evm | |
| LCPD-26692 | Hardware + Software IPSec Performance Test Failures | am335x-evm,am43xx-gpevm,am57xx-evm,am64xx-evm,j721e-idk-gw | |
| LCPD-24127 | AM654x IPSEC Software Crypto tests fail (Impact 4) | am654x-evm,j721e-idk-gw | |
| LCPD-32784 | Automated Test: J784S4: CPSW Ping fails | j784s4-evm,j784s4-hsevm | |
| LCPD-32725 | [Cpsw9g][VirtualDriver][VirtualMAC]Netdev driver should support operate as a virtual driver that interacts with switch firmware via IPC (AHP) RC 6 SDK 8.6 | j784s4-evm | |
| LCPD-32702 | J784S4 : USB Client : CDC ECM test failures | j784s4-evm | |
| LCPD-32701 | J7200 : USB Client : Mass storage performance tests failure | j7200-evm | |
| LCPD-32700 | Test: MCSPI loopback tests failing for all J7 Platforms | j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm | |
| LCPD-32699 | Test: CPSW Virtual Net driver: Ping test fails since interface is not up | j7200-evm | |
| LCPD-32565 | Serror while pcie bus scan | j721e-idk-gw | |
| LCPD-32564 | Failed to set irq type to MSI | j7200-evm | |
| LCPD-32563 | PCIe write test failed | j7200-evm | |
| LCPD-32542 | Failed to set irq type to MSI-X | j7200-evm | |
| LCPD-32471 | J7200: CPSW5G Virtual Eth Driver Performance Measurement | j7200-evm,j7200-hsevm | |
| LCPD-32334 | V4L2 driver compliance test is failing | j721e-idk-gw,j721e-sk,j721s2-evm,j784s4-evm | |
| LCPD-28087 | emmc: using RPMB panicks the TA on High speed mode | j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw | |
| LCPD-25304 | J7AEP: USB: USB 3.0 devices not getting enumerated in high speed | j721s2-evm | |
| LCPD-24725 | PCIE RC Link fails when linux prints are made quiet | j721e-idk-gw | |
| LCPD-24690 | Kernel: SDK: Set HIGH_SPEED_EN for MMC1 instance | am62xx-sk,am62xx_sk-fs,am62xx_sk-se,am64xx-evm,am64xx-sk,j721s2-evm,j7200-evm | |
| LCPD-24491 | Docs: MMC/SD supported modes not documented properly for J721E/J7200 | j721e-evm,j721e-evm-ivi,j721e-idk-gw,j7200-evm | |
| LCPD-22905 | UDMA: TR15 hangs if ICNT0 is less than 64 bytes | am654x-evm,j721e-idk-gw | |
| LCPD-20240 | MMC Modular testcase regression | j721e-idk-gw,j721e-sk | |
| LCPD-19659 | Doc: PCIe: Update documentation to indicate how to move to compliance mode | j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j7200-evm,j7200-hsevm | |
| LCPD-19499 | Kernel: OSPI write throughput is less than 1MB/s | j7200-evm,j7200-hsevm | |
| LCPD-19084 | Few SD cards not enumerating in Kernel with Alpha EVM | j721e-idk-gw | |
| LCPD-17421 | CPSW9G: Can’t bring up interface over NFS | j721e-idk-gw | |
| LCPD-17172 | Uboot USBhost: Sandisk Extreme USB 3.0 msc stick could not be detected at second time | j721e-idk-gw | |
| LCPD-17171 | Uboot dhcp occasionally failed | j721e-idk-gw | |
| LCPD-16640 | PCIe RC: GIC ITS misbehaves when more than 4 devices use it simultaneously | j721e-idk-gw | |
| LCPD-16396 | J721E: RC: Unsupported request in configuration completion packets results in an abort | j721e-evm,j721e-evm-ivi,j721e-idk-gw | Workaround for Multifunction: Configure all the physical functions supported by the endpoint. For configuring all the 6 functions of PCIe controller instance ‘1’ in J721E, the following can be used. mount -t configfs none /sys/kernel/config; cd /sys/kernel/config/pci_ep/; mkdir functions/pci_epf_test/func1; echo 0x104c > functions/pci_epf_test/func1/vendorid; echo 0xb00d > functions/pci_epf_test/func1/deviceid; echo 1 > functions/pci_epf_test/func1/msi_interrupts; echo 16 > functions/pci_epf_test/func1/msix_interrupts; ln -s functions/pci_epf_test/func1 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func2; echo 0x104c > functions/pci_epf_test/func2/vendorid; echo 0xb00d > functions/pci_epf_test/func2/deviceid; echo 1 > functions/pci_epf_test/func2/msi_interrupts; echo 16 > functions/pci_epf_test/func2/msix_interrupts; ln -s functions/pci_epf_test/func2 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func3; echo 0x104c > functions/pci_epf_test/func3/vendorid; echo 0xb00d > functions/pci_epf_test/func3/deviceid; echo 1 > functions/pci_epf_test/func3/msi_interrupts; echo 16 > functions/pci_epf_test/func3/msix_interrupts; ln -s functions/pci_epf_test/func3 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func4; echo 0x104c > functions/pci_epf_test/func4/vendorid; echo 0xb00d > functions/pci_epf_test/func4/deviceid; echo 1 > functions/pci_epf_test/func4/msi_interrupts; echo 16 > functions/pci_epf_test/func4/msix_interrupts; ln -s functions/pci_epf_test/func4 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func5; echo 0x104c > functions/pci_epf_test/func5/vendorid; echo 0xb00d > functions/pci_epf_test/func5/deviceid; echo 1 > functions/pci_epf_test/func5/msi_interrupts; echo 16 > functions/pci_epf_test/func5/msix_interrupts; ln -s functions/pci_epf_test/func5 controllers/d800000.pcie-ep/; mkdir functions/pci_epf_test/func6; echo 0x104c > functions/pci_epf_test/func6/vendorid; echo 0xb00d > functions/pci_epf_test/func6/deviceid; echo 1 > functions/pci_epf_test/func6/msi_interrupts; echo 16 > functions/pci_epf_test/func6/msix_interrupts; ln -s functions/pci_epf_test/func6 controllers/d800000.pcie-ep/; echo 1 > controllers/d800000.pcie-ep/start; echo 1 > /sys/bus/pci/devices/0000:00:00.0/remove; echo 1 > /sys/bus/pci/rescan; Workaround for switch card: No workarounds available. |
| LCPD-16031 | J721e: PCIe: Legacy interrupts do not work | j721e-evm,j721e-evm-ivi,j721e-idk-gw | |
| LCPD-32656 | AM69-SK: PCIe0 enumeration fails | am69_sk-fs,j784s4-evm,j784s4-hsevm | |
| LCPD-32655 | J784S4: CTRL MMR IO PADCONFIG size is incorrect for wakeup domain | am69_sk-fs,j784s4-evm,j784s4-hsevm | |
| LCPD-32581 | J721E HS: Boot is delayed because of a kernel warning for mmc recovery mode | j721e-hsevm | |
| LCPD-32560 | j7200-evm: FSCK<NNNN>.REC files are sporadically created on the EMMC partition | j7200-evm | |
| LCPD-32539 | J7AEP: Linux crash when we cat pinctrl debugfs node | j721s2-evm,j721s2-hsevm | |
| LCPD-32538 | J7AHP: Linux crash when we cat pinctrl debugfs node | j784s4-evm,j784s4-hsevm | |
| LCPD-32487 | J721S2: CTRL MMR IO PADCONFIG size is incorrect for wakeup domain | am68_sk-fs,j721s2-evm,j721s2-hsevm | |
| LCPD-32474 | k3conf: Unknown silicon for J784S4 | j784s4-evm | |
| LCPD-32279 | k3conf reports J7ES silicon rev version incorrectly | j721e-idk-gw | |
| LCPD-29648 | Failure logs during boot: Failed unmounting /var/lib & /var/volatile | j7200-evm | |
| LCPD-29647 | Non-fatal failure logs seen during system boot up | j7200-evm | |
| LCPD-29644 | MMC: SD Card doesn’t go into DDR50 mode | j784s4-evm | |
| LCPD-28861 | J721e/j7200: MCU/WKUP UART as console. The output gets garbled after sysfw/dm load | j721e-evm,j7200-evm | |
| LCPD-28250 | J7AEP: QSPI Write corrupted when the first operation after powerup is erase | j721s2-evm | |
| LCPD-25692 | linux needs to identify J7ES PG1.1 correctly | j721s2-evm,j721s2-hsevm | |
| LCPD-25686 | k3conf needs to identify J7ES PG1.1 correctly | j721s2-evm,j721s2-hsevm | |
| LCPD-25262 | j721s2-evm : cpuhotplug06 fails | j721s2-evm | |
| LCPD-25195 | j721s2-evm: audio device is not found | j721s2-evm | |
| LCPD-23010 | j721e-idk-gw stress boot test files | j721e-idk-gw | |
| LCPD-22715 | i2232: DDR: Controller postpones more than allowed refreshes after frequency change | am62xx-sk,am62xx_sk-fs,am62xx_sk-se,j721e-idk-gw,j721s2-evm,j7200-evm | Workaround 1: Disable dynamic frequency change by programing DFS_ENABLE = 0: DFS_ENABLE = 0
Workaround 2: If switching frequency, program the register field values as follows: if (old_freq/new_freq >= 7) {
if (PBR_EN==1) { // Per-bank refresh is enabled
AREF_HIGH_THRESHOLD = 19
AREF_NORM_THRESHOLD = 18
AREF_PBR_CONT_EN_THRESHOLD = 1
AREF_CMD_MAX_PER_TREF = 8
}
else { // Per-bank refresh is disabled
AREF_HIGH_THRESHOLD = 18
AREF_NORM_THRESHOLD = 17
AREF_CMD_MAX_PER_TREF = 8
}
} else {
AREF_HIGH_THRESHOLD = 21
AREF_CMD_MAX_PER_TREF = 8
}
|
| LCPD-22319 | OpenSSL performance test data out of bounds | j7200-evm | |
| LCPD-20653 | ltp: kernel syscall tests fail | am335x-evm,am43xx-gpevm,am654x-idk,j721e-idk-gw | |
| LCPD-19792 | j721e boot fails sometimes due to EL1 exception | j721e-idk-gw | |
| LCPD-18258 | IPSEC perfomance failures | am654x-evm,j721e-idk-gw | |
| LCPD-17543 | Some cpuhotplug tests failed | j721e-evm,j721e-evm-ivi,j721e-idk-gw | |
| LCPD-32556 | j721s2: kmstest fails when eDP is used | j721s2-evm | |
| LCPD-24502 | j721e-evm-ivi Universal Planes fails (Impact 1) | j721e-evm-ivi,j721e-idk-gw | |
| LCPD-19068 | DSS: Disabling a layer connected to Overlay may result in synclost during the next frame | j721e-evm,j721e-evm-ivi,j721e-idk-gw | |
| LCPD-17017 | J7: DSS underflows seen on various use cases | j721e-evm-ivi,j721e-idk-gw | |
| LCPD-25583 | H264 Encode followed by decode not working for all resolutions in Gstreamer | j721e-idk-gw | |
| LCPD-16531 | video decode: vxd_dec warnings displayed at end of gstreamer hevc playback to kmssink for certain video | j721e-idk-gw | |
| LCPD-22513 | Update SDK doc to include OSPI flashing instruction using dfu-util | j721e-evm,j7200-evm | |
| LCPD-18790 | eMMC tests failed on J7 rev E2 EVM | j721e-idk-gw | |
| LCPD-32709 | Test: QSPI tests are failing on J721E | j721e-idk-gw | |
| LCPD-29880 | CAN_S_FUNC_MODULAR test fail | am64xx-evm,j7200-evm,j784s4-evm | |
| LCPD-29865 | j721e-idk-gw: MMC_M_MODULAR_NEG_MOD_RW_SDHC Fails | j721e-idk-gw | |
| LCPD-29755 | j721e-idk-gw : Can Transmission and Reception Tests Fail | j721e-idk-gw | |
| LCPD-19743 | Packages.gz is missing | j7200-evm,j7200-hsevm | |
| LCPD-19739 | AM65 shutdown error | am654x-idk,j7200-evm | |
| LCPD-32762 | Delayed detection of HP SD Card on J721s2 | j721s2-evm | |
| LCPD-32722 | Linux SDK VENC: Performance - 1x 1080p60 [Failing on AHP] | j784s4-evm | |
| LCPD-32767 | CI/CD failure | j721s2-hsevm | |
| LCPD-32724 | remote proc booting of C7x in non-SMP mode (AHP) RC 6 SDK 8.6 | j784s4-evm | |
| LCPD-32723 | remote proc booting of C7x in non-SMP mode (AHP) RC 6 SDK 8.6 | am69_sk-fs,j784s4-evm | |
| LCPD-32469 | PVR profiling with PVRPerfServer arm8 64bits failure | j721s2-evm | |
| LCPD-22339 | PCI-E USBCARD, ETHCARD don’t indicate 2-lane support with lspci | j721e-idk-gw,j7200-evm | |
| LCPD-32771 | j721e: doc: Uboot: SD/eMMC build instructions is wrong | j721e-idk-gw,j721e-sk | |
| LCPD-32718 | GPIO_S_FUNC_EDGE_ALL_BANK and GPIO_S_FUNC_DIR_IN_ALL_BANK Test failing in SDK 8.6 | j784s4-evm | |
| LCPD-32708 | J721s2: OSPI: Flash write error during stress test on 8.5 SDK | j721s2-evm | |
| LCPD-32544 | J7200: OSPI Phy calibration fails intermittently | j7200-evm | |
| LCPD-29699 | J721E tidss fails to keep in sync with displays requesting resolutions > 2k | j721e-evm,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j721e-sk |
2.1.7.6. Linux RT Kernel Known Issues¶
There are no known issues in this release in the Linux RT Kernel.
2.1.8. Change Requests¶
2.1. SDK features descoped from 8.6 release¶
| ID | Head Line | Original Fix Version | New Fix Version |
|---|---|---|---|
| JACINTOREQ-5338 | Jacinto PSDK 8.6 AEP/AHP industrial APL pull-in impact | 08.06.00 | 09.00.00 |
2.1. SDK features descoped from 8.5 release¶
| ID | Head Line | Original Fix Version | New Fix Version |
|---|---|---|---|
| JACINTOREQ-5060 | Jacinto networking requirements - CR to 8.6 | 08.05.00 | 08.06.00 |
| JACINTOREQ-4991 | Jacinto Baseport, Graphics, Multimedia CR to 8.6 | 08.05.00 | 08.06.00 |
| JACINTOREQ-5001 | Configurable Buffering Descope | 08.05.00 | None |
| JACINTOREQ-4993 | Descope GLBenchmark | 08.05.00 | None |
| JACINTOREQ-4927 | J7AHP Graphics Scope Modify | 08.05.00 | 08.06.00 |
2.1.9. Installation and Usage¶
The Software Developer’s Guide provides instructions on how to setup your Linux development environment, install the SDK and start your development. It also includes User’s Guides for various Example Applications.