3.8.11. Weston
Weston provides support for many displays in an extended desktop mode and the ability to drag-and-drop windows from one display to the other.
It has support for many backends. By default it will use the drm backend
unless given the WAYLAND_DISPLAY environment variable. This backend will
register the compositor as the controller of the KMS interface and will pick up
human interface device (HID) input by using evdev.
If the WAYLAND_DISPLAY variable is present, Weston will use the wayland
backend for nested composition. This is useful for development, but is normally
not what you want for standard composition use. See
Starting Weston manually or the upstream weston documentation for more
information.
The J722S group of devices actually utilizes two separate
DSS modules enumerated under two different /dev/dri/card* devices.
Weston versions newer than 11.0.91 can specify additional card devices
via the --additional-devices command line parameter when using the
drm backend.
To launch Weston using both card0 and card1, you can use the following command:
# weston --drm-device=card0 --additional-devices=card1
You may also modify the Weston service to have systemd do this automatically
on launch by editing /usr/share/wayland-sessions/weston.desktop and
modifying the Exec line:
[Desktop Entry]
Exec=weston --drm-device=card0 --additional-devices=card1
Please note, however, that Weston cannot use by-path identifiers and consistent naming of DRI devices is not the default behavior.
3.8.11.1. Starting Weston with Emptty
Starting with SDK 11.0, the preferred way to start Weston is with the weston
user, using the display manager emptty. Emptty is a console based display
manager that coordinates the loading of devices with the initialization of any
specified graphical environment. By default it will automatically start
weston under the weston user on device startup.
The definition of the session, including the command used to start it is in
/usr/share/wayland-sessions/weston.desktop. This follows the desktop
entry initialization (INI) format. Some have argued that session entries do not
fully meet the Desktop Entry Specification due to the addition of some new
keys and silent disregard of other keys.
If you need to interact with this instance with any other user, then make sure
that user is capable of interacting with the wayland socket. This will be
wayland-1 under the weston user’s XDG_RUNTIME_DIR,
/run/user/1000/. We do not recommend running graphical applications as
root. See Running Weston clients for more information.
To start the systemd service manually, do the following:
# systemctl start emptty
To inspect the systemd service status, do the following:
# systemctl status emptty
3.8.11.2. Starting Weston manually
To start Weston manually with the DRM backend, do the following:
On the default display:
# weston --display=<default connector-id>
On the secondary display:
# weston --display=<secondary connector-id>
On all connected displays (LCD and HDMI):
# weston
By default, the screen saver timeout will be 300 seconds. The user can change the screen saver timeout using a command line option:
--idle-time=<number of seconds>
For example, to set timeout of 10 minutes and Weston configured to display on all connectors, use the following command:
# weston --idle-time=600
To disable the screen timeout and to configure Weston to display on all connectors, use the following command:
# weston --idle-time=0
If you face any issues with the earlier procedure, see the upstream weston documentation for troubleshooting tips.
The filesystem includes a preconfigured weston.ini file located at
/etc/xdg/weston/weston.ini.
3.8.11.3. Stopping Weston
Stop all Weston clients before exiting Weston. If you have invoked Weston from the serial console, exit Weston by pressing Ctrl-C.
If Weston started automatically through the display manager, then it the following will stop it:
# systemctl stop emptty
It is also possible to start Weston from the native console, exit Weston by pressing Ctrl-Alt-Backspace.
3.8.11.4. Running Weston clients
Weston client examples can run from the command line on a serial port console or an SSH console. After launching Weston, the user should be able to use the keyboard and the mouse for various controls.
The WAYLAND_DISPLAY variable informs clients what socket they should
interact with. Typically these sockets are under the XDG_RUNTIME_DIR,
allowing WAYLAND_DISPLAY to be a file name. The WAYLAND_DISPLAY variable
can also be a full path to the socket.
Applications stated from terminal sessions running under the Weston process will
have this variable set automatically. If it is not set automatically and the
process is running under the same user as Weston, then you should only have to
set WAYLAND_DISPLAY to wayland-X. Here X is the session
number, which should start at 1 and increment for each simultaneous instance of
Weston started.
Do not set the XDG_RUNTIME_DIR variable to any other user’s runtime
directory. This will cause issues with other applications. If that user can
interact with another users socket, point WAYLAND_DISPLAY to the full path
of the socket instead. For example WAYLAND_DISPLAY=/run/user/1000/wayland-1
allows an application to interact with user ID 1000’s session.
# /usr/bin/weston-flower
# /usr/bin/weston-clickdot
# /usr/bin/weston-cliptest
# /usr/bin/weston-dnd
# /usr/bin/weston-editor
# /usr/bin/weston-eventdemo
# /usr/bin/weston-image /usr/share/weston/terminal.png
# /usr/bin/weston-resizor
# /usr/bin/weston-simple-egl
# /usr/bin/weston-simple-shm
# /usr/bin/weston-simple-touch
# /usr/bin/weston-smoke
# /usr/bin/weston-info
# /usr/bin/weston-terminal
3.8.11.5. Running multimedia with Wayland sink
The GStreamer video sink for Wayland is the waylandsink. To use this
video-sink for video playback:
# gst-launch-1.0 playbin uri=file://<path_to_file_name> video-sink=waylandsink
3.8.11.6. Using in-vehicle infotainment shell feature
The SDK also has support for configuring Weston ivi-shell. The default shell in the SDK is the desktop-shell.
To change the shell to ivi-shell, the user will have to add the following lines
into the /etc/xdg/weston/weston.ini.
To switch back to the desktop-shell, comment these lines in the
/etc/xdg/weston/weston.ini (comments begin with a ‘#’ at the start of
line).
[core]
shell=ivi-shell.so
After the earlier configuration, we can restart Weston by running the following command:
# systemctl restart emptty
Note
When Weston starts with ivi-shell, the default background is black, this is different from the desktop-shell that brings up a window with background.
With ivi-shell configured for Weston, a central Human Machine Interface (HMI) manages Wayland client applications and they can use ivi-application protocol to interact with it.
The HMI central controller will assign clients with an unique numeric ID
assuming they support the ivi_application Wayland protocol.
See the following for more information about the Weston IVI-shell:
3.8.11.7. Screenshots
The weston-screenshooter utility allows for fast, full-screen
screenshots. It behaves similarly to any other weston client utility and
requires the WAYLAND_DISPLAY environment variable to point to a valid
Wayland socket. See Running Weston clients for more information.
For most Wayland compositors this would be enough, but Weston requires
additional configuration. Weston does not support the screen capture
protocol, and instead uses an internal helper to fetch and dump active display
contents. Weston only exposes this helper when launched in debug mode. To do
this, add the --debug argument when starting Weston.