2.1. Release Notes

2.1.1. Overview

The Processor Software Development Kit (Processor-SDK) for Linux provides a fundamental software platform for development, deployment and execution of Linux based applications and includes the following:

  • Bootloaders, Linux Kernel & Filesystem

  • SDK installer & Prebuilt Binaries

  • Setup scripts

  • Demo applications

  • Documentation

Note

For building some of the RTOS-based demonstrations, you should also download Processor SDK RTOS installer. For more information, refer to <PSDKRA install path>/index.html.

2.1.2. Licensing

Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below. In addition, see Processor SDK Linux GPLv3 Disclaimer.

2.1.3. Documentation

  • Processor SDK Linux Software Developer’s Guide: Provides information on features, functions, delivery package and, compile tools for the Processor SDK Linux release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.

  • Processor SDK Linux Getting Started Guide: Provides information on getting the software and running examples/demonstrations bundled in the SDK.

  • Software Manifest: Provides license information on software included in the SDK release. This document is in the release at [INSTALL-DIR]/manifest.

  • EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.

2.1.4. Supported Platforms

See here for a list of supported platforms and links to more information.

2.1.5. Release 11.02.01

Released June 2026

What’s New

Processor SDK 11.02.01 Release supports the following platforms:

  • J721E

  • J7200

  • J721S2

  • J784S4

  • J722S

  • J742S2

Processor SDK 11.02.01 Release has following features

  • Fourth 2025 LTS (Linux 6.12 and u-boot 2025.01)

  • ATF v2.13.0+

  • OPTEE 4.7.0

  • Yocto Scarthgap/5.0

  • Bug fixes for errata.

2.1.6. Build Information

2.1.6.1. U-Boot

Head Commit: 1612e4d1deb11d49304c715576854b28cc10e34d: TI: dts: upstream: arm64: ti: Sync dtbs from ti-linux sha 98bbe0d37952
Date: Thu Jun 11 18:38:10 2026 +0530
uBoot Version: 2025.01
uBoot Description: 11.02.15
Repo: git://git.ti.com/ti-u-boot/ti-u-boot.git
Branch: ti-u-boot-2025.01
uBoot Tag: 11.02.15
Compiler Information: arm-oe-eabi-gcc (GCC) 13.4.0, aarch64-oe-linux-gcc (GCC) 13.4.0

Note

meta-edgeai Yocto layer contains additional patches for U-Boot here.

2.1.6.2. Kernel

Linux Kernel

Head Commit: 98bbe0d37952d0ce1b6508f108c357ceb6d58bf3: PENDING: remoteproc: k3-dsp: Add support to suspend attached rprocs
Date: Thu Jun 11 17:56:58 2026 +0530
Kernel Version: 6.12.57
Kernel Description: 11.02.15
Repo: git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git
Branch: ti-linux-6.12.y
Tag: 11.02.15
Non-RT Kernel defconfig: defconfig + ti_arm64_prune.config
RT Kernel defconfig: defconfig + ti_rt.config + ti_arm64_prune.config
Compiler Information: aarch64-oe-linux-gcc (GCC) 13.4.0, GNU ld (GNU Binutils) 2.42.0

Note

meta-edgeai Yocto layer contains additional patches for Kernel here.

2.1.6.3. TF-A

Head Commit: e0c4d3903b382bf34f552af53e6d955fae5283ab: Merge changes from topic “xlnx_fix_gen_con_datatype” into integration
Date : Tue Jul 1 07:01:36 2025 +0000
Version: 2.13

Note

meta-ti Yocto layer contains additional patches for TF-A here.

2.1.6.4. OP-TEE

Head Commit: a9690ae39995af36a31b7a4f446f27ea0787e3a4: plat-k3: drivers: Add TRNG driver support in AM62L
Date : Fri Aug 1 15:40:58 2025 +0530
Version: 4.7.0
Branch: master
Tag: 4.7.0

Note

meta-ti Yocto layer contains additional patches for OP-TEE here.

2.1.6.5. ti-linux-firmware

Head Commit: 59351d453295295909a25a68b30f87e5c85a6e8a: ti-ipc: j721s2/j7200/j784s4/j742s2/j721e/j722s: update ipc binaries
Date: Mon Jun 8 16:45:01 2026 +0530
Branch: ti-linux-firmware
Tag: 11.02.15

2.1.6.6. Yocto

meta-ti

Head Commit: 9859d582984a87b42db107127e829c976f315ee3: CI/CD Auto-Merger: cicd.scarthgap.202606151035
Date: Mon Jun 15 10:35:34 2026 -0500
Branch: scarthgap
Release Tag: 11.02.15

meta-arago

Head Commit: f6dc5e4817c6551ea5250ab1beed6ffc6fc235f2: CI/CD Auto-Merger: cicd.scarthgap.202606151035
Date: Thu Feb 12 15:38:01 2026 -0600
Branch: scarthgap
Release Tag: 11.02.15

meta-tisdk

Head Commit: 8ccd0f212ef01517a9c92f77dfb4da0f4ee0cb65 recipes-graphics: disable emptty for AM62A
Date: Wed Jan 28 00:33:58 2026 -0600
Branch: scarthgap
Release Tag: REL.PSDK.ANALYTICS.11.02.01.02

meta-edgeai

Head Commit: 04db1a86f468b1072eaf72cb723b0d1b76a505ce tisdk-adas-image: Add edgeai-gst-plugins into ADAS_STACK
Date: Sat June 27 01:38:24 2026 -0500
Clone: git://git.ti.com/edgeai/meta-edgeai.git
Branch: scarthgap
Release Tag: REL.PSDK.ANALYTICS.11.02.01.02

2.1.7. Issues Tracker

2.1.7.1. Issues opened in previous releases that were closed on this release

Record ID

Title

Platform

LCPD-45902

J722s/AM67 & AM62P: eDP HPD failure

am62pxx_sk-fs,j722s_evm-fs,j722s_evm-se

LCPD-45771

GPIO PADCONFIG Bits Changing after using gpiod userspace

am62pxx_sk-fs,am62pxx_sk-se,j722s_evm-fs,j722s_evm-se

LCPD-45577

Job_ready false reporting ready state too frequently in Wave5 driver

am62axx_sk-fs,am62pxx_sk-fs,am68_sk-fs,am69_sk-fs,j721s2-evm,j722s_evm-fs,j742s2_evm-fs,j784s4-evm

LCPD-45257

MK-Image tool packaged in U-boot increasing size of u-boot.img

j721e-hsevm,j721s2_evm-se,j722s_evm-se,j784s4-hsevm

LCPD-44298

J722s: MAIN_I2C4 device tree node is missing

j722s_evm-fs,j722s_evm-se

LCPD-42341

Missing Test support to verify order of remotecores being loaded at U-Boot

j7200-evm,j721e-idk-gw,j721s2-evm,j722s_evm-fs,j784s4-evm

LCPD-24654

MCAN: Implement workaround for errata i2279

j7200-evm,j721e-idk-gw,j721s2-evm,j722s_evm-fs,j742s2_evm-fs,j784s4-evm

LCPD-19068

DSS: Disabling a layer connected to Overlay may result in synclost during the next frame

j721e-evm,j721e-evm-ivi,j721e-idk-gw,j721s2-evm,j722s_evm-fs,j742s2_evm-fs,j784s4-evm


2.1.7.2. Issues found and closed on this release that may be applicable to prior releases

Record ID

Title

Platform

LCPD-47654

DDR: Valid VRef range must be defined during LPDDR4 Command Bus Training

j7200-evm,j7200-hsevm,j721e-idk-gw,j721s2-hsevm,j721s2_evm-fs,j722s_evm-fs,j722s_evm-se,j784s4-evm,j784s4-hsevm

LCPD-47605

k3conf tool does not show k3conf ddrbw

j722s_evm-fs

LCPD-47389

USART: Erroneous clear/trigger of timeout interrupt

j7200-evm,j7200-hsevm,j7200_evm-fs,j721e-evm-ivi,j721e-hsevm,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j722s_evm-se,j742s2_evm-fs,j784s4-evm,j784s4-hsevm

LCPD-47381

MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID

j7200-evm,j7200-hsevm,j7200_evm-fs,j721e-evm-ivi,j721e-hsevm,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j722s_evm-se,j742s2_evm-fs,j784s4-evm,j784s4-hsevm

LCPD-46928

gstreamer 1.26.9: v4l2src format negotiation fails with capsfilter constraints

am62axx_sk-fs,am62dxx_evm-fs,am62pxx_sk-fs,am62xx_lp_sk-fs,am62xx_sk-fs,am62xxsip_sk-fs,am68_sk-fs,am69_sk-fs,j721e-idk-gw,j721s2_evm-fs,j722s_evm-fs,j784s4-hsevm

LCPD-46401

Resolve and test the parameters passed to cppi5_trdesc_calc_size() function

am62axx_sk-fs,am62axx_sk-se,am62dxx_evm-fs,am62dxx_evm-se,am62lxx_evm-fs,am62lxx_evm-se,am62pxx-zebu,am62pxx_sk-fs,am62pxx_sk-se,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62xx_p0_sk-fs,am62xx_sk-fs,am62xx_sk-se,am62xxsip_sk-fs,am62xxsip_sk-se,am64xx-evm,am64xx-hsevm,am64xx-hssk,am64xx_evm-se,am64xx_sk-fs,am64xx_sk-se,am654x-evm,am654x-hsevm,am654x-idk,am68_sk-fs,am68_sk-se,am69_sk-fs,bbai64-gp,beagleplay-gp,beagleplay-gp-uart,beagley_ai,j7200-evm,j7200-hsevm,j7200_evm-fs,j721e-evm-ivi,j721e-hsevm,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j722s_evm-se,j742s2_evm-fs,j784s4-evm,j784s4-hsevm


2.1.7.3. Errata Fixes Available Before this Release

Record ID

Title

Platform

ErrataId

LCPD-47389

USART: Erroneous clear/trigger of timeout interrupt

j7200-evm,j7200-hsevm,j7200_evm-fs,j721e-evm-ivi,j721e-hsevm,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j722s_evm-se,j742s2_evm-fs,j784s4-evm,j784s4-hsevm

i2310

LCPD-32351

MMCSD: HS200 and SDR104 Command Timeout Window Too Small

am62axx_sk-fs,am62axx_sk-se,am62pxx_sk-fs,am62pxx_sk-se,am62xx-sk,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62xx_sk-fs,am62xx_sk-se,am62xxsip_sk-fs,am62xxsip_sk-se,am64xx-hsevm,am68_sk-fs,am69_sk-fs,j7200-evm,j721e-idk-gw,j721s2-evm,j722s_evm-fs,j742s2_evm-fs,j784s4-evm

i2312


2.1.7.4. Errata Workarounds Available in this Release

Record ID

Title

Platform

ErrataId

LCPD-47654

DDR: Valid VRef range must be defined during LPDDR4 Command Bus Training

j7200-evm,j7200-hsevm,j721e-idk-gw,j721s2-hsevm,j721s2_evm-fs,j722s_evm-fs,j722s_evm-se,j784s4-evm,j784s4-hsevm

i2160

LCPD-47381

MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID

j7200-evm,j7200-hsevm,j7200_evm-fs,j721e-evm-ivi,j721e-hsevm,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j722s_evm-se,j742s2_evm-fs,j784s4-evm,j784s4-hsevm

i2278

LCPD-24654

MCAN: Implement workaround for errata i2279

j7200-evm,j721e-idk-gw,j721s2-evm,j722s_evm-fs,j742s2_evm-fs,j784s4-evm

i2279

LCPD-19068

DSS: Disabling a layer connected to Overlay may result in synclost during the next frame

j721e-evm,j721e-evm-ivi,j721e-idk-gw,j721s2-evm,j722s_evm-fs,j742s2_evm-fs,j784s4-evm

i2097


2.1.7.5. Errata Rejected as Not Applicable

Record ID

Title

Platform

ErrataId

LCPD-43439

J722S: ROM boot fails for large file sizes

j722s_evm-fs

i2466


2.1.7.6. Open Erratum

Record ID

Title

Platform

ErrataId

LCPD-47799

BCDMA RX_IGNORE_LONG setting in RX CHAN CFG register doesnt work

j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j722s_evm-se,j742s2_evm-fs,j784s4-evm,j784s4-hsevm

i2436


2.1.7.7. U-Boot Known Issues

Record ID

Title

Platform

Workaround

LCPD-44857

j722s_evm-fs: RC-08: Failure: UBOOT : MSC boot shall be supported

j722s_evm-fs

LCPD-38569

j722s: Unable to communicate with MCU R5 and Main R5 when FW loaded from U-Boot

j722s_evm-fs


2.1.7.8. Linux Known Issues

Record ID

Title

Platform

Workaround

LCPD-48097

MCAN: Implement workaround for errata i2279

j7200-evm,j721e-idk-gw,j721s2-evm,j722s_evm-fs,j742s2_evm-fs,j784s4-evm

LCPD-48096

MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID

j7200-evm,j7200-hsevm,j7200_evm-fs,j721e-evm-ivi,j721e-hsevm,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j722s_evm-se,j742s2_evm-fs,j784s4-evm,j784s4-hsevm

Workaround #1: After writing the Tx messages with same Message ID to the Message RAM, request transmission of all these message concurrently by single write access to TXBAR. Make sure none of these messages have a pending Tx request before making the concurrent request. Workaround #2: Use the Tx FIFO instead of dedicated Tx Buffers (set bit MCAN_TXBC[30] TFQM = 0 to use Tx FIFO) for the transmission of several messages with the same Message ID in a specific order.

LCPD-48061

DSS: Disabling a layer connected to Overlay may result in synclost during the next frame

j721e-evm-ivi,j721e-idk-gw,j721s2-evm,j722s_evm-fs,j742s2_evm-fs,j784s4-evm

LCPD-48060

J722s/AM67 & AM62P: eDP random display init failure

am62pxx_sk-fs,j722s_evm-fs,j722s_evm-se

LCPD-48059

J722s/AM67 & AM62P: eDP HPD failure

am62pxx_sk-fs,j722s_evm-fs,j722s_evm-se

LCPD-47981

NFS BOOT Fails while at CORE LINUX FUCNTIONALITY level while running ETHFW standalone code

j722s_evm-fs

LCPD-47918

Kernel crash due to CPSW Tx timeout

j722s_evm-fs

LCPD-47868

When booted in attached mode (IPC does not work after s2r)

j7200-evm,j721s2-evm,j722s_evm-se,j742s2_evm-fs,j784s4-evm

LCPD-47799

BCDMA RX_IGNORE_LONG setting in RX CHAN CFG register doesnt work

j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j722s_evm-se,j742s2_evm-fs,j784s4-evm,j784s4-hsevm

Workaround: RX_IGNORE_LONG is unusable, so remote endpoint such as PDMA should close packet by sending EOP to match TR boundary (PDMA X*Y*Z should match TR ICNT0*ICNT1*ICNT2*ICNT3). If infinite stream is desired (PDMA Z=0) then switch to PKTDMA and use Single Buffer Mode

LCPD-47763

Defects for J7AEN 11.02 release

j722s_evm-fs,j722s_evm-se

LCPD-47749

NFS boot fails when EthFW is enabled on MCU2_0 R5F core due to CPSW Proxy Client driver circular dependency

j722s_evm-fs,j722s_evm-se

LCPD-47686

ETH_CPSW2g_PTP_DUT_TEE is failing in 11.02.13

j722s_evm-fs

LCPD-47393

DWC3 USB should not be configured as a wakeup source by default

j722s_evm-fs,j722s_evm-se

LCPD-47267

J722S: Dual Ethernet port testcases are failing

j722s_evm-fs

LCPD-47223

TEST: RC-07: CPSW: Add test automation support for packet classification based on ALE engine

j722s_evm-fs

LCPD-47220

TEST: RC-07: CPSW: Capability gap for testing XDP tests on j722s

j722s_evm-fs

LCPD-46418

Crypto: cbc and ecb sa2ul self tests fails on few platforms

am62axx_sk-fs,am62pxx_sk-fs,j722s_evm-fs

LCPD-46190

j722s_evm-fs: RC-08: TESTGAP: Linux SDK: CPSW: Native XDP Support + zero copy su…

j722s_evm-fs

LCPD-46120

cpuloadgen testcase fails to run on all cores

j7200-evm,j721e-idk-gw,j721s2-evm,j722s_evm-fs,j742s2_evm-fs,j784s4-evm

LCPD-46058

USBDEV_fullspeed_cdc_ping is failing in 12.00.00.07

am62xxsip_sk-fs,j722s_evm-fs

LCPD-46057

USBDEV_fullspeed_msc_func is failing in 12.00.00.07

j722s_evm-fs

LCPD-46056

USBDEV_highspeed_cdc_ping_zlp is failing in 12.00.00.07

j722s_evm-fs

LCPD-46055

USBDEV_highspeed_msc_enumeration is failing in 12.00.00.07

j722s_evm-fs

LCPD-46054

USBDEV_highspeed_cdc_ncm_ping is failing in 12.00.00.07

j722s_evm-fs

LCPD-46052

USBDEV_highspeed_cdc_ping is failing in 12.00.00.07

j722s_evm-fs

LCPD-46050

USBDEV_fullspeed_cdc_ncm_ping is failing in 12.00.00.07

j722s_evm-fs

LCPD-46049

USBDEV_fullspeed_serial_enumerate is failing in 12.00.00.07

j722s_evm-fs

LCPD-46047

USBDEV_highspeed_serial_enumerate is failing in 12.00.00.07

j722s_evm-fs

LCPD-46045

ETH_CPSW2g_PTP_Switch is failing in 12.00.00.07

am62axx_sk-fs,am62xxsip_sk-fs,j7200-evm,j721e-idk-gw,j722s_evm-fs,j784s4-evm

LCPD-46044

USBDEV_highspeed_msc_slave_perf is failing in 12.00.00.07

j722s_evm-fs

LCPD-46043

ETH_CPSW2g_CBS_DUT_TEE is failing in 12.00.00.07

j722s_evm-fs

LCPD-45969

J722S: Changing DPHY parent refclk breaks USB

am62pxx_sk-fs,j722s_evm-fs

LCPD-45963

OPTEE xtest failures

am62pxx_sk-fs,am64xx-hsevm,am64xx-hssk,j722s_evm-fs

LCPD-45903

J722s/AM67 & AM62P: eDP random display init failure

am62pxx_sk-fs,j722s_evm-fs,j722s_evm-se

LCPD-45253

c7x ipc failure on linux loading remote core firmwares

j722s_evm-fs

LCPD-45239

VTM module sensor reset sequence modification for reliable functionality

am62axx_sk-fs,am62axx_sk-se,am62dxx_evm-fs,am62dxx_evm-se,am62lxx_evm-fs,am62lxx_evm-se,am62pxx-zebu,am62pxx_sk-fs,am62pxx_sk-se,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62xx_p0_sk-fs,am62xx_sk-fs,am62xx_sk-se,am62xxsip_sk-fs,am62xxsip_sk-se,am64xx-evm,am64xx-hsevm,am64xx-hssk,am64xx_evm-se,am64xx_sk-fs,am64xx_sk-se,am654x-evm,am654x-hsevm,am654x-idk,am68_sk-fs,am68_sk-se,am69_sk-fs,j7200-evm,j7200-hsevm,j7200_evm-fs,j721e-evm-ivi,j721e-hsevm,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j722s_evm-se,j742s2_evm-fs,j784s4-evm,j784s4-hsevm

LCPD-44854

Test: Ethernet slave peripheral boot failure

am62pxx_sk-fs,am62xx_lp_sk-fs,am62xx_sk-fs,am69_sk-fs,j722s_evm-fs

LCPD-44841

PCI_S_FUNC_CDNS_MSIX is failing in 12.00.00.07

j722s_evm-fs

LCPD-44505

WDT_RTI: Make the watchdog timeout configurable

j722s_evm-fs,j722s_evm-se

LCPD-43407

IPC Graceful Shutdown on C7x cores

j721e-idk-gw,j721s2-evm,j722s_evm-fs,j784s4-evm

LCPD-43304

CSI RX driver does not consider byterperline parameter in set format

am62axx_sk-fs,am62axx_sk-se,j721e-evm-ivi,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j722s_evm-se,j742s2_evm-fs,j784s4-evm,j784s4-hsevm

LCPD-42843

remoteproc/k3-dsp: PDK IPC echo test binaries fails to do IPC in remoteproc mode on second run

j7200-evm,j721e-idk-gw,j721s2-evm,j722s_evm-fs,j784s4-evm

LCPD-41066

CSI outputs black images when DMA is set to ASEL 15

am62pxx_sk-fs,j722s_evm-fs

LCPD-41044

ARM toolchain used in Yocto build keeps on updating every release

am62axx_sk-fs,am62axx_sk-se,am68_sk-fs,am68_sk-se,am69_sk-fs,j721e-evm-ivi,j721e-hsevm,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j742s2_evm-fs,j784s4-evm,j784s4-hsevm

LCPD-38311

Power off test case failing

j7200-evm,j721e-idk-gw,j721s2-evm,j722s_evm-fs,j742s2_evm-fs,j784s4-evm

LCPD-38267

J722S: tiboot3.bin / R5 SPL within size limit fails to boot

j722s_evm-fs

LCPD-37705

crypto perf failure

am68_sk-fs,j7200-evm,j722s_evm-fs

LCPD-37702

J722S : Crypto perf (ipsec) test failed

j722s_evm-fs

LCPD-37314

NFS in UBOOT on J722S EVM (HS-FS) Fails

j722s_evm-fs

LCPD-34712

OSPI: 2-byte address is not supported in PHY DDR mode

j7200-evm,j721e-idk-gw,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j722s_evm-fs,j722s_evm-se,j742s2_evm-fs,j784s4-evm,j784s4-hsevm

For compatible OSPI memories that have programmable address byte settings, set the amount of address bytes required from 2 to 4 on the flash. This may involve sending a specific command to change address bytes and/or writing a configuration register on the flash. Once done, update the amount of address bytes sent in the controller settings from 2 to 4. For compatible OSPI memories that only support 2-byte addressing and cannot be re-programmed, PHY DDR mode will not be compatible with that memory. Alternative modes include: PHY SDR mode TAP (no-PHY) DDR mode TAP (no-PHY) SDR mode

LCPD-20653

ltp: kernel syscall tests fail

am335x-evm,am43xx-gpevm,am654x-idk,j721e-idk-gw,j722s_evm-fs


2.1.7.9. Issues closed in system firmware in this release

2.1.7.10. System firmware Known Issues

2.1.8. Change Requests

2.1.8.1. SDK features descoped from 11.02 (J722s) release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-9373

Scope Change for LPM Support on J722S

J722S

11.02.00

12.02.00

2.1.8.2. SDK features descoped from 11.02 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-9115

Linux DSS driver to support frame freeze detect

All J7 Platforms

11.02.00

Dropped

JACINTOREQ-8931

J784S4 firewalling support

J784S4,J742S2

11.02.00

Future Release

JACINTOREQ-9146

Low power support on HS-SE/J784S4, R5 as suspend master

J784S4,J7200

11.02.00

11.02.01

2.1.8.3. SDK features descoped from 11.01 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-7915

J7: Support for Kexec/Kdump in Linux

All J7 Platforms

11.01.00

12.00.00

JACINTOREQ-7596

[Linux]: Support for Headless display using QT

J722S,J7ES,J784S4,J721S2

11.01.00

Future Release

2.1.8.4. SDK features descoped from 11.00 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-3987

Linux SDK shall support ADC: 12-bit, 4MSPS analog to digital converter

J784S4

11.00.00

Descoped

JACINTOREQ-5770

U-Boot: support remoteproc load of HSM M4F core

J722S

11.00.00

11.01.00

2.1.8.5. SDK features descoped from 10.01 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-5776

Linux Driver for GPMC - FPGA connection

J722S

10.01.00

Dropped

JACINTOREQ-5138

Linux SDK shall support SA2UL: HMAC using MD5, SHA1, SHA2-224, SHA2-256 and SHA2-512

J784S4, J721E, J721S2, J7200, J722S

10.00.00

11.01.00

JACINTOREQ-5529

Power Management support

J722S

10.01.00

11.01.00

2.1.8.6. SDK features descoped from 10.00 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-7514

Linux SDK shall support MSMC: Security Firewall

J784S4

10.00.00

10.01.00

JACINTOREQ-5042

Linux SDK shall support cpufreq [opp] DFS

J784S4, J721E, J721S2, J7200, J722S

10.00.00

Dropped

JACINTOREQ-4121

Support to boot MCU R5 1_1 in split mode

J784S4, J721E, J721S2, J7200

10.00.00

10.01.00

2.1.8.7. SDK features descoped from 9.2 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-3970

Linux SDK shall support MSMC: Security Firewall

J784S4

09.02.00

10.00.00

JACINTOREQ-5042

AM69/J784S4 Linux SDK shall support cpufreq [opp]

AM69, J784S4

09.02.00

10.00.00

2.1.8.8. SDK features scoped in 9.1 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-3761

Linux SDK shall support RTI: Watchdog support J721S2

J721S2

09.02.00

09.01.00

JACINTOREQ-3981

Linux SDK shall support RTI: Watchdog support J784S4

J784S4

09.02.00

09.01.00

2.1.8.9. SDK features descoped from 9.1 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-3970

Linux SDK shall support MSMC: Security Firewall

J784S4

09.01.00

09.02.00

JACINTOREQ-3920

Linux SDK shall support SA2UL: HMAC using MD5, SHA1, SHA2-224, SHA2-256 and SHA2-512

J784S4

09.01.00

09.02.00

2.1.8.10. SDK features descoped from 9.0 release

ID

Head Line

Platform

Original Fix Version

New Fix Version

JACINTOREQ-3598

Jacinto Device firewalling support

J7200, J721e, J721s2, J784s4

09.00.00

09.01.00

2.1.8.11. SDK features descoped from 8.6 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-5338

Jacinto PSDK 8.6 AEP/AHP industrial APL pull-in impact

J721e, J7200, J721S2 , J784S4

08.06.00

09.00.00

2.1.8.12. SDK features descoped from 8.5 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-5060

Jacinto networking requirements - CR to 8.6

J721S2, J784S4

08.05.00

08.06.00

JACINTOREQ-4991

Jacinto Baseport, Graphics, Multimedia CR to 8.6

J721S2, J784S4

08.05.00

08.06.00

JACINTOREQ-4934

CSI Capture Automated Testing for J7AEP

J721S2

08.05.00

08.06.00

JACINTOREQ-4928

J7AEP Multimedia Scope Modify

J721S2

08.05.00

08.06.00

JACINTOREQ-5001

Configurable Buffering Descope

J784S4

08.05.00

None

JACINTOREQ-4993

Descope GLBenchmark

J784S4

08.05.00

None

JACINTOREQ-4927

J7AHP Graphics Scope Modify

J784S4

08.05.00

08.06.00

2.1.8.13. SDK features scope change for 8.5 release

ID

Headline

Platform

JACINTOREQ-4994

Video Codec Memory Optimization Scope Change

J721e

2.1.8.14. SDK features descoped from 8.4 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-4930

k3conf Doc and Test Modify

J721e

08.04.00

08.05.00

JACINTOREQ-4905

J7AEP Graphics Scope Modify

J721s2

08.04.00

08.05.00/08.06.00

JACINTOREQ-4898

SERDES: PCIe + USB schedule update

J721s2

08.04.00

08.05.00

JACINTOREQ-4864

4k Resolution Scope change

J721s2

08.04.00

08.05.00

JACINTOREQ-4854

McASP Scope Change

J721s2

08.04.00

08.05.00

JACINTOREQ-4930

k3conf Doc and Test Modify

J721s2

08.04.00

08.05.00

2.1.8.15. SDK features descoped from 8.0 release

ID

Headline

Platform

Original Fix Version

New Fix Version

JACINTOREQ-1559

Linux H264 decoder support

J721e

08.00.00

08.01.00

JACINTOREQ-1485

Linux writeback pipeline support

J721e

08.00.00

None

JACINTOREQ-1444

Vision apps inclusion in yocto build

J721e

08.00.00

None

2.1.8.16. SDK features present in 7.0 that were descoped in 7.1

Feature

Comments

Platform

HS support

Restored in 7.3

J721e

SPL/Uboot boot modes restricted to SD card boot mode

Restored in 7.3

J721e

1s Linux boot

J721e

Descope for support of native H264 encode/decode

Use R5F based driver with OpenVX as interface. H.264 decoder support restored in 7.3

J721e

GPU compression

J712e

SA2UL driver optimization

J721e

Display Sharing

Display sharing demo available in SDK v6.1

J721e

Virtualization (Jailhouse hypervisor/IPC virtualization/CPSW9G virtualization)

Does not affect 3P virtualization solutions. Basic Jailhouse demo can be seen in SDK 7.0

J721e

2.1.9. Installation and Usage

The Software Developer’s Guide provides instructions on how to setup your Linux development environment, install the SDK and start your development. It also includes User’s Guides for various Example Applications.


2.1.10. Host Support

For the specific supported hosts for current SDK, see this page.

Note

Processor SDK Installer is 64-bit, and installs only on 64-bit host machine.