3.6.10. GTK+ Graphics Framework
GTK+, or the GIMP Toolkit, is a multi-platform toolkit for creating graphical user interfaces. Offering a complete set of widgets, GTK+ is suitable for projects ranging from small one-off tools to complete application suites.
Please refer to https://www.gtk.org/ for additional details on GTK+.
The PSDK target file system includes the pre-built GTK+ libraries under
/usr/lib for GTK+3 over Wayland support. There is also a comprehensive
GTK+3 demo application (gtk3-demo) under /usr/bin to demonstrate GTK+3
APIs and their usages.
3.6.10.1. Demos
GTK+ will attempt to interact with a windowing system on startup. If one is not running, or it fails to connect to one for any reason, you will see the following error:
(<application-name>:<pid>): Gtk-WARNING **: 21:21:27.361: cannot open display: <display>
If no display value is returned, then you are more than likely missing the
WAYLAND_DISPLAY environment variable. Check the Weston
section for more information.