3.7.6. OpenGL ES
The OpenGL® ES and EGL® libraries packaged with the Processor SDK Linux J721s2 used by graphics stacks such as Wayland/Weston provide accelerated rendering capabilities. The drivers run on an ARM core and program the firmware running inside a GPU core with rendering commands submitted by the user applications.
For more information about OpenGL® ES and EGL® extensions see: