2.3. Yocto Layer Configuration¶
Processor SDK Linux J721s2 uses the ‘oe-layersetup’ tool to configure the meta layers. If you do not have the Linux SDK package installed:
git clone https://git.ti.com/git/arago-project/oe-layersetup.git yocto-build
cd yocto-build
./oe-layertool-setup.sh -f configs/processor-sdk-linux/<Config File>
The Linux SDK package also has the above tool cloned at the top level. If you have it installed:
cd <SDK INSTALL DIR>/yocto-build
./oe-layertool-setup.sh -f configs/processor-sdk-linux/<Config File>
Use below in place of <Config File>, to setup the meta layers for the current release version.
Config File | Description | Supported machines |
---|---|---|
processor-sdk-linux-08_06_00.txt | Processor SDK Linux 08_06_00 Release | j721s2-evm |