3.1.2.5. USB Mass Storage

USB Mass Storage (UMS) functionality, allows a connected USB host to access U-Boot block devices and enable file transfer. This is useful for accessing storage devices such as SD or MMC from a USB host such as host PC.

3.1.2.5.1. Configuration requirements

Set the following configuration in the U-Boot config file to enable UMS support:

CONFIG_CMD_USB_MASS_STORAGE=y

3.1.2.5.2. Usage

To use the UMS command:

=> ums <dev> [<interface>] <devnum[:partnum]>

dev

USB gadget device number.

interface

Interface for accessing block device (MMC, SATA, ….), default is MMC.

devnum

Device number for selected interface.

partnum

Partition number for selected device, default is 0. 0 to expose all partitions.

Example usage:

=> mmc list
mmc@fa10000: 0 (eMMC)
mmc@fa00000: 1 (SD)
=> ums 0 mmc 1
UMS: LUN 0, dev mmc 1, hwpart 0, sector 0x0, count 0x3b72400

This example exposes the SD card (mmc 1) as a USB mass storage device to the connected host PC. The host PC can then mount and access the storage device for file transfer. Press Ctrl+C to exit UMS command and return to the U-boot prompt.

Note

The USB controller must be in peripheral mode for UMS to work. If the controller is in host mode, then reconfigure it to peripheral mode before using the UMS command. The USB controller can be configured to operate in peripheral mode by changing the value of dr_mode property of USB controller node in device tree to peripheral.