2.3. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layertool-setup.sh -f <config>
The following config files are located in the yocto-build/configs/processor-sdk-linux
directory.
Config File | Description | Supported machines |
---|---|---|
processor-sdk-linux-08_01_00.txt | Processor SDK Linux 08_01_00 Release | j7200-evm |