5.1.9. How to flash eMMC and boot from eMMC UDA

5.1.9.1. Overview

This how to guide allows to prepare and flash the eMMC device to boot using MMCSD boot, from eMMC UDA in fs mode.

Note

This process will require a working SD card that can boot the device to Linux kernel.

  • To flash eMMC using a partitioned wic image from the SDK, go here

  • To flash eMMC manually, go here

5.1.9.2. Flash eMMC with disk image

Copy the .wic formatted disk image from the SDK installer to target filesystem, boot the device via SD card boot and at linux prompt, find the eMMC block device as shown here and flash the eMMC as shown below:

root@<machine>:~# ls
tisdk-base-image-<soc>-evm.rootfs.wic.xz
root@<machine>:~# xz -d -k tisdk-base-image-<soc>-evm.rootfs.wic.xz
root@<machine>:~# ls
tisdk-base-image-<soc>-evm.rootfs.wic tisdk-base-image-<soc>-evm.rootfs.wic.xz
root@<machine>:~# umount /dev/mmcblk0*
root@<machine>:~# dd if=tisdk-base-image-<soc>-evm.rootfs.wic of=/dev/mmcblk0

5.1.9.3. Manually flash eMMC device

To boot with MMCSD boot from eMMC UDA in fs mode, the eMMC needs to be prepared before hand. The recommended process is to flash an SD card with TI SDK image, copy the bootlader binaries that will be flashed to eMMC in the SD card “boot” partition in emmc/ folder, boot the board with MMCSD boot from SD (FS mode), and proceed to create disk partitions and flash the eMMC from linux.

Create disk partitions

In Linux, create a “boot” partition to store bootloader binaries as shown here and a “root” partition partition for the rootfs: as shown here.

Format partitions

For the “boot” partition, format as vfat type as shown here and for the “root” partition, format as ext4 type as shown here.

Flash eMMC UDA

Mount the new “boot” partition and copy the bootloader binaries to the new partition as shown here. Mount the new “root” partition and copy the rootfs to the parititon as shown here

5.1.9.4. MMCSD boot configuration from eMMC UDA

Now that we have flashed the eMMC device, reboot the board and stop at u-boot prompt to set configuration for MMCSD boot from UDA.

Enable boot from eMMC UDA

After flashing binaries to eMMC flash, the eMMC device Extended CSD register fields: BUS_WIDTH and PARTITION_CONFIG must be set so ROM will use the correct configuration for MMCSD boot from UDA.

Set using the mmc bootbus and mmc partconf commands. Go to Boot from UDA.

  • The mmc bootbus command sets the BOOT_BUS_WIDTH field where mmc bootbus 0 2 0 0 selects x8 (sdr/ddr) buswidth in boot operation mode.

  • The mmc partconf command can be used to configure what hardware partition to boot from. The general syntax is:

$ mmc partconf <dev> [[varname] | [<boot_ack> <boot_partition> <partition_access>]]

Where <dev> is MMC device index.

  • For more information on these commands, please go here.

Boot from UDA

=> mmc partconf 0 1 7 1
=> mmc bootbus 0 2 0 0

Enable warm reset

On eMMC devices, warm reset will not work if EXT_CSD[162] bit is unset since the reset input signal will be ignored. Warm reset is required to be enabled in order for the eMMC to be in a “clean state” on power-on reset so that ROM can do a clean enumeration. To set the EXT_CSD[162] bit, stop at u-boot prompt and execute the following command:

=> mmc rst-function 0 1

Warning

This is a write-once field. For more information, please refer to the u-boot doc found here.

U-boot environment

The command saveenv is no longer used in TI SDK, thus, the following environment workarounds must be implemented to boot from eMMC UDA.

At u-boot prompt, run the following commands to boot Linux from UDA:

=> setenv mmcdev 0
=> setenv bootpart 0:2
=> boot

Or change the u-boot environment for MMCSD boot to boot completely from eMMC.

First apply the following change in u-boot for any SoC.

diff --git a/board/ti/<soc>/<soc>.env b/board/ti/<soc>/<soc>.env
index 82b9f0741bb..73d59ac425c 100644
--- a/board/ti/<soc>/<soc>.env
+++ b/board/ti/<soc>/<soc>.env
@@ -17,8 +17,8 @@ run_kern=booti ${loadaddr} ${rd_spec} ${fdtaddr}

 boot_targets=mmc1 mmc0 usb pxe dhcp
 boot=mmc
-mmcdev=1
-bootpart=1:2
+mmcdev=0
+bootpart=0:2
 bootdir=/boot
 rd_spec=-

Re-build bootloader binaries and copy build outputs to the SD card “boot” partition and emmc/ folder. Proceed to flash eMMC with these binaries as shown in this step-by-step guide.

5.1.9.5. Boot from eMMC UDA

Finally we can proceed to change boot mode pins to MMCSD boot from eMMC (port 0) in fs mode as per specific TRM, under: Initialization/Boot Mode Pins and power cycle the board.