5. Demo ApplicationsΒΆ
The SDK supports the following Out-Of-Box demo-applications
Use the tisdk-default-image-j784s4-evm to be able to run the above demo applications.
Refer to Hardware EVM Setup for preliminary hardware setup.
Refer to Create SD Card to prepare a SD card with the tisdk-default-image provided in the SDK.
To run a demo refer to the respective user guide from above