4.2.2. AM68 SK Hardware Setup¶
4.2.2.1. AM68 SK¶
AM68 SK is a low cost, small form factor board designed to bring smart cameras, robots and intelligent machines to life. For more information related to the board, full list of peripherals supported, pin settings for boot modes and more visit AM68 SK User guide
To run the demos on AM68 SK you will require,
AM68 SK
Minimum 16GB high performance SD card
External Power Supply or Power Accessory Requirements
USB 2.0 mouse
Full-HD (1080p) HDMI display
Optional 100Base-T Ethernet cable connected to internet
Optional UART cable
Optional USB camera (Any V4L2 compliant 1MP/2MP camera, Eg. Logitech C270/C920/C922)
Nominal Output Voltage: 5-20VDC
Maximum Output Current: 5000 mA
Refer to AM68 SK User guide for more details.
Connect the components to the EVM as shown in the image.
![../../../_images/am68_sk.jpg](../../../_images/am68_sk.jpg)
Fig. 4.1 AM68 SK connections¶
Set the boot pins to SD boot mode as shown in the following image.
![../../../_images/am68_sk_bootpins.jpg](../../../_images/am68_sk_bootpins.jpg)
Fig. 4.2 AM68 SK boot pins¶
4.2.2.2. USB Camera¶
UVC (USB video class) compliant USB cameras are supported by AM68 SK. The driver for the same is enabled in SDK. The SDK has been tested with C270/C920/C922 versions of Logitech USB cameras. Streaming from multiple USB cameras simultaneously is also supported.