3.1.1.12. DDRSS ECC
3.1.1.12.1. Overview
The DDR subsystem (DDRSS) comprises DDR controller, DDR PHY and wrapper logic to integrate these blocks in the device. For SDRAM data integrity, the DDRSS bridge supports inline ECC on the data written to or read from the SDRAM. ECC is stored together with the data so that a dedicated SDRAM device for ECC is not required. The 8-bit single error correction double error detection (SECDED) ECC data is calculated over 64-bit data quanta. For every 256-byte data block 32 bytes of ECC is stored inline. Thus 1/9th of the total SDRAM space is used for ECC storage and the remaining 8/9th of the SDRAM data space are seen as consecutive byte addresses. Even if there are non-ECC protected regions the previously described 1/9th-8/9th rule still applies and consecutive byte addresses are seen from system point of view. AM68 supports up to 3 ECC protected non-overlapping memory ranges. The current U-Boot release supports a single region covering the entire SDRAM space.
ECC is calculated for all accesses that are within the address ranges protected by it. 1-bit error is correctable by ECC, but multi-bit and multiple 1-bit errors are not correctable and will be treated as an uncorrectable error. Any uncorrectable error will cause a bus abort.
3.1.1.12.1.1. DDRSS ECC handling
Note
The ECC feature of DDRSS is not enabled by default in U-Boot.
3.1.1.12.1.1.1. Enabling ECC
The ECC feature of DDRSS can be enabled by the following two steps:
Add
ti,ecc-enableboolean property to thememorycontrollernode// u-boot/arch/arm/dts/k3-*-ddr.dtsi &memorycontroller { power-domains = <&k3_pds 170 TI_SCI_PD_SHARED>, <&k3_pds 55 TI_SCI_PD_SHARED>; clocks = <&k3_clks 170 0>, <&k3_clks 16 4>; ti,ecc-enable; };Re-build U-Boot with
CONFIG_K3_INLINE_ECCenabled# u-boot/configs/*_r5_defconfig CONFIG_PINCTRL_SINGLE=y CONFIG_POWER_DOMAIN=y CONFIG_TI_POWER_DOMAIN=y CONFIG_K3_INLINE_ECC=y CONFIG_K3_SYSTEM_CONTROLLER=y CONFIG_REMOTEPROC_TI_K3_ARM64=y CONFIG_RESET_TI_SCI=y
3.1.1.12.1.1.2. Priming with BIST Engine
The bootloader has the responsibility to pre-load the ECC protected region with known data before functional reads and writes are performed. During the ECC initialization, the R5 SPL fills the entire memory with zeros using the BIST engine in the DDR controller. The BIST engine method allows priming the entire region with zeros in much less time.