5.2.1. J722S EVM Hardware Setup
Description
The J722S evaluation module (or TDA4VEN and AM67 EVM) is a stand-alone test and development platform built around the J722S system-on-a-chip (SoC). J722S processors are comprised of a quad-core 64-bit Arm®-Cortex®-A53 microprocessor, dual-core Arm Cortex-R5F microcontroller (MCU). The EVM gives developers the basic resources needed for most general‐purpose type projects.
J722S EVM
Fig. 5.1 J722S EVM Front
Fig. 5.2 J722S EVM Back
Key Features of EVM
J722S SoC
20V DC nominal supply (Max output current 5A)
1x 8GB LPDDR4 memory
1x Octal‐SPI NOR flash, 512Mb memory
512Mb Octal NAND
eMMC flash memory (32GB memory)
XDS110 Emulator support
1x Display Port Interface (DP0 from eDP bridge)
DVI (v1.0) via HDMI Type A, supports 1080p
4x UART terminals via 1x USB FTDI (UART‐over‐USB)
1x Gigabit Ethernet (RJ45 Connector)
3x CAN Headers, full CAN‐FD support
4x 22‐Pin Flex Cable Interface (CSI‐4L)
2x 40‐pin High Speed Connector
Audio Line in and MIC + Headphone out
USB3.1 (Gen1) Hub to 3x Type A (Host)
USB3.1 (Gen1) Type C (DFP,UFP modes)
USB2.0 Micro B (for Quad UART‐over‐USB Transceiver)
USB 2.0 Micro B (for XDS110)
Expansion and Add-on support
1‐Lane PCIe Card Slot Gen3
Fan Header(12V)
40‐pin Header (2x20)
4x CSI‐RX ports support over QSH connector for Add on Card
LVDS Display connector (OLDI)
DSI Display connector
Refer to EVM connections for detailed information regarding connecting peripherals to the EVM
Switch settings
Bootmodes are selected using the SW3 and SW4 switches on the EVM. Most common boot method is to use SD card. Following are the switch settings to set the boot mode to SD for the EVM.
SW3[1:8] = 1100 0010 SW4[1:8] = 0100 0000
When you want the binaries to be loaded from a debugger like CCS, the common processor boards has to be set in the NO boot mode. Following are the switch settings to do the same.
SW3[1:8] = 1101 111 SW4[1:8] = 0000 0000
EVM connections
Connect Following peripherals for working with processor SDK Linux
USB connector (J6) connect to 4x UART devices that are registered as /dev/ttyUSB[0-3] in your Linux machine.
MAIN_UART and MCU_UART are muxed through the same USB connector(J6). MAIN_UART is /dev/ttyUSB2 and MCU_UART is /dev/ttyUSB0
Connect a Display Port 1080p monitor to the Display0 port of the EVM (J19).
Connect ethernet at the RJ45 connector (J11) in the EVM as shown.
Insert micro SD card at the slot shown in (J38)
Connect the XDS110 connector (J15) if you want to run RTOS demos or use CCS.
Connect a 1080p HDMI monitor to the HDMI port (J19) on the EVM.
Connect a 12V C-type power supply (J24)
Power on the board