4.1. Developer Notes
- 4.1.1. Connect to an EVM via Telnet
- 4.1.2. How to Setup a Samba Server
- 4.1.3. Boot Sequence
- 4.1.4. Moving Files to the Target System
- 4.1.5. How to Flash from U-boot Shell
- 4.1.6. SDK File System Optimization/Customization
- 4.1.7. How to change dtb files
- 4.1.8. How to flash eMMC device and boot from UDA partition
- 4.1.9. How to enable DT overlays in linux
- 4.1.10. How to visualize statistics data
- 4.1.11. How to Use K3Conf Tool
- 4.1.12. Real-Time Linux on TI SoCs
- 4.1.13. How to verify IPC between Linux and MCU R5 in Keystone devices?
- 4.1.14. How to configure K3 MSMC memory for use as SRAM or L3 cache?
- 4.1.15. How to check some device tree information from user-space of Linux?
- 4.1.16. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux AM67?
- 4.1.17. How to Build a Ubuntu Linux host under VMware
- 4.1.18. K3 Resource Partitioning Tool
- 4.1.19. Latest FAQs on TDA4