3.2.2.6. DSS

3.2.2.6.1. Introduction

This page gives a basic description of DSS (Display SubSystem) hardware, the Linux kernel drivers (tidss) and various TI boards that use DSS. The technical reference manual (TRM) for the SoC in question, and the board documentation give more detailed descriptions.

3.2.2.6.2. Supported Devices

There are many DSS IP versions, all of which support slightly different set of features. DSS versions up to 5 are supported by the omapdrm driver, and DSS versions 6 and up are supported by the tidss driver. This document covers DSS6, DSS7-L, and DSS7-UL which are used on the following TI SoCs or SoC families: K2G, AM65x, AM62x, AM62Ax, AM62Px, J721E, J721S2, J784S4.

3.2.2.6.3. Hardware Architecture

The Display Subsystem (DSS) is a hardware block responsible for fetching pixel data from memory and sending it to a display peripheral like an LCD panel or an DisplayPort monitor. DSS hardware can be divided into two major parts:

  • Display Controller (DISPC), which handles fetching the pixel data, doing color conversions, composition, and other pixel manipulation

  • Peripherals, which encode the raw pixel data to standard display signals, like MIPI DPI or DP.

In addition to the SoC’s DSS, boards often contain external display bridges (for example, DPI-to-HDMI bridge) and display panels.

../../../../../_images/DSS7Lite_HW.png

The above image gives an overview of the DSS hardware.

  • The J722S SoC has 2 instances of the DSS7-UL, connected to different display peripherals, inside the SoC.

  • Note: The Video Pipelines from one instance of DSS cannot overlay image planes via the Overlay Managers of another DSS.

The arrows show how pipelines are connected to overlay managers, which are further connected to video-ports, which finally create an encoded pixel stream for display on the LCD or monitor.

3.2.2.6.3.1. Display Controller (DISPC)

DISPC is the block which is responsible for fetching pixel data from the memory through DMA pipelines, and then create a pixel stream for the peripheral. The pixel stream comprises of a composition of one or more image layers which we finally want to present on the display. DISPC can be split into 3 major sub-blocks:

  • Pipelines

  • Overlay Managers (Compositors)

  • Video Ports (Timing generators)

The next three sub-sections provide details on these sub-blocks.

3.2.2.6.3.1.1. Pipelines

Pipelines (or DMA channels) consist of the HW block which performs DMA to fetch image pixels (of different color formats) from RAM. Besides performing DMA, pipelines perform other functions like replication, ARGB expansion, scaling, color conversion, VC1 range mapping on the input pixels before it’s passed on to the overlay manager. An overlay manager receives pixel data from one or more such pipelines, and performs the task of composing them and passing it on to the video-port.

There are two types of pipelines: VIDL and VID. The difference between the two is that VID pipelines support scaling, and VIDL does not. The number of pipelines within DSS varies with the DSS IP version used in the SoC.

3.2.2.6.3.1.2. Overlay Managers (Compositors)

Overlay managers are the blocks which take pixel data from one or more pipelines, layer them to form a composition, and create a pixel stream for the video-ports to consume.

The compositor part takes pixel data from multiple pipelines, composing them on the basis of their position with respect to the complete overlay manager size. Tasks like alpha blending, color-keying and z-order are also performed by the compositor in the overlay manager.

3.2.2.6.3.1.3. Video Ports (Timing generators)

Video ports take a pixel stream from an overlay manager, and encode it into a standard video signal which is understood by the LCD panel/monitor or an internal peripheral (like eDP). These video standards are specified by MIPI or general video/display bodies.

The timing generator part of the video port is responsible for providing the pixel stream generated by the compositor above according to the timings desired by the peripheral. The timing generator is a state machine which provides RGB data along with control signals like pixel clock, hsync, vsync and data enable. This timing info is used by the panel / peripheral to display the composited frame on the screen.

3.2.2.6.3.2. SoC Hardware Description

SoC Family: AM67

DSS version

Outputs

Pipes

Video ports

2x DSS7-UL

OLDI, DPI, DSI

2x VID, 2x VIDL

4

Note that while there are 4 video pipes and ports available, only 3 display streams can be output at any given time, as there are only 3 PLLs that generate independent pixel clocks.

The DSS7 hardware also supports resource sharing across multiple processing cores with separate register region per sub-component and interrupt duplication for each processing core, thus allowing independent context update for the associated pipelines.

../../../../../_images/DSS7_resource_paritioning_HW.png

3.2.2.6.3.3. Supported Features

3.2.2.6.3.3.1. SoC Outputs

  • MIPI DPI
    • Active matrix

    • RGB

    Note: TI EVMs do not provide the DPI signals through a connector, but instead pass the RGB data through an DP/HDMI transmitters on-board. Custom EVMs based on these SoCs can provide such connectors and can use the Active Matrix LCDs.

  • MIPI DSI
    • 4 Lane MIPI DSI output

  • Open LVDS Display Interface (OLDI)
    • Single Link OLDI

    • Dual Link OLDI

    • 2x Single Link Independent OLDI

3.2.2.6.3.3.2. EVM Outputs

  • HDMI Output
    • DPI output from SoC converted to HDMI via HDMI encoders on Starter-Kit (SK) EVMs.

  • Open LVDS Display Interface (OLDI)
    • Single Link OLDI output from the SoC directly.

    • Dual Link OLDI output from the SoC directly.

    • 2x Single Link Independent OLDI output from the SoC directly.

  • MIPI DSI
    • 4 Lane MIPI DSI output from the SoC directly.

    • The connector is compatible with 22 pin RPi DSI Connector.

3.2.2.6.4. Driver Architecture

The driver for DSS6 / DSS7-L / DSS7-UL IPs is tidss. tidss is a Direct Rendering Manager (DRM) driver, located in the directory drivers/gpu/drm/tidss/ in the kernel tree. tidss does not implement any 3D GPU features, only the Kernel Mode Setting (KMS) features, used to display pixel data on a display.

In addition to tidss, there are a number of bridge and panel drivers located in drivers/gpu/drm/bridge/ and drivers/gpu/drm/panel/ which provide support for various panels and bridges (both external and internal to SoC).

The mapping of DRM entities to DSS hardware is roughly as follows:

DRM term

HW term

plane

DSS pipeline

crtc

DSS videoport

encoder

Internal and external bridges

connector

Connector or a panel

3.2.2.6.4.1. Driver Features

Note: this is not a comprehensive list of features supported/not supported, and new features may be added in every release.

DRM Plane Features
  • CSC

  • Scaler

  • Z-order

  • Global alpha blending

  • Alpha blending (pre-multipled & non-pre-multiplied)

  • Input Video Formats (Fourcc codes of supported formats: AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 AR15 AB15 XR24 XB24 RX24 BX24 XR30 XB30 YUYV UYVY NV12)

DRM CRTC Features
  • Gamma table

Display Sharing mode

The display sharing solution at Linux side is designed in such a way that the underlying kernel framework takes care of the display sharing functionality without requiring any updates in user-space API. This ensures that existing display server based windowing systems and display applications can leverage display in shared mode directly without any additional update or handling. The DSS resources can be partitioned across multiple processing cores by setting the ti,dss-sharing-mode and associated properties in the device-tree. A static resource partitioning scheme is designed where each of the DSS resources are given attributes related to sharing and ownership as desribed below :

  1. Display controller register region (Common or Common1 register space) :

Each processing core is given separate register region for controlling the display, with only one of the processing cores having access to global configuration region, Also each processing core has access only to the corresponding register region owned by it with other register regions completely inaccessible to it. The processing core running Linux can be assigned one of the available display controller register spaces using the “ti,dss-shared-mode-common” device-tree property.

  1. Video Pipeline :

This resource also can be exclusively owned by only one processing core, thus remaining completely inaccesible to other processing cores which are not owning it, so there is no sharing possible for this resource actually. The processing core running Linux can be assigned one or more of the available video pipelines using “ti,dss-shared-mode-plane” device-tree property. The relative z-order of planes owned by processing core running Linux can be set using ti,dss-shared-mode-plane-zorder.

  1. Video Port :

A video port can drive multiple video pipelines which are being independently controlled by different processing cores, so it can act as shared resource too where although only one of the processing cores has an exclusive write access to it but any other processing cores which are owning the Video piplines driven by this video port can be given read-only access to this Video Port’s register space.

To summarize, this resource can have exclusive ownership attribute with write access to only one processing core but shared attribute for other processing cores which are provided read-only access, but this is for only those processing cores which are using this video port for driving their video pipelines. The read-only access also helps such processing cores to determine the video port configuration like screen width, screen height e.t.c directly from video port registers without any communication requirement with the processing core owning this video port. The corresponding overlay managers associated with this video port are automatically given same ownership and sharing attributes.

The processing core running Linux can be assigned one or more of the available video ports either with read only access (i.e with only shared attribute) or write access (i.e. with exclusive ownership attribute), but for both the cases the driver enumerates corresponding connectors and video encoders attached to this video port thus making the full display pipeline visible to end user.

The device-tree property “ti,dss-shared-mode-vp” can be used by processing core running Linux to enlist one or more video ports being used by it and the ownership related information can be set using ti,dss-shared-mode-owned-vp device-tree property.

To summarize, below is the list of device-tree properties which can be added to display node, using these properties one can set up a resource paritioning scheme tailored as per the desired end use-case:

ti,dss-shared-mode :  Enable display sharing mode
ti,dss-shared-mode-planes : Enumerate Display planes owned by Linux
ti,dss-shared-mode-vp :  Enumerate Video Ports being used to control above planes
ti,dss-shared-mode-owned-vp : Specify which of the above Video Ports are actually owned by Linux , i.e. those video ports for which Linux has write access
ti,dss-shared-mode-common : Specify which of the common region i.e register space should be used by Linux for programming the DSS.
ti,dss-shared-mode-plane-zorder : Specify the relative plane ordering for the planes owned by Linux

Note

For display sharing mode to work with chosen resource paritioning between Linux and remote core, the remote core needs to be running appropriate firmware which programs the display hardware by supporting this resource paritioning scheme.

More detailed description of these properties can be found at: Display device-tree file Also there is a how-to guide available for dss sharing which walks through different examples for resource paritioning using these device-tree properties : How to enable dss sharing between remote core and Linux

3.2.2.6.4.1.1. Unsupported Features/Limitations

  • DPI output
    • TDM

    • BT-656/1120

    • MIPI DBI/RFBI

    • Interlace

  • DisplayPort (MHDP)
    • The SoC doesn’t support the MHDP IP, and doesn’t provide the DP output.

3.2.2.6.5. Driver Configuration

3.2.2.6.5.1. Kernel Configuration Options

tidss supports building both as built-in or as a module.

tidss can be found under “Device Drivers/Graphics support” in the kernel menuconfig. You need to enable DRM (CONFIG_DRM) before you can enable tidss (CONFIG_DRM_TIDSS).

  • Enable DSS Display Subsystem support (CONFIG_DRM_TIDSS)

Additional kernel config options may be needed, depending on the SoC and board.

  • Panels under “Device Drivers/Graphics support/Display Panels”

  • Bridges under “Device Drivers/Graphics support/Display Interface Bridges”

  • PHYs under “Device Drivers/PHY Subsystem”

3.2.2.6.5.2. Device Tree Node

Documentation for tidss device tree node and its properties can be found in linux kernel device tree bindings in below directory Documentation/devicetree/bindings/display/ti/. Seperate binding files are present for different version of the DSS controller.

3.2.2.6.6. Driver Usage

3.2.2.6.6.1. Loading tidss

If built as a module, you need to load all the drm, tidss, bridge and panel modules before tidss will start. When tidss starts, it will prints something along these lines:

[    9.207746] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 0

3.2.2.6.6.2. Using tidss

tidss is usually used by the windowing system like X server or Weston, so normally users don’t need to use tidss directly.

tidss device appears under /dev/dri/ directory, normally card0.

There is also so called DRM render device node, renderD128, which point to the same tidss device. Only buffer allocations can be done via the render node. The render node can be given more relaxed access restrictions, as the applications can only do buffer allocations from there, and cannot affect the system (except by allocating all the memory).

Low level userspace applications can use tidss via DRM ioctls. This is made a bit easier with libdrm, which is a wrapper library around DRM ioctls, or kms++ which is a C++11 library, or by Python bindings provided by kms++.

libdrm is included in TI releases and its sources can be found from:

https://gitlab.freedesktop.org/mesa/drm

libdrm also contains ‘modetest’ tool, which can be used to get basic information about DRM state, and to show a test pattern on a display. Refer to the section Testing tidss properties with modetest and kmstest below for some examples.

Another option is kms++, a C++11 library for kernel mode setting which includes a bunch of test utilities and also V4L2 classes and Python bindings for DRM and V4L2. Some kms++ tools are included in TI releases. kms++ can be found from:

https://github.com/tomba/kmsxx

For the J722S SoC, there are 2 instances of the DSS7-UL controller, and so will be the number of driver instances available. The AM62P5-SK EVM supports Hot Plug Detect for the HDMI output, which is currently served from the first DSS instance (DSS0). For the OLDI and DSI outputs, the devicetree (DT) overlays can be used to enable them. The OLDI output, configured as Dual-Link in the DT overlay, is sourced from DSS0, while the DSI output gets sourced from the DSS1. Either DSS instance can be enabled from the DT sources, simultaneously or otherwise. To enable these displays on AM62P5-SK, refer the How to enable DT overlays in linux guide, and enable the k3-am62p5-sk-microtips-mf101hie-panel.dtbo DT overlay for OLDI output, and k3-am62p5-sk-dsi-rpi-7inch-panel.dtbo DT overlay for the DSI output.

In the event, where a multi display is enabled on the AM62P5-SK/J722S EVM, with each DSS instance supporting at-least one display output, there will be two instances of tidss driver, and by extension, the drm framework driver, running on the platform. The GUI applications can capture them through the DRI card instances. Usually, the DSS0 will be /dev/dri/card0. The DSS1 however, can either be /dev/dri/card1 or /dev/dri/card2, depending on whether or not the GPU is enabled on the platform. The GPU, if present, associates with the card1, which leaves card2 for DSS1. In a case where GPU driver is not present, DSS1 will take up card1.

  • Note: Most display applications and windowing managers are programmed in such a way that

they can only access a display DRM card (card0) and a GPU DRM card (card1). This is why, the second DSS instance, will not show up running Weston or any framebuffer application, even when GPU is not present, in which case the windowing manager will only use card0. This makes DSS1 completely available for a 2nd DRM Master. This can be a custom display application, helping out in the most niche of use-cases.

3.2.2.6.6.3. Testing tidss

kmstest from kms++ is a good tool for testing tidss features. Note that any other applications using DRM (Weston, X) must be killed first. Another tool from kms++ is kmsprint, which can be used to print various bits of information about tidss.

$ kmsprint
Connector 0 (39) DP-1 (connected)
  Encoder 0 (38) NONE
    Crtc 0 (37) 1920x1080 148.500 1920/88/44/148 1080/4/5/36 60 (60.00)
      Plane 0 (31) fb-id: 62 (crtcs: 0 1) 0,0 1920x1080 -> 0,0 1920x1080 (AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 AR15 AB15 XR24 XB24 RX24 BX24 XR30 XB30 YUYV UYVY NV12)
        FB 62 1920x1080
Connector 1 (48) HDMI-A-1 (disconnected)
  Encoder 1 (47) NONE
$ kmstest -c dp -r 640x480
Connector 0/@39: DP-1
  Crtc 0/@37: 640x480 25.175 640/16/96/48/- 480/10/2/33/- 60 (59.94) 0xa 0x40
  Plane 0/@31: 0,0-640x480
    Fb 63 640x480-XR24
press enter to exit

When enabled, the second DSS instance can be tested as follows. Note that if the GPU entity is present, DSS1 will become card2, as GPU will assume the card1 instanciation.

$ kmsprint --device=/dev/dri/card2
Connector 0 (40) DSI-1 (connected)
  Encoder 0 (39) NONE
    Crtc 0 (38) 800x480 28.569 800/48/32/80 480/3/7/6 60 (60.00)
      Plane 0 (31) fb-id: 48 (crtcs: 0) 0,0 800x480 -> 0,0 800x480 (AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 XR15 XB15 XR24 XB24 RX24 BX24 XR30 XB30 YUYV UYVY NV12)
        FB 48 800x480
$ kmstest --device=/dev/dri/card2
Connector 0/@40: DSI-1
  Crtc 0/@38: 800x480 28.569 800/48/32/80/- 480/3/7/6/- 60 (60.00) 0xa 0x48
  Plane 0/@31: 0,0-800x480
    Fb 49 800x480-XR24
press enter to exit

3.2.2.6.6.4. tidss properties

tidss supports configuration via DRM properties. These are standard DRM properties, and DRM documentation describes them. Also, kmsprint can be used to show the supported properties.

Property

Object

Description

zpos

plane

Z position of a plane

COLOR_ENCODING

plane

Selects between BT.601 and BT.709 YCbCr color encoding

COLOR_RANGE

plane

Selects between full range and limited range YCbCr encoding

alpha

plane

Full plane alpha-blending

CTM

crtc

Color Transformation Matrix blob property. Implemented trough Color phase rotation matrix in DSS IP.

GAMMA_LUT

crtc

Blob property to set the gamma lookup table (LUT) mapping pixel data sent to the connector.

GAMMA_LUT_SIZE

crtc

Number of elements in gammma lookup table.

3.2.2.6.6.4.1. Testing tidss properties with modetest and kmstest

As the name suggests, modetest is DRM based mode setting test program available along with libdrm. It is an easy-to-use tool to test different features provided by display HWs. The DRM driver for, the display HWs, exposes these features as DRM properties, (see the table above), and the modetest utility uses these properties to configure the display HW.

modetest outputs look different based on the number and types of displays connected, but the format remains the same. Before looking at this particular modetest output, kmsprint output is provided as reference.

$ kmsprint
Connector 0 (40) LVDS-1 (connected)
  Encoder 0 (39) LVDS
    Crtc 0 (38) 1920x1200@60.00 150.275 1920/32/52/24/? 1200/24/8/3/? 60 (60.00) 0x0 0x48
      Plane 0 (31) fb-id: 51 (crtcs: 0 1) 0,0 1920x1200 -> 0,0 1920x1200 (AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 XR15 XB15 XR24 XB24 RX24 BX24 XR30 XB30 YUYV UYVY NV12)
        FB 51 1920x1200
Connector 1 (50) HDMI-A-1 (disconnected)
  Encoder 1 (49) NONE

In the example below, AM625 SK-EVM has been used, but this could extrapolated to all the EVMs running TI SoCs that support DSS7-L / DSS7-UL. An OLDI display is being run on the AM625 SK-EVM, while the HDMI is disconnected.

Now, a shortened version of the command: modetest -M tidss that highlights some information used in the examples later.

$ modetest -M tidss
Encoders:
id      crtc    type    possible crtcs  possible clones
39      38      LVDS    0x00000001      0x00000001
49      0       none    0x00000002      0x00000002

Connectors:
id      encoder status          name            size (mm)       modes   encoders
40      39      connected       LVDS-1          217x136         1       39
  modes:
        index name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot
  #0 1920x1200 60.00 1920 1952 2004 2028 1200 1224 1232 1235 150275 flags: ; type: preferred, driver
  props:
[ ... ]

50      0       disconnected    HDMI-A-1        0x0             0       49
  props:
[ ... ]

CRTCs:
id      fb      pos     size
38      51      (0,0)   (1920x1200)
  #0 1920x1200 60.00 1920 1952 2004 2028 1200 1224 1232 1235 150275 flags: ; type: preferred, driver
  props:
[ ... ]

48      0       (0,0)   (0x0)
  #0  nan 0 0 0 0 0 0 0 0 0 flags: ; type:
  props:
[ ... ]

Planes:
id      crtc    fb      CRTC x,y        x,y     gamma size      possible crtcs
31      38      51      0,0             0,0     0               0x00000003
  formats: AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 XR15 XB15 XR24 XB24 RX24 BX24 XR30 XB30 YUYV UYVY NV12
  props:
[ ... ]

41      0       0       0,0             0,0     0               0x00000003
  formats: AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 XR15 XB15 XR24 XB24 RX24 BX24 XR30 XB30 YUYV UYVY NV12
  props:
[ ... ]

From the information above, it can be inferred that the LVDS display ouput has these objects associated with it.

  • Plane with ID = 31.

  • CRTC with ID = 38.

  • Encoder with ID = 39.

  • Connector with ID = 40.

Note that the plane 31 is the primary plane for CRTC 38 (LVDS Display). And for the HDMI display, the associated objects are as follows.

  • Encoder with ID = 49.

  • Connector with ID = 50.

Since HDMI display is disconnected at the moment, no CRTC object has been enumerated for it, and hence plane 41 remains unused.

  • Z order

Z position of the plane when multiple planes are being displayed.

This property is enumerated as zpos in the modetest output. This property can be used with the -w option of modetest. However, this property is not useful without plane overlaying, as it won’t show use any discernible change on the display. Hence, refer the example given in the next section.

  • Plane Overlaying

Use unused planes as overlay planes.

Based on the version, the DSS controller can have 2 to 4 video pipelines, which get enumerated as DRM planes. If the number of displays connected is less than the number of video pipes in the DSS controller, the extra pipes can be used as overlay planes.

In this example, plane 41 remains an unused plane, while plane 31 acts as a primary plane for CRTC 38. To use plane 41 as an overlay on top of plane 31, the following command can be used.

$ modetest -M tidss -s 40@38:1920x1200 -P 41@38:1280x720 -w 41:zpos:1
setting mode 1920x1200-60.00Hz on connectors 40, crtc 38
testing 1280x720@XR24 overlay plane 41

In this example, we use the primary plane via its connector and crtc using the -s option. -s 40@38:1920x1200 renders vertical color bars on the LVDS display. Adding the -P option, -P 41@38:1280x720, renders another frame of color bars (diagonal in this case) of resolution 1280x720. The -w 41:zpos:1 ensures that the plane 41 is displayed on top of plane 31 (or else, if plane 31 is on top, then plane 41 will be underneath and hence won’t show up on the display).

  • Global Alpha Blending

Full plane alpha-blending

When displaying multiple planes on top of one another, we can assign transparency levels to each of the planes using the alpha property. For tidss, the value of this property ranges from 0 with complete transparency to 65535 with complete opacity.

$ modetest -M tidss -s 40@38:1920x1200 -P 41@38:1280x720 -w 41:zpos:0 -w 31:zpos:1 -w 31:alpha:10000
setting mode 1920x1200-60.00Hz on connectors 40, crtc 38
testing 1280x720@XR24 overlay plane 41

In this example, we are displaying the overlay plane (41) behind the primary plane (31) by manipulating the zpos property. Since the overlay plane is of a smaller resolution (1280x720) and the primary plane is of resolution 1920x1200, the overlay plane is expected to not be seen. However, with the introduction of the alpha property on the primary plane that doesn’t happen. With alpha = 10000 (out of 65535), faint vertical color bars can be seen on the display, along with diagonal color bars as solid.

  • Scaling

Scale the frame smaller or larger.

This feature will only work for plane IDs that map to the VID pipeline of tidss (and not the VIDL pipe). Follow this simple rule of thumb to find out if a particular DRM plane is VID or not. DSS-7 has 4 pipelines in total, while DSS7-UL has 2 pipelines. The VIDL pipelines get enumerated as DRM planes first, and then the VID pipes do. Therefore

  • For DSS7-L with 4 pipelines and DRM plane IDs 31, 41, 51, and 58, the DRM planes 51 and 58 are VID pipelines and thus have scaling support.

  • For DSS7-UL with 2 pipelines and DRM plane IDs 31, and 41, the DRM plane 41 is the VID pipeline and thus have scaling support.

The following example was run on DSS7-UL and hence the pipe with scaling capability is DRM plane 41.

$ modetest -M tidss -s 40@38:1920x1200@AR24 -P 41@38:400x400*2
setting mode 1920x1200-60.00Hz on connectors 40, crtc 38
testing 400x400@XR24 overlay plane 41

Note that the *2 at the end of -P 41@38:400x400*2 is the scaling factor.

  • Cropping

kmstest utility can be used to demonstrate cropping in a video frame using a test pattern. The user can specify the main video frame size and an input color format using the -f argument. Then the source region, also known as a view region, can be specified using the -v argument. This takes a secondary width and height to create a rectangle starting at a given coordinate. The destination region, or plane region, for the view can be specified using -p argument. This takes a third width, height and coordinate position to place an overlay with the associated view region’s content.

$ kmstest -c hdmi -p 0:0,0-1000x1000 -f 1000x1000-XR24 -v 0,0-1000x1000
Connector 1/@50: HDMI-A-1
Crtc 1/@48: 1920x1080@59.93 138.500 1920/48/32/80/+ 1080/3/5/23/- 60 (59.93) 0x9 0x48
Plane 0/@31: 0,0-1000x1000
Fb 55 1000x1000-XR24

The above example displays a 1000x1000 video frame on the screen at coordinates 0,0.

../../../../../_images/DSS_cropping_example_1.jpg
$ kmstest -c hdmi -p 0:0,0-800x800 -f 1000x1000 -v 0,0-800x800
Connector 1/@50: HDMI-A-1
Crtc 1/@48: 1920x1080@59.93 138.500 1920/48/32/80/+ 1080/3/5/23/- 60 (59.93) 0x9 0x48
Plane 0/@31: 0,0-800x800
Fb 55 1000x1000-XR24

Taking as an input a video frame of dimensions 1000x1000,the example creates a cropped source rectangle of dimensions 800x800, starting at coordinates 0,0 and displays it on screen at coordinates 0,0.

../../../../../_images/DSS_cropping_example_2.jpg
$ kmstest -c hdmi -p 0:500,200-800x800 -f 1000x1000 -v 200,100-800x800
Connector 1/@50: HDMI-A-1
Crtc 1/@48: 1920x1080@59.93 138.500 1920/48/32/80/+ 1080/3/5/23/- 60 (59.93) 0x9 0x48
Plane 0/@31: 500,200-800x800
Fb 54 1000x1000-XR24

Taking as an input a video frame of dimensions 1000x1000, this example creates a cropped source rectangle of dimensions 800x800, starting at coordinates 500,200 and displays it on screen at coordinates 200,100 keeping the same dimensions as source rectangle i.e 800x800 without scaling.

../../../../../_images/DSS_cropping_example_3.jpg

3.2.2.6.6.5. Buffers

The buffers used for tidss can be either allocated from tidss or imported from some other driver (dmabuf import). All buffers must be contiguous.

tidss supports generic DRM dumb buffers. Dumb buffers are allocated using the generic DRM_IOCTL_MODE_CREATE_DUMB ioctl.

3.2.2.6.6.6. fbdev emulation (/dev/fb0)

DRM framework supports “emulating” the legacy fbdev API. This feature can be enabled or disabled in the kernel config (CONFIG_DRM_FBDEV_EMULATION). The fbdev emulation offers only basic feature set and the fb is shown on the first display. Fbdev emulation is mainly intended for kernel console or boot splash screens.