3.2.2.3. CSI2RX
3.2.2.3.1. Introduction
The CSI2RX subsystem is present on some TI SoCs which facilitates the capture of camera frames over a MIPI CSI-2 bus. The driver is based on the Video for Linux 2 (V4L2) API. It implements V4L2’s Media Controller (MC) API.
3.2.2.3.2. Hardware Architecture
The CSI2RX subsystem is composed of 3 IPs: Cadence DPHY, Cadence CSI2RX bridge, TI CSI2RX DMA wrapper (aka the SHIM layer).

The CSI2RX subsystem supports the following features:
Compliant to MIPI CSI v1.3
Supports up to 16 virtual channels per input (partial MIPI CSI v2.0 feature).
Data rate up to 2.5 Gbps per lane (wire rate).
Supports 1, 2, 3, or 4 data lane connection to DPHY_RX.
Programmable formats including YUV420, YUV422, RGB, Raw, etc.
See the the technical reference manual (TRM) for the SoC in question for more detailed information.
3.2.2.3.3. Driver Architecture
The driver is based on the Video 4 Linux 2 (V4L2) API. It is implemented according to the V4L2 standard for capture devices. The driver is only responsible for programming the SoC components for capture like the DPHY, CSI bridge, DMA. For external devices like camera sensors separate V4L2 subdevice drivers are needed.
3.2.2.3.3.1. The Media Controller API
The driver is implemented using V4L2’s Media Controller (MC) API. In the MC API, each element in the media pipeline is configured individually by the user-space application. In comparison, in the legacy or non-MC API drivers, only the /dev/videoX node needs to be configured, and it propagates the configuration up the chain. With this model, the MC API allows for more flexible pipeline configurations which can all be controlled from user-space without having to change the driver or the device tree.
For example, with the legacy API the format is set on /dev/videoX and that will set it for the entire pipeline (sensor, bridge, DMA engine, etc). With the MC API, the format needs to be set on each individual element in the pipeline. So with a single camera setup, for capturing 1920x1080 @ 60fps UYVY, the camera (/dev/v4l-subdevX) should first be configured to use that format via the V4L2 subdev ioctls. Then the /dev/videoX node (which represents the DMA context) should be configured to use matching configuration. The Media Controller framework checks for mismatches and reports errors if something is not right.
In similar fashion, the DMA context does not care about frame rate. It can capture at any rate, so the driver does not implement the G_PARM or S_PARM ioctls. Instead, the frame rate should be set on the sensor using VIDIOC_SUBDEV_S_FRAME_INTERVAL.
Quick links for relevant Linux Kernel documentation:
3.2.2.3.3.2. Utilities to interact with the driver
Standard V4L2 utilities can be used to set these formats and frame rates. One such tool is media-ctl.
To see the media pipeline to understand how all the components are connected in
software, the pipeline can be printed to the console using media-ctl -p
. This
would list all the elements in the pipeline, what they are connected to, and
their names. This information can then be used to set formats and frame rates on
various elements for the pipeline. For example, below command can be used to set
1920x1080 @ 30fps UYVY format on the sensor node:
media-ctl --set-v4l2 '"sensor-name 9-0012":0 [fmt:UYVY8_2X8/1920x1080@1/30]'
This just sets the formats on the sensor and bridge. The format on the DMA
context (/dev/videoX) needs to be set separately. This can be done while
starting the capture with yavta for example. The below command can
be run next to start capturing the video stream to a file called
capture
:
yavta -c -Fcapture -s 1920x1080 -f UYVY /dev/video0
This command first sets the 1920x1080 UYVY format on the DMA context (which must
match the format on the sensor), and then starts capturing frames to a file
called capture
.
It is often useful to see the pipeline visually. media-ctl can print the pipeline as a dot graph which can then be converted to an image for viewing. The below set of commands can achieve this:
media-ctl --print-dot | dot -Tpng > graph.png
3.2.2.3.3.3. Building the driver
First, enable the DPHY using CONFIG_PHY_CADENCE_DPHY. Then enable the CSI2RX bridge using CONFIG_VIDEO_CADENCE and CONFIG_VIDEO_CADENCE_CSI2RX. Finally, enable CONFIG_VIDEO_TI_J721E_CSI2RX. The config for the sensor should also be enabled.
The driver can be built-in or it can be a loadable module. If the driver is
built as a module, the module will be called j721e-csi2rx
. Along with that,
the Cadence bridge and DPHY modules must also be loaded, which are called
cdns-csi2rx
and cdns-dphy
respectively.
3.2.2.3.4. Creating device tree nodes for sensor
Since the sensor is a separate module and any sensor can be plugged in to the board, the sensor device tree nodes are not included in the base dtb. Instead, it should be added in as an overlay.
Below overlay is an example for a sensor module connected to the board using I2C2 and CSI-RX Port 0:
// SPDX-License-Identifier: GPL-2.0
/*
* Example Camera Module
* Copyright (C) 2024 Texas Instruments Incorporated - https://www.ti.com/
*/
/dts-v1/;
/plugin/;
#include <dt-bindings/gpio/gpio.h>
&{/} {
clk_sensor_fixed: sensor-xclk {
compatible = "fixed-clock";
#clock-cells = <0>;
clock-frequency = <24000000>;
};
};
&main_i2c2 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
camera@10 {
compatible = "manufacturer,sensor-compatible";
reg = <0x10>;
clocks = <&clk_sensor_fixed>;
clock-names = "xclk";
port {
csi2_cam0: endpoint {
remote-endpoint = <&csi2rx0_in_sensor>;
clock-lanes = <0>;
/*
* This example sensor uses 2 lanes. Other sensors might use
* 1, 2, 3, or 4 lanes. Populate this property accordingly.
* See Documentation/devicetree/bindings/media/video-interfaces.yaml
* for more info.
*/
data-lanes = <1 2>;
};
};
};
};
&cdns_csi2rx0 {
ports {
#address-cells = <1>;
#size-cells = <0>;
csi0_port0: port@0 {
reg = <0>;
status = "okay";
csi2rx0_in_sensor: endpoint {
remote-endpoint = <&csi2_cam0>;
bus-type = <4>; /* CSI2 DPHY. */
clock-lanes = <0>;
data-lanes = <1 2>;
};
};
};
};
&ti_csi2rx0 {
status = "okay";
};
&dphy0 {
status = "okay";
};
3.2.2.3.5. Enabling camera sensors
J722S has two instances of CSI2RX capture subsystem and can support upto eight IMX390 cameras using FPDLink fusion EVM. J722S also supports OV5640 and IMX219 module connected to MIPI connector.
3.2.2.3. Applying sensor overlays
To enable FPDLink cameras you will need to apply the device tree overlays for both the fusion board and the sensor at U-boot prompt:
# For single RCM IMX390 connected to RX port 0 on Fusion board EVM on J722S EVM:
# FPDLink IMX390 camera overlays are named according to the port connected in the following
# format : ti/k3-fpdlink-imx390-rcm-<csi_port>-<fusion_rx_port>.dtbo
=> setenv name_overlays ti/k3-j721s2-evm-fusion.dtbo ti/k3-fpdlink-imx390-rcm-0-0.dtbo
=> boot
For more details on building or applying overlays permanently, refer to the How to enable DT overlays in linux guide.
3.2.2.3. CSI2RX testing details
The following combinations of sensors are tested in the latest sdk.
Hardware
Sensor
Default format and resolution
J722S
OV5640 TEVI/PCAM Rpi Module
YUYV8_1X16/1280x720 at 30 fps
J722S
FPDLink fusion 1 EVM, IMX390
SRGGB12_1X12/1936x1100 at 30 fps
J722S
IMX219 RPi Camera
SRGGB8_1X8/1920x1080 at 30 fps