Vision Apps Release Notes
Version: 11.02.00
Contents
- Introduction
- Licensing
- Getting Started
- Documentation
- What's New
- Upgrade and Compatibility Information
- Device Support
- Validation Information
- Fixed Issues
- Open Defects
- Technical Support
- Package Versioning
Introduction
The Vision Apps package consists of ADAS, vision, deep learning, perception demos/applications for Jacinto 7 platform
To run the demos in vision apps, the companion Processor SDK Linux for Jacinto 7 also needs to be downloaded separately.
Licensing
Refer to Processor SDK RTOS manifest at top level [HTML]
Getting Started
The Vision Apps User Guide [HTML] provides the documentation and references necessary to begin development on TI's platforms using Vision Apps.
Documentation
Refer to following documentation for further details:
| Vision Apps User Guide | Build instructions, API Guide | [HTML] |
| Surround View Manual Calibration Tool | Instructions for Generating Calibration Binaries | [PDF] |
| Release Notes Archive | Previous release notes | [FOLDER] |
What's New
New features in this release are highlighted in bold- OpenVX based demos for ADAS, Vision, deep learning applications
- Free RTOS and Safe RTOS on C7x and R5F and Linux or QNX on A72
- Integrates all major PSDK RTOS and PSDK Linux SW components like TIDL, MMALIB, PDK, OpenVX, ETHFW, OpenGL, C7x algorithms, imaging/sensors, IPC, Linux, TI-RTOS, SPL/uboot.
- Integrates all major HW components like CSI2 camera, eDP/HDMI display, UART, I2C, ethernet, SD card
- Deep Learning demos
- Image Classification demo
- File based
- Camera based
- Standalone Semantic Segmentation application
- File based
- Camera based
- Standalone Object Detection application
- File based
- Camera based
- Auto valet parking (AVP) demo
- semantic segmentation, Parking spot detect and Vehicle detect algorithms
- 1 channel, 3 algo mode
- 3 channel, 3 algo mode (combined network for parking spot and vehicle detect)
- 3 channel, 5 algo mode - combined network for parking spot and vehicle detect + Three task network for Semantic Segmentation, Motion Segmentation and Depth Estimation (AVP3 demo)
- DKAZE-based Visual Localization application
- Debug support for the ability to debug intermediate layer information from TIDL node
- Surround View demos
- 3D surround view using GPU on 4x 2MP 30fps live camera input
- 3D surround view calibration application
- Demo uses GLTF 3D Model.
- ADAS/Vision demos
- Dense optical flow (DOF) demo
- Stereo disparity engine demo
- Single and multi camera CSI2RX + VISS + LDC + MSC + Display demo
- Multi channel codec demo utilizing CSI2RX + VISS + LDC + MSC + Display with Linux and QNX running on A72
- C7x algorithm offload demo (with DMA acceleration)
- CV Demos
- Structure from motion
- OpenVX target nodes
- image pre-processing (YUV 2 RGB) nodes for DL demos
- image post-processing and visualization nodes for deep learning, DOF, Stereo demos
- OpenGL nodes for surround view
- Multi-threading support in MSC mosaic node
- Profiling, logging and other utility APIs
- General stability, performance, documentation improvements
- Memory map updated to accomodate increase of DDR_SHARED_MEM to 1GB. Please check vision_apps/platform/j784s4/rtos/system_memory_map.html for more details
- All included MCU tasks are split between MCU2_0 (ETHFW, VPAC0 HWA), MCU2_1 (DMPAC HWA), MCU4_0 (VPAC1 HWA) leaving MCU3_0, MCU3_1, MCU4_1 free on the main island
- Enabled support to get DDR BW per initiator using CtoolsLib on HS-FS Device.
- VISS Node Optimizations and performance related bug fixes
- [Optimization] Moved VISS configuration memory to cache write-through region to save 125us of configuration time per camera frame (eliminating cache write-back maintenance operation time)
- [Perf Bug Fix] Removed unnecessary cache invalidate maintenance operation on the VISS configuration memory to save 125us of configuration time per camera frame
- [Perf Bug Fix] Removed redundant cpu copies of DCC tables per camera frame (EdgeEnhancement, gamma tables, raw histogram lut)
Device Support
Refer Processor SDK RTOS release notes [HTML]
Validation Information
The tools used to validate this package are listed in top level user guide [HTML]
Fixed Issues
| ID | Summary |
|---|---|
| ADASVISION-6386 | QoS Settings cause artifacts in DSS M2M output |
| ADASVISION-6679 | [QNX] GCC version of compiler is used in concerto instead of QCC |
| ADASVISION-6738 | [QNX] vx_app_tidl app build broken for debug mode |
| ADASVISION-6647 | MMALIB profile is hardcoded to "release" in linker paths |
| ADASVISION-6470 | Dual Display with both DP ports is failing with Linux+RTOS |
Open Defects
| ID | Summary |
|---|---|
| ADASVISION-4923 | Single cam error on ports other than port 1 after running multi cam |
| ADASVISION-5555 | SDE disparity artifacts on EVM |
| ADASVISION-6199 | Race Conditions in c7x-mma-tidl and tiadalg builds |
| ADASVISION-6531 | 4k Display Flickers high C7x load |
| ADASVISION-6387 | No option to set vpParams->scanFmt in the dss utility from vision_apps |
| ADASVISION-6451 | mailbox queue overflowing while running vx_app_arm_ipc.out |
| ADASVISION-6452 | SFM demo failing on J784S4 and J742S2 |
| ADASVISION-6453 | SRV + AVP demo not working |
| ADASVISION-6488 | More than 1000% CPU Load for C7X & MCU |
| ADASVISION-6520 | Apps killed with Cntrl^C do not do proper cleanup ... can't be run again |
| ADASVISION-6564 | Vision app utils: qnx: All thread creation must use default stack instead of global stack |
| ADASVISION-6809 | [SafeRTOS]: Initialize task stack section in system_pre_init API |
Technical Support
For technical support and additional assistance, contact local TI Field Application Engineer
Package Versioning
Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.
| Digit | Meaning | Description |
|---|---|---|
| 1 (M=Major) | Major revision | Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered. |
| 2 (m=minor) | Minor revision | Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set. |
| 3 (p=patch) | Patch number | Incremented for all other source code changes. This include any packaging support code. |
| 4 (b=build) | Build number | Incremented for each release delivery to CM. Reset for any change to M, m or p |
Copyright 2020, Texas Instruments Incorporated