5.4.9.1.4.1. Enet lwIP Example¶
5.4.9.1.4.1.1. Building LWIP example¶
Enabling specific features in the test
To configure what gets built in the example, navigate to the example directory
pdk/packages/ti/drv/enet/examples/enet_lwip_exampleand find thelwipcfg.hfile. Inside, change the macros corresponding to the program that you wish to build to 1.For example, if udpecho is required, set:
#define LWIP_UDPECHO_APP 1Note
The heap memory may need to be increased in the
FreeRTOSConfig.hfile to accomodate multiple apps.
To build the lwip example, issue the following command:
make -s enet_lwip_example_freertos BOARD=<BOARD> CORE=<CORE>
5.4.9.1.4.1.2. Running LWIP example¶
Load and run the enet_lwip_example image from the corresponding binaries folder.
The setup requires a LAN cable to be connected between the device and a multiport-router for the link status to be UP and aquire an IP address.
Connect the LAN cable between the same router and Laptop/PC from where the ping/echo tests are run.
Wait until the local interface IP is assigned and printed on the console like below.
Starting lwIP, local interface IP is dhcp-enabled CPSW_2G Test on MCU NAVSS EnetPhy_bindDriver: PHY 0: OUI:080028 Model:23 Ver:01 <-> 'dp83867' : OK PHY 0 is alive Host MAC address: 70:ff:76:01:02:03 [LWIPIF_LWIP] CPSW has been started successfully [LWIPIF_LWIP] NETIF INIT SUCCESS status_callback==UP, local interface IP is 0.0.0.0 Cpsw_handleLinkUp: Port 1: Link up: 100-Mbps Full-Duplex MAC Port 1: link up link_callback==UP status_callback==UP, local interface IP is 192.168.0.9 Initializing apps UDP server listening on port 5001
5.4.9.1.4.1.3. Testing LWIP example¶
Prerequisites: LAN cable setup and device link is UP and Local interface IP is successfully aquired.
Ping test
ping -t <ip_addr> ping -t 192.168.0.9
UDP/ TCP echo test
Download echotool from this website and execute the commands to see the response.
UDP echo command:
echotool.exe <ip_addr> /p udp /r 7 /n 0 echotool.exe 192.168.0.9 /p udp /r 7 /n 0
TCP echo command:
echotool.exe <ip_addr> /p tcp /r 7 /n 0 echotool.exe 192.168.0.9 /p tcp /r 7 /n 0
iperf test
Download iperf2.0.10 from iperf website and execute the commands to see the response.
iperf TCP test command:
iperf.exe -c <ip_addr> -r iperf.exe -c 192.168.0.9 -r
iperf UDP test command:
iperf.exe -c <ip_addr> -r -u iperf.exe -c 192.168.0.9 -r -u
Static IP
The Enet lwIP example uses DHCP by default. If static IP needs to be tested, the following
two config options need to be disabled in examples/enet_lwip_example/lwipcfg.h.
#define USE_DHCP 0 #define USE_AUTOIP 0
The IP address, gateway and netmask can be set in the same lwipcfg.h file.
#define LWIP_PORT_INIT_IPADDR(addr) IP4_ADDR((addr), 192,168,1,200) #define LWIP_PORT_INIT_GW(addr) IP4_ADDR((addr), 192,168,1,1) #define LWIP_PORT_INIT_NETMASK(addr) IP4_ADDR((addr), 255,255,255,0)