34 #ifndef MATHLIB_POW_H_
35 #define MATHLIB_POW_H_
43 #include "../common/MATHLIB_types.h"
MATHLIB_STATUS MATHLIB_pow(size_t length, T *pSrc0, T *pSrc1, T *pDst)
Performs the elementwise power of input vectors. Function can be overloaded with float and double poi...
MATHLIB_STATUS MATHLIB_pow_sp(size_t length, float *pSrc0, float *pSrc1, float *pDst)
This function is the C interface for MATHLIB_pow. Function accepts float pointers.
MATHLIB_STATUS MATHLIB_pow_dp(size_t length, double *pSrc0, double *pSrc1, double *pDst)
This function is the C interface for MATHLIB_pow. Function accepts double pointers.
MATHLIB_STATUS_NAME
The enumeration of all status codes.