34 #ifndef MATHLIB_DIV_H_
35 #define MATHLIB_DIV_H_
43 #include "../common/MATHLIB_types.h"
102 MATHLIB_div_sp(
size_t length,
float* pSrc0,
float* pSrc1,
float* pDst);
MATHLIB_STATUS MATHLIB_div(size_t length, T *pSrc0, T *pSrc1, T *pDst)
Performs the elementwise divide of two input vectors. Function can be overloaded with float or double...
MATHLIB_STATUS MATHLIB_div_sp(size_t length, float *pSrc0, float *pSrc1, float *pDst)
This function is the C interface for MATHLIB_div. Function accepts float pointers.
MATHLIB_STATUS_NAME
The enumeration of all status codes.