63 #ifndef HWA_VPAC_VISS_FCP_H_ 64 #define HWA_VPAC_VISS_FCP_H_ 67 #include <VX/vx_kernels.h> 85 #define TIVX_VPAC_VISS_MUX0_Y12 (0U) 87 #define TIVX_VPAC_VISS_MUX0_VALUE12 (3U) 89 #define TIVX_VPAC_VISS_MUX0_NV12_P12 (4U) 92 #define TIVX_VPAC_VISS_MUX0_IR8 (6U) 94 #define TIVX_VPAC_VISS_MUX0_IR12_P12 (7U) 98 #define TIVX_VPAC_VISS_MUX1_UV12 (0U) 100 #define TIVX_VPAC_VISS_MUX1_C1 (2U) 103 #define TIVX_VPAC_VISS_MUX2_Y8 (0U) 105 #define TIVX_VPAC_VISS_MUX2_RED (1U) 107 #define TIVX_VPAC_VISS_MUX2_C2 (2U) 109 #define TIVX_VPAC_VISS_MUX2_VALUE8 (3U) 111 #define TIVX_VPAC_VISS_MUX2_NV12 (4U) 113 #define TIVX_VPAC_VISS_MUX2_YUV422 (5U) 116 #define TIVX_VPAC_VISS_MUX2_IR12_U16 (6U) 120 #define TIVX_VPAC_VISS_MUX3_UV8 (0U) 122 #define TIVX_VPAC_VISS_MUX3_GREEN (1U) 124 #define TIVX_VPAC_VISS_MUX3_C3 (2U) 127 #define TIVX_VPAC_VISS_MUX4_BLUE (1U) 129 #define TIVX_VPAC_VISS_MUX4_C4 (2U) 131 #define TIVX_VPAC_VISS_MUX4_SAT (3U) 134 #define TIVX_VPAC_VISS_EE_MODE_OFF (0U) 136 #define TIVX_VPAC_VISS_EE_MODE_FCP0_Y12 (1U) 138 #define TIVX_VPAC_VISS_EE_MODE_FCP0_Y8 (2U) 140 #define TIVX_VPAC_VISS_EE_MODE_FCP1_Y12 (4U) 142 #define TIVX_VPAC_VISS_EE_MODE_FCP1_Y8 (8U) 144 #define TIVX_VPAC_VISS_EE_MODE_Y12 TIVX_VPAC_VISS_EE_MODE_FCP0_Y12 146 #define TIVX_VPAC_VISS_EE_MODE_Y8 TIVX_VPAC_VISS_EE_MODE_FCP0_Y8 148 #define TIVX_VPAC_VISS_EE_MODE_MV_Y12 TIVX_VPAC_VISS_EE_MODE_FCP1_Y12 150 #define TIVX_VPAC_VISS_EE_MODE_MV_Y8 TIVX_VPAC_VISS_EE_MODE_FCP1_Y8 153 #define TIVX_VPAC_VISS_CHROMA_MODE_420 (0U) 155 #define TIVX_VPAC_VISS_CHROMA_MODE_422 (1U) uint32_t ee_mode
Definition: hwa_vpac_viss_fcp.h:263
uint32_t chroma_mode
Definition: hwa_vpac_viss_fcp.h:281
uint32_t mux_output3
Definition: hwa_vpac_viss_fcp.h:240
The Flex Color Processing (FCP) data structure used in the tivx_vpac_viss_params_t structure for prog...
Definition: hwa_vpac_viss_fcp.h:181
uint32_t mux_output2
Definition: hwa_vpac_viss_fcp.h:227
uint32_t mux_output0
Definition: hwa_vpac_viss_fcp.h:194
uint32_t mux_output4
Definition: hwa_vpac_viss_fcp.h:251
uint32_t mux_output1
Definition: hwa_vpac_viss_fcp.h:206