63 #ifndef HWA_VPAC_VISS1_H_ 64 #define HWA_VPAC_VISS1_H_ 67 #include <VX/vx_kernels.h> 78 #define TIVX_VPAC_VISS_FCP_NUM_INSTANCES (1U) 82 #define TIVX_VPAC_VISS_MAX_OUTPUTS (6U) 115 uint32_t output_fcp_mapping[5];
349 vx_user_data_object configuration,
350 vx_user_data_object ae_awb_result,
351 vx_user_data_object dcc_buf,
358 vx_user_data_object h3a_output,
359 vx_distribution histogram0,
360 vx_distribution histogram1,
361 vx_distribution raw_histogram);
uint32_t fcp1_config
Definition: hwa_vpac_viss1.h:105
uint32_t channel_id
Definition: hwa_vpac_viss1.h:175
The Flex Color Processing (FCP) data structure used in the tivx_vpac_viss_params_t structure for prog...
Definition: hwa_vpac_viss_fcp.h:181
uint32_t bypass_cac
Definition: hwa_vpac_viss1.h:118
uint32_t h3a_aewb_af_mode
Definition: hwa_vpac_viss1.h:155
VX_API_ENTRY vx_node VX_API_CALL tivxVpacVissNode(vx_graph graph, vx_user_data_object configuration, vx_user_data_object ae_awb_result, vx_user_data_object dcc_buf, tivx_raw_image raw, vx_image output0, vx_image output1, vx_image output2, vx_image output3, vx_image output4, vx_user_data_object h3a_output, vx_distribution histogram0, vx_distribution histogram1, vx_distribution raw_histogram)
[Graph] Creates a VPAC_VISS Node.
#define TIVX_VPAC_VISS_MAX_OUTPUTS
Max Output Channels.
Definition: hwa_vpac_viss1.h:82
uint64_t timestamp
Timestamp value.
Definition: hwa_vpac_viss1.h:214
uint32_t h3a_in
Definition: hwa_vpac_viss1.h:144
uint32_t bypass_nsf4
Definition: hwa_vpac_viss1.h:125
uint32_t sensor_dcc_id
Definition: hwa_vpac_viss1.h:96
uint32_t bypass_glbce
Definition: hwa_vpac_viss1.h:129
#define TIVX_VPAC_VISS_FCP_NUM_INSTANCES
Definition: hwa_vpac_viss1.h:78
uint32_t enable_ctx
Definition: hwa_vpac_viss1.h:171
uint32_t bypass_dwb
Definition: hwa_vpac_viss1.h:121
uint32_t enable_psa
Definition: hwa_vpac_viss1.h:198
The configuration data structure used by the TIVX_KERNEL_VISS kernel.
Definition: hwa_vpac_viss1.h:93
uint32_t use_case
Definition: hwa_vpac_viss1.h:101
uint32_t enable_error_events
Definition: hwa_vpac_viss1.h:193
Definition: hwa_vpac_viss1.h:201