![]() |
PDK API Guide for J742S2
|
===========================================================================
This is the CSL-FL for the EMIF controller/PUB. It provides the structures and APIs needed to configure and initialize the EMIF controller/PUB. Once the EMIF is initialized, additional API functions are available to implement runtime operations
The following lists the steps required to use this CSL-FL:
Sub Modules | |
| EMIF Data Structures | |
| EMIF Enumerated Data Types | |
| EMIF Functions | |