7. EVM Setup for J742S2¶
This section is intended to give a quick reference of EVM related to SDK usage. Full EVM documentation will be referenced at TDA4AP, TDA4VP EVM at a later time.
Important
The power supply requires an output voltage of 24-48 VDC, and output capacity of 100-160W, depending on use case and connected peripherals.
When connecting the fusion daughter card, the power cable connecting processor board and fusion board should look exactly like the picture in section Fusion daughter card. (P.S. The same cable from TDA2P EVM has the opposite wire connection at one end)
7.1. EVM Setup to run SDK demos¶
7.1.1. Daughter card requirements¶
Below table shows the daughter cards required for various features/demos
Feature |
Fusion 1 card |
IMX390+UB953 FPDLink sensors |
QPENet card |
|---|---|---|---|
eDP (DisplayPort) display (1) |
na |
na |
na |
HDMI display (2) |
na |
na |
na |
CSI2RX camera input |
REQURIED |
REQURIED |
na |
CAN demos (1) |
na |
na |
na |
7.1.2. UART terminal setup¶
Connect USB cable to Main UART port on EVM (see EVM)
4 UART ports would be visible at the PC side
Port 0 from this is used this for Linux, RTOS UART terminal from A72
Setup UART for 115200 baud rate, 8 data bits, no party, 1 stop bit
7.1.3. Boot Modes¶
Bootmodes are selected using the SW11 and SW7 switches on the EVM.
7.1.3.1. No Boot Mode¶
When you want the binaries to be loaded from a debugger (CCS), the EVM has to be set in the NO boot mode.
Following are the switch settings to do the same.:
SW11[1-8] = 1000 1000
SW7[1-8] = 0111 0000
Fig. 7.1 No Boot Mode¶
7.1.3.2. SD Boot Mode¶
Following are the switch settings to set the boot mode to SD for EVM.:
SW11[1-8] = 1000 0010
SW7[1-8] = 0000 0000
Fig. 7.2 MMC/SD Boot Mode¶
7.2. EVM and Daughter Card information¶
7.2.1. EVM¶
Whereas other J7 family boards consist of a Common Processor Board plus SOM, the J742S2 Evaluation Module (EVM) has these two components combined into a single board. The J742S2 EVM is the main board which includes the following:
J742S2 SoC
Leo PMIC (Power controller)
16 (2x8) GiB LPDDR4 RAM
XSPI NOR flash
In addition, the J742S2 EVM has peripherals to provide most common functionality. It has expander ports to connect to different adapter cards.
Fig. 7.7 J742S2 EVM¶
Contents of the board
4xUART to USB port for Main uarts
Port0 from this is used this for Linux, RTOS UART terminal from A72
2xUART to USB port MCU domain uarts
Port0 from this is used for Cortex M4F UART
Port1 from this is used for MCU R5F UART
6x CAN FD Interfaces
Main Domain Ethernet (CPSW2G) port
MCU Domain Ethernet (CPSW2G) port
MIPI JTAG connector
SD card slot
XDS110 on board USB JTAG connector
USB Host ports
Quad Port Ethernet daughter card (bottom of EVM) sold separately
2x Display (eDP/DP) ports
Display0 is used by software for eDP/DP output
USBC port
12V Power input
Power switch
7.2.2. Quad Port Ethernet daughter card¶
Quad Port Ethernet (QPENet) board is an adapter board which offers additional CPSW9G Ethernet port capabilities to the Jacinto7 EVM. It is connected to the bottom of the EVM beneath the 2x Display (eDP/DP) ports.
Fig. 7.8 QPENet daughter card¶
7.2.3. Fusion daughter card¶
Fusion daughter card is adapter board to connect 8 camera sensors (IMX390+UB953 serializer) through de-serializer (UB960) available on the Fusion1 daughter card to CSI2RX ports of J742S2 SoC.
Connect the daughter card to bottom side of EVM at connector J57.
Fig. 7.9 CSI2 Exp Connector¶
Fig. 7.10 Fusion1 Board¶
Fig. 7.11 Fusion1 Mounting¶