3.2.2.10.3.2.3.1. CPSW Proxy Client
3.2.2.10.3.2.3.1.1. Introduction
The CPSW Proxy Client driver in Linux interfaces with Ethernet Switch Firmware (EthFw) via RPMsg using the Linux Remoteproc framework. The CPSW Ethernet Switch on the SoC is configured by EthFw which acts as the Server and provides services to Clients on remote cores with the Linux Client on A72 core being the CPSW Proxy Client and the driver corresponding to it located at: drivers/net/ethernet/ti/cpsw-proxy-client.c in the SDK’s Linux Source.
The CPSW Proxy Client driver registers itself with the RPMsg framework and is probed when EthFw announces the endpoint name “ti.ethfw.ethdevice” over the RPMsg-bus. On being probed, the CPSW Proxy Client driver begins querying EthFw for the resources available for its use. All the ABIs used for RPMsg communication between EthFw and the CPSW Proxy Client driver are defined in: drivers/net/ethernet/ti/eth_remote_msg.h in the SDK’s Linux Source.
The network data is sent/received over DMA Channels allocated for the Linux Client’s use. The allocated channels are communicated to the Client over RPMsg.
Note
More details about EthFw can be found at: Ethernet Firmware User Guide
Note
With the migration of EthFw to the standard RPMsg framework, the RPMsg-Kdrv framework is no longer required. The cpsw-proxy-client.c driver is the new Linux Client driver for the now deprecated j721e-cpsw-virt-mac.c driver. Any logs corresponding to the older “j721e-cpsw-virt-mac.c” driver may be safely ignored.
3.2.2.10.3.2.3.1.1.1. Terminology
- Virtual Port
A virtual port refers to the Software View of an Ethernet port.
- Virtual MAC Only Port
A virtual MAC only port refers to a dedicated physical port for Linux’s use. This corresponds to MAC Mode of operation in Ethernet Terminology where there is no broadcast traffic from other Physical Ports being forwarded to Linux and at the same time there is no broadcast traffic from Linux being sent out of other Physical ports.
- Virtual Switch Port
A virtual Switch Port refers to a group of physical ports with Switching enabled across them implying that any traffic sent from Linux using the Network interface corresponding to the Virtual Switch Port could potentially exit out of any of the group of physical ports based on the ALE’s (Address Lookup Engine) decision.
- Network Interface
The user-visible interface in Linux userspace exposed to applications which serves as the entry/exit point for traffic to/from the Virtual Ports. A single network interface maps to either a Virtual MAC Only Port (implying a single physical port) or a Virtual Switch Port (implying a group of physical ports enabling the Switching functionality).
3.2.2.10.3.2.3.1.1.2. Configuration
All resources are allocated by EthFw to the Linux Client. Therefore all configuration has to be performed only in EthFw and no changes are necessary in the Linux Client. It is possible to configure the number of MAC Only Ports and Switch Ports allocated to Linux Client providing flexibility based on the use-case.
3.2.2.10.3.2.3.1.1.3. Enabling CPSW Proxy Client Driver for Linux
The following Linux build config need to be enabled for availing the CPSW Proxy Client functionality:
CONFIG_TI_CPSW_PROXY_CLIENT
The CPSW Proxy Client functionality is enabled by applying the corresponding Linux device-tree overlay at U-Boot prompt.
To enable Linux CPSW Proxy Client functionality, save the following command in uEnv.txt:
name_overlays="ti/k3-j784s4-evm-ethfw.dtbo"
Note
The overlays have to be applied to ensure that Linux doesn’t override the Serdes configuration and also to reserve Shared Memory for EthFw.
3.2.2.10.3.2.3.1.1.4. Execution Flow
The CPSW Proxy Client driver registers itself with the Linux RPMsg Framework as an RPMsg Endpoint.
EthFw announces the endpoint name “ti.ethfw.ethdevice” over the RPMsg-bus resulting in the CPSW Proxy Client driver getting probed.
On being probed, the CPSW Proxy Client driver requests EthFw for details regarding the number of Virtual Ports as well as their types.
In response to the request, EthFw replies with details regarding the allocated Virtual Ports and their types.
With the knowledge of the available Virtual Ports, the Client driver requests details of the allocated DMA Channels and MAC Addresses corresponding to each of the Virtual Ports.
The Client driver receives the details from EthFw and proceeds to request the creation of the DMA Channels using the Linux DMA APIs for requesting the DMA driver correspondig to the SoC.
The Client driver proceeds with the creation of one Network Interface per Virtual Port and registers the MAC Address corresponding to the Virtual Port with the Linux Network Subsystem.
In the case of Virtual Ports that are Switch Ports, the Client driver registers the IP Address allocated to the Network Interface with EthFw. The Network Interface could obtain an IP Address either through DHCP protocol or could be assigned a static IP Address from userspace as well.
At this point all Network Interfaces corresponding to the Virtual Ports are up and functional and can transmit and receive Network Traffic from the Ethernet Ports corresponding to the CPSW Ethernet Switch that is managed by EthFw.
3.2.2.10.3.2.3.1.1.5. Interpreting the boot logs
The CPSW Proxy Client driver logs can be filtered using the command:
dmesg | grep ti_cpsw_proxy_client
If the driver is probed successfully, something similar to the following content will show up in the filtered logs based on the configuration performed on EthFw for the allocation of Virtual Ports to the Linux Client:
ti_cpsw_proxy_client virtio2.ti.ethfw.ethdevice.-1.101: 1 Virtual Switch Port(s), 1 Virtual MAC Only P
ti_cpsw_proxy_client virtio2.ti.ethfw.ethdevice.-1.101: Virt Port: 0, Type: Switch Port, Iface: eth1, Num TX: 2, Num RX: 1, Token: 0
ti_cpsw_proxy_client virtio2.ti.ethfw.ethdevice.-1.101: Virt Port: 4, Type: MAC Port, Iface: eth2, Num TX: 1, Num RX: 1, Token: 400
The logs indicate that 1 Virtual Switch Port and 1 Virtual MAC Only Port have been allocated to the Linux Client. Therefore the CPSW Proxy Client driver shall create two interfaces corresponding to each of the Virtual Ports. The logs indicate that the network interface “eth1” corresponds to the “Switch Port” as indicated in the “Type” field. Similarly, the network interface “eth2” corresponds to the “MAC Port” (MAC Only Port). Additionally, the interface eth1 has been allocated “2” TX DMA Channels and “1” RX DMA Flow, while the interface eth2 has been allocated “1” TX DMA Channel and “1” RX DMA Flow.
3.2.2.10.3.2.3.1.1.6. Features
3.2.2.10.3.2.3.1.1.6.1. Fetching/Setting IP Address
Each interface can either get an IP address dynamically allocated to it by a DHCP server using the command:
udhcpc -i <ethX>
Or it can be assigned a Static IP address manually using the command:
ifconfig <ethX> <IP-Address>
3.2.2.10.3.2.3.1.1.6.2. Setting MAC Address
MAC Address can be assigned to interfaces using the commands:
ifconfig <ethX> down
ifconfig <ethX> hw ether <MAC-Address>
ifconfig <ethX> up
3.2.2.10.3.2.3.1.1.6.3. Multicast Filtering
EthFW supports Multicast Filtering which allows offloading Multicast addresses to CPSW Ethernet Switch thereby allowing Multicast addresses to be forwarded to Linux.
EthFW supports the following logical types of Multicast addresses:
- Exclusive Multicast Addresses
Traffic with such multicast addresses will be directed exclusively to Linux via the Linux Client driver.
- Shared Multicast Addresses
Traffic with such multicast addresses will be delivered to Linux host by other means (i.e. shared memory based TAP interface). Shared multicast addresses are used to deliver traffic to more than one core on the J742S2 SoC. The TAP interface is not implemented by the CPSW Proxy Client driver. The TAP interface has to be present and enabled in order to receive the traffic corresponding to the Shared Multicast Addresses. For more details on the TAP interface, please refer to: TAP interface for intercore traffic
- Reserved Multicast Addresses
Traffic with such multicast addresses is reserved and intended to be consumed by EthFW only.
The CPSW Proxy Client driver offloads all requested multicast addresses irrespective of their type. Reserved multicast addresses which are offloaded are treated as NOP by EthFw.
Multicast MAC addresses can be added/deleted using the ip maddr command:
# Add Multicast address <Multicast-Address>
ip maddr add <Multicast-Address> dev <ethX>
# Check if entry has been added successfully
ip maddr show dev <ethX>
# Delete Multicast address <Multicast-Address>
ip maddr del <Multicast-Address> dev <ethX>
3.2.2.10.3.2.3.1.1.6.4. TX QoS
QoS on the transmit path from the Client to the external network consists of two stages:
TX DMA Channel QoS
CPSW MAC Port FIFO QoS
3.2.2.10.3.2.3.1.1.6.4.1. Stage-1: TX DMA Channel QoS
EthFw supports allocating multiple TX DMA Channels to a Virtual Port used by the Linux Client. The presence of multiple TX DMA Channels allows the client to enable QoS functionality by distributing the traffic across the DMA Channels on the transmit path by using the mapping between the traffic priority and the DMA Channel. The “tc” framework in Linux is used to specify this mapping between the traffic priority (DSCP to SKB priority) and the traffic class (DMA Channel). There are as many traffic classes as the TX DMA Channels available for the interface. Traffic classes range from 0 to N-1 where N is the number of TX DMA Channels.
Consider the example of the interface eth1 having 2 TX DMA Channels. For the mapping defined as:
Priorities 0, 1, 2 and 3 belong to TC 0 (Traffic Class 0 => TX DMA Channel 0)
Priorities 4, 5, 6 and 7 belong to TC 1 (Traffic Class 1 => TX DMA Channel 1)
the corresponding “tc” command to be run in userspace is:
tc qdisc add dev eth1 handle 100: parent root mqprio num_tc 2 \
map 0 0 0 0 1 1 1 1 0 0 0 0 0 0 0 0 queues 1@0 1@1 hw 0
For more details on the above command, please refer: tc-mqprio
With the above command executed, all traffic transmitted on the eth1 interface from the Client having SKB priorities 0,1,2 and 3 will be sent using TX DMA Channel 0 of the eth1 interface while traffic having SKB priorities 4,5,6 and 7 will be sent using TX DMA Channel 1 of the eth1 interface.
Note
3.2.2.10.3.2.3.1.1.6.4.2. Stage-2: CPSW MAC Port FIFO QoS
When the DSCP tagged traffic sent from the Client over the TX DMA Channels is received by the CPSW Host Port, the DSCP priority of the traffic is used to determine the FIFO in the Egress MAC Port that the traffic has to be queued into. Each MAC Port has 8 TX FIFOs corresponding to 8 priorities. Traffic from different Clients having the same DSCP priority and egressing on the same MAC Port will be queued in the same TX FIFO of the MAC Port, thereby providing uniform QoS across clients.