61 #ifndef ti_sysbios_family_arm_vxm_TimestampProvider__include 62 #define ti_sysbios_family_arm_vxm_TimestampProvider__include 73 #include "TimestampProvider_defs.h" 118 extern void TimestampProvider_init(
void);
Basic constants and types.
uint32_t TimestampProvider_get32(void)
Return a 32-bit timestamp.
void TimestampProvider_getFreq(Types_FreqHz *freq)
Get the timestamp timer's frequency (in Hz)
void TimestampProvider_get64(Types_Timestamp64 *timestamp64)
Return a 64-bit timestamp.
64-bit frequency struct (in Hz)
Definition: Types.h:98
64-bit timestamp struct
Definition: Types.h:81